Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum DRV102!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 2 answers
  • Subscribers 316 subscribers
  • Views 2565 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

DRV102!

Former Member
Former Member over 11 years ago

regarding the duty cycle of TO220 How to adjust the duty cycle continuously for example from 20% to 50% to 90% and so on at one operation?

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    John, you're a borderline claim-jumper!  How are things?  Thawed out yet?

     

    When you degenerate a potentiometer into a variable resistor, the naive thing to do is connect the wiper end and use one leg of the resistor and float the other.  This leaves the unused end of the resistor to act as a little antenna, bollixing your precision.  If you tie what was going to be the free end of the resistor to the wiper, you can avoid this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to D_Hersey

    thanks a lot

    but what about if program an arduino to get the listed voltage instead of the variable resistor then i use DAC to duty cycle pin, so i can achieve  what i want which is  the operation to work continuously without manual adjusting?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to D_Hersey

    thanks a lot

    but what about if program an arduino to get the listed voltage instead of the variable resistor then i use DAC to duty cycle pin, so i can achieve  what i want which is  the operation to work continuously without manual adjusting?