Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Palladium hydride electrical generation?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 338 subscribers
  • Views 1976 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Palladium hydride electrical generation?

e14 Contributor
e14 Contributor over 12 years ago

So this is a rather complex question but can't Palladium hydride be used for generating electrical power?

 

Palladium hydride contains hydrogen gas. How much gas is in a 1 pound block though? How much electricity could that generate?

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 12 years ago

    It can - you can burn the hydrogen in a fuel cell or a heat engine. There are issues:

    1) Palladium is very expensive, but it can be used to store hydrogen at lowish pressure.

    2) The hydrogen has to come from somewhere, either from electrolysis which requires energy from one of the usual sources (nuke, fossil , solar etc) or chemically from fossil fuel.

     

    The energy density by weight and cost is quite low - which is another way of saying that there are better ways to do the same thing. There is a reason that almost all commercially available electric cars (hybrid or full) use lithium batteries - that reason is that it is currently the most cost effective solution.

     

    You would almost certainly do better to make methanol with the original input energy (and CO2 and water) and then burn that in an internal combustion engine.

     

    Google this stuff - there is lots of information around.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago

    It can - you can burn the hydrogen in a fuel cell or a heat engine. There are issues:

    1) Palladium is very expensive, but it can be used to store hydrogen at lowish pressure.

    2) The hydrogen has to come from somewhere, either from electrolysis which requires energy from one of the usual sources (nuke, fossil , solar etc) or chemically from fossil fuel.

     

    The energy density by weight and cost is quite low - which is another way of saying that there are better ways to do the same thing. There is a reason that almost all commercially available electric cars (hybrid or full) use lithium batteries - that reason is that it is currently the most cost effective solution.

     

    You would almost certainly do better to make methanol with the original input energy (and CO2 and water) and then burn that in an internal combustion engine.

     

    Google this stuff - there is lots of information around.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer