Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Ideas? Detecting a narrow frequency within an audio signal
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 2 answers
  • Subscribers 324 subscribers
  • Views 4062 views
  • Users 0 members are here
  • microprocessor_controlled
  • bandpass
  • filter
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Ideas? Detecting a narrow frequency within an audio signal

Former Member
Former Member over 11 years ago

I am looking for a way to detect the presence of a single musical note that lies within a real-world audio signal. For example, from a piano recording, I want to detect when Middle C (440 hz) is sounded while ignoring all the other notes.

 

Perhaps some kind of tunable bandpass filter would do the job? If so, it would have to be a very narrow bandpass filter because musical notes are separated in frequency by a ratio of about 1.06, which is quite close.

 

The thing might also be thought of as an AM receiver that operates with a carrier frequency not in the RF but in the audio frequency range.

 

In my application, the centre (detected) frequency will be controlled by microprocessor. The receiver will frequency-hop, quickly changing the detection frequency. I am imagining that the microprocessor might do this by supplying a clock frequency or by directly writing a digital value.

 

It does not need to be a precision circuit — simplicity and low cost are more important. The application can tolerate a fair degree of error.

 

Any ideas?

 

Thank-you!

 

Gordon Hicks

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    Three-op-amp state-variable filter perfects the notch | EDN

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MicrochipRTCfr
    0 MicrochipRTCfr over 11 years ago in reply to D_Hersey

    Hi,

     

    For detecting frequencies, DSP based architectures are generally doing much better. In general fixed point DSP units are very efficient for filters.

    As an example dsPIC from the DSC family (Digital Signal Controllers) can implement filters up to the 10th order.

    The free XC16 compiler contains DSP libraries which can be used to implement FIR, IIR or even FFT.

    The IDE is also free (MPLAB X) and runs native on Linux, Mac and windows.

    You may also want to use a specialised SW like Digital Filter Design to fasten your design.

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • MicrochipRTCfr
    0 MicrochipRTCfr over 11 years ago in reply to D_Hersey

    Hi,

     

    For detecting frequencies, DSP based architectures are generally doing much better. In general fixed point DSP units are very efficient for filters.

    As an example dsPIC from the DSC family (Digital Signal Controllers) can implement filters up to the 10th order.

    The free XC16 compiler contains DSP libraries which can be used to implement FIR, IIR or even FFT.

    The IDE is also free (MPLAB X) and runs native on Linux, Mac and windows.

    You may also want to use a specialised SW like Digital Filter Design to fasten your design.

     

    Regards