Hello - forgive me if this is a double up. I have a raspberry pi B version 2 with the Volumio image that was modified to include the wolfson drivers by folks on that forum. I have only been able to get white noise out of the line out and headphone out. Here is output from dmesg.
I hope someone can help.
Thanks,
George
Volumio 1.4 wolfson image - edited config.txt to kernel=kernel_new.img - changed the mixer setting to software and ran dmesg.
Here is the output:
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 3.12.13-rt21+ (georg@musicbox) (gcc version 4.8.3 20140106 (prerelease) (crosstool-NG linaro-1.13.1-4.8-2014.01 - Linaro GCC 2013.11) ) #1 PREEMPT RT Thu Mar 27 16:58:09 CET 2014
[ 0.000000] CPU: ARMv6-compatible processor [410fb767] revision 7 (ARMv7), cr=00c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
[ 0.000000] Machine: BCM2708
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] On node 0 totalpages: 126976
[ 0.000000] free_area_init_node: node 0, pgdat c069a0e4, node_mem_map c074e000
[ 0.000000] Normal zone: 992 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 126976 pages, LIFO batch:31
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 125984
[ 0.000000] Kernel command line: dma.dmachans=0x7f35 bcm2708_fb.fbwidth=1184 bcm2708_fb.fbheight=624 bcm2708.boardrev=0xe bcm2708.serial=0xd2fba881 smsc95xx.macaddr=B8:27:EB:FB:A8:81 sdhci-bcm2708.emmc_clock_freq=250000000 vc_mem.mem_base=0x1fa00000 vc_mem.mem_size=0x20000000 force_turbo=1 dwc_otg.lpm_enable=0 console=ttyAMA0,115200 kgdboc=ttyAMA0,115200 console=tty1 root=/dev/mmcblk0p3 elevator=noop rootfstype=ext4 rootwait smsc95xx.turbo_mode=N
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] allocated 3555328 bytes of page_cgroup
[ 0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups
[ 0.000000] Memory: 492520K/507904K available (4500K kernel code, 299K rwdata, 1780K rodata, 147K init, 714K bss, 15384K reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xdf800000 - 0xff000000 ( 504 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xdf000000 ( 496 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc062a294 (6281 kB)
[ 0.000000] .init : 0xc062b000 - 0xc064fe54 ( 148 kB)
[ 0.000000] .data : 0xc0650000 - 0xc069acc8 ( 300 kB)
[ 0.000000] .bss : 0xc069acd4 - 0xc074d648 ( 715 kB)
[ 0.000000] SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:460
[ 0.000000] sched_clock: 32 bits at 1000kHz, resolution 1000ns, wraps every 4294967ms
[ 0.000000] Switching to timer-based delay loop
[ 0.000000] Console: colour dummy device 80x30
[ 0.000000] console [tty1] enabled
[ 0.001388] Calibrating delay loop (skipped), value calculated using timer frequency.. 2.00 BogoMIPS (lpj=10000)
[ 0.001393] pid_max: default: 32768 minimum: 301
[ 0.001936] Mount-cache hash table entries: 512
[ 0.002774] Initializing cgroup subsys memory
[ 0.002856] Initializing cgroup subsys devices
[ 0.002865] Initializing cgroup subsys freezer
[ 0.002873] Initializing cgroup subsys blkio
[ 0.003017] CPU: Testing write buffer coherency: ok
[ 0.003420] Setting up static identity map for 0xc04475c0 - 0xc044761c
[ 0.006245] devtmpfs: initialized
[ 0.018956] VFP support v0.3: implementor 41 architecture 1 part 20 variant b rev 5
[ 0.019873] regulator-dummy: no parameters
[ 0.020494] NET: Registered protocol family 16
[ 0.025496] DMA: preallocated 4096 KiB pool for atomic coherent allocations
[ 0.026171] cpuidle: using governor ladder
[ 0.026220] cpuidle: using governor menu
[ 0.026703] bcm2708.uart_clock = 0
[ 0.028875] hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
[ 0.028934] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.028971] mailbox: Broadcom VideoCore Mailbox driver
[ 0.029350] bcm2708_vcio: mailbox at f200b880
[ 0.029496] bcm_power: Broadcom power driver
[ 0.029536] bcm_power_open() -> 0
[ 0.029562] bcm_power_request(0, 8)
[ 0.530294] bcm_mailbox_read -> 00000080, 0
[ 0.530340] bcm_power_request -> 0
[ 0.530634] Serial: AMBA PL011 UART driver
[ 0.530801] dev:f1: ttyAMA0 at MMIO 0x20201000 (irq = 83, base_baud = 0) is a PL011 rev3
[ 0.906639] console [ttyAMA0] enabled
[ 0.936711] bio: create slab <bio-0> at 0
[ 0.942059] platform bcm2708-dmaengine: Driver bcm2708-dmaengine requests probe deferral
[ 0.950433] DC_3V3: 1800 mV
[ 0.953629] DC_5V: 5000 mV
[ 0.957101] SCSI subsystem initialized
[ 0.961090] usbcore: registered new interface driver usbfs
[ 0.966701] usbcore: registered new interface driver hub
[ 0.972303] usbcore: registered new device driver usb
[ 0.977902] Advanced Linux Sound Architecture Driver Initialized.
[ 0.985240] Switched to clocksource stc
[ 0.989567] FS-Cache: Loaded
[ 0.992772] CacheFiles: Loaded
[ 1.010140] NET: Registered protocol family 2
[ 1.015837] TCP established hash table entries: 4096 (order: 3, 32768 bytes)
[ 1.023064] TCP bind hash table entries: 4096 (order: 4, 98304 bytes)
[ 1.029765] TCP: Hash tables configured (established 4096 bind 4096)
[ 1.036228] TCP: reno registered
[ 1.039490] UDP hash table entries: 256 (order: 2, 16384 bytes)
[ 1.045481] UDP-Lite hash table entries: 256 (order: 2, 16384 bytes)
[ 1.052418] NET: Registered protocol family 1
[ 1.057486] RPC: Registered named UNIX socket transport module.
[ 1.063448] RPC: Registered udp transport module.
[ 1.068169] RPC: Registered tcp transport module.
[ 1.072891] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.080356] bcm2708_dma: DMA manager at f2007000
[ 1.085115] bcm2708_gpio: bcm2708_gpio_probe c065e080
[ 1.090680] vc-mem: phys_addr:0x00000000 mem_base=0x1fa00000 mem_size:0x20000000(512 MiB)
[ 1.100263] audit: initializing netlink socket (disabled)
[ 1.105771] type=2000 audit(1.100:1): initialized
[ 1.292030] VFS: Disk quotas dquot_6.5.2
[ 1.296338] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.306038] FS-Cache: Netfs 'nfs' registered for caching
[ 1.312919] NFS: Registering the id_resolver key type
[ 1.318093] Key type id_resolver registered
[ 1.322299] Key type id_legacy registered
[ 1.327107] msgmni has been set to 961
[ 1.333313] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)
[ 1.341144] io scheduler noop registered (default)
[ 1.345980] io scheduler deadline registered
[ 1.350631] io scheduler cfq registered
[ 1.354882] bcm2708_fb_debugfs_init: could not create debugfs entry
[ 1.361287] BCM2708FB: allocated DMA memory 5e9a0000
[ 1.366543] BCM2708FB: allocated DMA channel 0 @ f2007000
[ 1.380837] Console: switching to colour frame buffer device 148x39
[ 1.393290] uart-pl011 dev:f1: no DMA platform data
[ 1.398315] kgdb: Registered I/O driver kgdboc.
[ 1.403635] vc-cma: Videocore CMA driver
[ 1.407660] vc-cma: vc_cma_base = 0x00000000
[ 1.414731] vc-cma: vc_cma_size = 0x00000000 (0 MiB)
[ 1.422609] vc-cma: vc_cma_initial = 0x00000000 (0 MiB)
[ 1.441596] brd: module loaded
[ 1.453258] loop: module loaded
[ 1.459176] vchiq: vchiq_init_state: slot_zero = 0xdf804000, is_master = 0
[ 1.469522] Loading iSCSI transport class v2.0-870.
[ 1.478674] bcm2708_spi bcm2708_spi.0: master is unqueued, this is deprecated
[ 1.491427] LDO1: 1200 <--> 1800 mV at 1800 mV
[ 1.498413] LDO1: supplied by DC_3V3
[ 1.526836] arizona spi0.1: WM5102 revision C
[ 1.546679] MICVDD: 1700 <--> 3300 mV at 3000 mV
[ 1.553844] MICVDD: supplied by DC_3V3
[ 1.560332] gpiochip_find_base: cannot find free range
[ 1.567782] gpiochip_add: gpios -1..3 (arizona) failed to register
[ 1.576266] arizona-gpio arizona-gpio: Could not register gpiochip, -28
[ 1.585185] arizona-gpio: probe of arizona-gpio failed with error -28
[ 1.594754] bcm2708_spi bcm2708_spi.0: SPI Controller at 0x20204000 (irq 80)
[ 1.604501] usbcore: registered new interface driver smsc95xx
[ 1.612722] dwc_otg: version 3.00a 10-AUG-2012 (platform bus)
[ 1.821019] Core Release: 2.80a
[ 1.826555] Setting default values for core params
[ 1.833692] Finished setting default values for core params
[ 2.041949] Using Buffer DMA mode
[ 2.047559] Periodic Transfer Interrupt Enhancement - disabled
[ 2.055733] Multiprocessor Interrupt Enhancement - disabled
[ 2.063622] OTG VER PARAM: 0, OTG VER FLAG: 0
[ 2.070388] Dedicated Tx FIFOs mode
[ 2.076611] dwc_otg: Microframe scheduler enabled
[ 2.076671] dwc_otg bcm2708_usb: DWC OTG Controller
[ 2.083988] dwc_otg bcm2708_usb: new USB bus registered, assigned bus number 1
[ 2.093981] dwc_otg bcm2708_usb: irq 32, io mem 0x00000000
[ 2.101973] Init: Port Power? op_state=1
[ 2.108210] Init: Power Port (0)
[ 2.113967] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.123261] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.132914] usb usb1: Product: DWC OTG Controller
[ 2.140126] usb usb1: Manufacturer: Linux 3.12.13-rt21+ dwc_otg_hcd
[ 2.148776] usb usb1: SerialNumber: bcm2708_usb
[ 2.156714] hub 1-0:1.0: USB hub found
[ 2.162966] hub 1-0:1.0: 1 port detected
[ 2.170080] dwc_otg: FIQ enabled
[ 2.170102] dwc_otg: NAK holdoff enabled
[ 2.170111] dwc_otg: FIQ split fix enabled
[ 2.170132] Module dwc_common_port init
[ 2.170642] usbcore: registered new interface driver usb-storage
[ 2.179520] mousedev: PS/2 mouse device common for all mice
[ 2.187517] i2c /dev entries driver
[ 2.193544] bcm2708_i2c_init_pinmode(0,0)
[ 2.200109] bcm2708_i2c_init_pinmode(0,1)
[ 2.207133] bcm2708_i2c bcm2708_i2c.0: BSC0 Controller at 0x20205000 (irq 79) (baudrate 100k)
[ 2.218151] bcm2708_i2c_init_pinmode(1,2)
[ 2.224577] bcm2708_i2c_init_pinmode(1,3)
[ 2.231814] bcm2708_i2c bcm2708_i2c.1: BSC1 Controller at 0x20804000 (irq 79) (baudrate 100k)
[ 2.243718] bcm2835-cpufreq: min=700000 max=700000 cur=700000
[ 2.252116] bcm2835-cpufreq: switching to governor powersave
[ 2.260155] bcm2835-cpufreq: switching to governor powersave
[ 2.268254] sdhci: Secure Digital Host Controller Interface driver
[ 2.276785] sdhci: Copyright(c) Pierre Ossman
[ 2.283568] sdhci: Enable low-latency mode
[ 2.290420] mmc0: no vqmmc regulator found
[ 2.296783] mmc0: no vmmc regulator found
[ 2.345413] mmc0: SDHCI controller on BCM2708_Arasan [platform] using platform's DMA
[ 2.365083] mmc0: BCM2708 SDHC host at 0x20300000 DMA 2 IRQ 77
[ 2.365521] Indeed it is in host mode hprt0 = 00021501
[ 2.413028] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.432856] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.437454] mmc0: new high speed SDHC card at address aaaa
[ 2.445385] mmcblk0: mmc0:aaaa SL16G 14.8 GiB
[ 2.446940] mmcblk0: p1 p3
[ 2.486829] usbcore: registered new interface driver usbhid
[ 2.494765] usbhid: USB HID core driver
[ 2.501179] platform arizona-extcon: Driver arizona-extcon requests probe deferral
[ 2.512557] ------------[ cut here ]------------
[ 2.519653] WARNING: CPU: 0 PID: 1 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()
[ 2.529639] sysfs: cannot create duplicate filename '/devices/platform/bcm2708_spi.0/spi_master/spi0/spi0.1/regulator/regulator.3/spi0.1-DCVDD'
[ 2.545064] Modules linked in:
[ 2.550729] CPU: 0 PID: 1 Comm: swapper Not tainted 3.12.13-rt21+ #1
[ 2.559744] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)
[ 2.570978] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)
[ 2.582658] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)
[ 2.595086] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)
[ 2.605385] usb 1-1: new high-speed USB device number 2 using dwc_otg
[ 2.605680] Indeed it is in host mode hprt0 = 00001101
[ 2.642891] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)
[ 2.675337] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)
[ 2.696804] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)
[ 2.717585] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)
[ 2.729842] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0373064>] (wm_adsp2_init+0x5c/0x13c)
[ 2.743749] [<c0373064>] (wm_adsp2_init+0x5c/0x13c) from [<c0370d78>] (wm5102_probe+0x90/0x188)
[ 2.757516] [<c0370d78>] (wm5102_probe+0x90/0x188) from [<c02854e0>] (really_probe+0x60/0x1e4)
[ 2.770957] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0285750>] (__driver_attach+0x98/0x9c)
[ 2.784696] [<c0285750>] (__driver_attach+0x98/0x9c) from [<c0283a84>] (bus_for_each_dev+0x60/0x94)
[ 2.798987] [<c0283a84>] (bus_for_each_dev+0x60/0x94) from [<c0284d5c>] (bus_add_driver+0x1c4/0x274)
[ 2.813206] [<c0284d5c>] (bus_add_driver+0x1c4/0x274) from [<c0285d54>] (driver_register+0x78/0xf8)
[ 2.827508] [<c0285d54>] (driver_register+0x78/0xf8) from [<c000861c>] (do_one_initcall+0x114/0x178)
[ 2.841784] [<c000861c>] (do_one_initcall+0x114/0x178) from [<c062bb74>] (kernel_init_freeable+0xf4/0x1b4)
[ 2.857120] [<c062bb74>] (kernel_init_freeable+0xf4/0x1b4) from [<c043c51c>] (kernel_init+0x8/0x150)
[ 2.866256] usb 1-1: New USB device found, idVendor=0424, idProduct=9512
[ 2.866327] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 2.895685] [<c043c51c>] (kernel_init+0x8/0x150) from [<c000e058>] (ret_from_fork+0x14/0x3c)
[ 2.909440] ---[ end trace 0000000000000001 ]---
[ 2.920377] LDO1: could not add device link spi0.1 err -17
[ 2.921083] hub 1-1:1.0: USB hub found
[ 2.921374] hub 1-1:1.0: 3 ports detected
[ 2.952773] LDO1: Failed to create debugfs directory
[ 2.970969] bcm2708-i2s bcm2708-i2s.0: Failed to create debugfs directory
[ 3.195514] usb 1-1.1: new high-speed USB device number 3 using dwc_otg
[ 3.316200] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00
[ 3.335305] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 3.358329] smsc95xx v1.0.4
[ 3.434174] smsc95xx 1-1.1:1.0 eth0: register 'smsc95xx' at usb-bcm2708_usb-1.1, smsc95xx USB 2.0 Ethernet, b8:27:eb:fb:a8:81
[ 3.545565] usb 1-1.2: new full-speed USB device number 4 using dwc_otg
[ 3.677600] usb 1-1.2: New USB device found, idVendor=046d, idProduct=c52b
[ 3.696434] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 3.715561] usb 1-1.2: Product: USB Receiver
[ 3.722973] usb 1-1.2: Manufacturer: Logitech
[ 3.767474] input: Logitech USB Receiver as /devices/platform/bcm2708_usb/usb1/1-1/1-1.2/1-1.2:1.0/input/input0
[ 3.790274] hid-generic 0003:046D:C52B.0001: input,hidraw0: USB HID v1.11 Keyboard [Logitech USB Receiver] on usb-bcm2708_usb-1.2/input0
[ 3.846437] input: Logitech USB Receiver as /devices/platform/bcm2708_usb/usb1/1-1/1-1.2/1-1.2:1.1/input/input1
[ 3.867764] hid-generic 0003:046D:C52B.0002: input,hiddev0,hidraw1: USB HID v1.11 Mouse [Logitech USB Receiver] on usb-bcm2708_usb-1.2/input1
[ 3.912972] hid-generic 0003:046D:C52B.0003: hiddev0,hidraw2: USB HID v1.11 Device [Logitech USB Receiver] on usb-bcm2708_usb-1.2/input2
[ 4.025603] usb 1-1.3: new high-speed USB device number 5 using dwc_otg
[ 4.137164] usb 1-1.3: New USB device found, idVendor=1e3d, idProduct=2096
[ 4.149013] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 4.165363] usb 1-1.3: Product: Flash Disk
[ 4.177145] usb 1-1.3: Manufacturer: Generic
[ 4.190295] usb 1-1.3: SerialNumber: CCBB1108020140313241603106
[ 4.206480] usb-storage 1-1.3:1.0: USB Mass Storage device detected
[ 4.223932] scsi0 : usb-storage 1-1.3:1.0
[ 5.004296] wm8804 1-003a: revision E
[ 5.013429] bcm2708-i2s bcm2708-i2s.0: ASoC: pcm constructor failed: -517
[ 5.024049] snd-rpi-wsp snd-rpi-wsp.0: ASoC: can't create pcm WM5102 AiFi :-517
[ 5.034711] snd-rpi-wsp snd-rpi-wsp.0: ASoC: failed to instantiate card -517
[ 5.057394] snd-rpi-wsp snd-rpi-wsp.0: Failed to register card: -517
[ 5.067236] platform snd-rpi-wsp.0: Driver snd-rpi-wsp requests probe deferral
[ 5.079079] TCP: cubic registered
[ 5.085794] Initializing XFRM netlink socket
[ 5.093740] NET: Registered protocol family 17
[ 5.102298] Key type dns_resolver registered
[ 5.111669] registered taskstats version 1
[ 5.121239] platform arizona-extcon: Driver arizona-extcon requests probe deferral
[ 5.226857] scsi 0:0:0:0: Direct-Access Generic Flash Disk 5.00 PQ: 0 ANSI: 2
[ 5.247102] sd 0:0:0:0: [sda] 3913728 512-byte logical blocks: (2.00 GB/1.86 GiB)
[ 5.263106] sd 0:0:0:0: [sda] Write Protect is off
[ 5.272988] sd 0:0:0:0: [sda] Mode Sense: 0b 00 00 08
[ 5.274037] sd 0:0:0:0: [sda] No Caching mode page found
[ 5.286464] sd 0:0:0:0: [sda] Assuming drive cache: write through
[ 5.306960] sd 0:0:0:0: [sda] No Caching mode page found
[ 5.318299] sd 0:0:0:0: [sda] Assuming drive cache: write through
[ 5.330221] sda: sda1
[ 5.346245] sd 0:0:0:0: [sda] No Caching mode page found
[ 5.358043] sd 0:0:0:0: [sda] Assuming drive cache: write through
[ 5.370051] sd 0:0:0:0: [sda] Attached SCSI removable disk
[ 6.199061] ------------[ cut here ]------------
[ 6.206576] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()
[ 6.216963] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.0/regulator/regulator.1/wm5102-codec-DBVDD2'
[ 6.231772] Modules linked in:
[ 6.237755] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G W 3.12.13-rt21+ #1
[ 6.248672] Workqueue: deferwq deferred_probe_work_func
[ 6.257259] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)
[ 6.268751] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)
[ 6.280954] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)
[ 6.293589] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)
[ 6.306103] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)
[ 6.318899] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)
[ 6.332121] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)
[ 6.344875] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)
[ 6.357482] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)
[ 6.371238] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)
[ 6.385599] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)
[ 6.399061] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)
[ 6.412507] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)
[ 6.426476] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)
[ 6.439132] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)
[ 6.451578] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)
[ 6.464428] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)
[ 6.476967] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)
[ 6.490680] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)
[ 6.504144] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)
[ 6.517080] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)
[ 6.529379] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)
[ 6.541274] ---[ end trace 0000000000000003 ]---
[ 6.549833] DC_3V3: could not add device link wm5102-codec err -17
[ 6.560036] DC_3V3: Failed to create debugfs directory
[ 6.569037] ------------[ cut here ]------------
[ 6.577494] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()
[ 6.588922] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.0/regulator/regulator.1/wm5102-codec-DBVDD3'
[ 6.605022] Modules linked in:
[ 6.611958] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G W 3.12.13-rt21+ #1
[ 6.623981] Workqueue: deferwq deferred_probe_work_func
[ 6.633345] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)
[ 6.645914] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)
[ 6.659046] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)
[ 6.672760] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)
[ 6.685672] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)
[ 6.699432] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)
[ 6.713681] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)
[ 6.726896] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)
[ 6.740162] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)
[ 6.754516] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)
[ 6.769544] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)
[ 6.783520] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)
[ 6.797534] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)
[ 6.811851] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)
[ 6.825333] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)
[ 6.838112] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)
[ 6.851051] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)
[ 6.864060] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)
[ 6.877954] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)
[ 6.892039] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)
[ 6.905489] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)
[ 6.917633] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)
[ 6.929819] ---[ end trace 0000000000000004 ]---
[ 6.938289] DC_3V3: could not add device link wm5102-codec err -17
[ 6.948249] DC_3V3: Failed to create debugfs directory
[ 6.957474] ------------[ cut here ]------------
[ 6.966081] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()
[ 6.977723] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.0/regulator/regulator.1/wm5102-codec-CPVDD'
[ 6.993599] Modules linked in:
[ 7.000895] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G W 3.12.13-rt21+ #1
[ 7.012555] Workqueue: deferwq deferred_probe_work_func
[ 7.021774] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)
[ 7.034452] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)
[ 7.047544] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)
[ 7.061088] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)
[ 7.074302] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)
[ 7.087794] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)
[ 7.101631] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)
[ 7.115044] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)
[ 7.128547] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)
[ 7.142705] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)
[ 7.157694] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)
[ 7.171828] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)
[ 7.185951] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)
[ 7.200045] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)
[ 7.213147] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)
[ 7.226422] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)
[ 7.239216] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)
[ 7.251926] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)
[ 7.266016] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)
[ 7.279918] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)
[ 7.293008] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)
[ 7.305537] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)
[ 7.317449] ---[ end trace 0000000000000005 ]---
[ 7.326134] DC_3V3: could not add device link wm5102-codec err -17
[ 7.336386] DC_3V3: Failed to create debugfs directory
[ 7.345377] ------------[ cut here ]------------
[ 7.353841] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()
[ 7.365348] sysfs: cannot create duplicate filename '/devices/platform/bcm2708_spi.0/spi_master/spi0/spi0.1/regulator/regulator.4/wm5102-codec-MICVDD'
[ 7.386901] Modules linked in:
[ 7.393953] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G W 3.12.13-rt21+ #1
[ 7.405691] Workqueue: deferwq deferred_probe_work_func
[ 7.414935] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)
[ 7.427549] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)
[ 7.440651] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)
[ 7.454079] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)
[ 7.467339] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)
[ 7.481219] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)
[ 7.495111] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)
[ 7.508291] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)
[ 7.521702] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)
[ 7.535879] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)
[ 7.550651] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)
[ 7.564779] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)
[ 7.579041] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)
[ 7.593319] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)
[ 7.606501] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)
[ 7.619361] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)
[ 7.632371] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)
[ 7.645253] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)
[ 7.659333] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)
[ 7.673381] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)
[ 7.686498] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)
[ 7.698833] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)
[ 7.710942] ---[ end trace 0000000000000006 ]---
[ 7.719463] MICVDD: could not add device link wm5102-codec err -17
[ 7.729493] MICVDD: Failed to create debugfs directory
[ 7.738604] ------------[ cut here ]------------
[ 7.747009] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()
[ 7.758676] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.1/regulator/regulator.2/wm5102-codec-SPKVDDL'
[ 7.774865] Modules linked in:
[ 7.781821] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G W 3.12.13-rt21+ #1
[ 7.793684] Workqueue: deferwq deferred_probe_work_func
[ 7.802847] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)
[ 7.815556] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)
[ 7.828482] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)
[ 7.842220] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)
[ 7.855173] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)
[ 7.868735] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)
[ 7.882901] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)
[ 7.896321] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)
[ 7.909519] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)
[ 7.923867] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)
[ 7.938886] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)
[ 7.952916] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)
[ 7.966939] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)
[ 7.981104] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)
[ 7.994629] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)
[ 8.007707] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)
[ 8.020449] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)
[ 8.033421] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)
[ 8.047318] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)
[ 8.061221] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)
[ 8.074624] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)
[ 8.086955] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)
[ 8.098987] ---[ end trace 0000000000000007 ]---
[ 8.107624] DC_5V: could not add device link wm5102-codec err -17
[ 8.117738] DC_5V: Failed to create debugfs directory
[ 8.126935] ------------[ cut here ]------------
[ 8.135445] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()
[ 8.146890] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.1/regulator/regulator.2/wm5102-codec-SPKVDDR'
[ 8.163108] Modules linked in:
[ 8.170439] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G W 3.12.13-rt21+ #1
[ 8.182003] Workqueue: deferwq deferred_probe_work_func
[ 8.191288] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)
[ 8.203675] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)
[ 8.216877] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)
[ 8.230408] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)
[ 8.243604] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)
[ 8.257486] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)
[ 8.271327] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)
[ 8.284383] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)
[ 8.297986] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)
[ 8.312161] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)
[ 8.327060] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)
[ 8.341129] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)
[ 8.355270] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)
[ 8.369582] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)
[ 8.382719] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)
[ 8.395853] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)
[ 8.408914] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)
[ 8.421618] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)
[ 8.435632] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)
[ 8.449755] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)
[ 8.462886] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)
[ 8.475341] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)
[ 8.487514] ---[ end trace 0000000000000008 ]---
[ 8.495955] DC_5V: could not add device link wm5102-codec err -17
[ 8.505941] DC_5V: Failed to create debugfs directory
[ 8.516191] genirq: Flags mismatch irq 404. 00002000 (Thermal warning) vs. 00002000 (Thermal warning)
[ 8.516235] arizona spi0.1: Failed to get thermal warning IRQ: -16
[ 8.539859] genirq: Flags mismatch irq 405. 00002000 (Thermal shutdown) vs. 00002000 (Thermal shutdown)
[ 8.539894] arizona spi0.1: Failed to get thermal shutdown IRQ: -16
[ 9.357971] wm8804 1-003a: revision E
[ 9.370678] snd-rpi-wsp snd-rpi-wsp.0: wm5102-aif1 <-> bcm2708-i2s.0 mapping ok
[ 9.635324] arizona spi0.1: FLL1: Timed out waiting for lock
[ 9.751283] input: Headset as /devices/platform/bcm2708_spi.0/spi_master/spi0/spi0.1/arizona-extcon/input/input2
[ 9.765733] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[ 9.779653] ALSA device list:
[ 9.786824] #0: snd_rpi_wsp
[ 9.793489] #1: bcm2835 ALSA
[ 9.817235] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
[ 9.829353] VFS: Mounted root (ext4 filesystem) on device 179:3.
[ 9.849958] devtmpfs: mounted
[ 9.857334] Freeing unused kernel memory: 144K (c062b000 - c064f000)
[ 11.706818] udevd[178]: starting version 175
[ 17.279454] FAT-fs (sda1): utf8 is not a recommended IO charset for FAT filesystems, filesystem will be case sensitive!
[ 22.426633] EXT4-fs (mmcblk0p3): re-mounted. Opts: (null)
[ 22.984120] EXT4-fs (mmcblk0p3): Mount option "nouser_xattr" will be removed by 3.5
[ 22.984120] Contact linux-ext4@vger.kernel.org if you think we should keep it.
[ 22.984120]
[ 23.013262] EXT4-fs (mmcblk0p3): re-mounted. Opts: nouser_xattr,errors=remount-ro
[ 30.557712] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 33.920234] NET: Registered protocol family 10
[ 34.383429] smsc95xx 1-1.1:1.0 eth0: hardware isn't capable of remote wakeup
[ 34.396243] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 36.005659] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 36.009996] smsc95xx 1-1.1:1.0 eth0: link up, 100Mbps, full-duplex, lpa 0xCDE1
[ 44.751296] Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
[ 206.942589] bcm2835-cpufreq: switching to governor performance
[ 206.952880] bcm2835-cpufreq: switching to governor performance
[ 208.515088] arizona spi0.1: FLL1: Timed out waiting for lock
[ 208.532148] bcm2708-i2s bcm2708-i2s.0: I2S SYNC error!
[ 310.227715] EXT4-fs (mmcblk0p3): error count: 3
[ 310.236615] EXT4-fs (mmcblk0p3): initial error at 1396987247: mb_free_blocks:1426: block 309248
[ 310.249886] EXT4-fs (mmcblk0p3): last error at 1396987322: ext4_remount:4680