I am hoping to be able to take a serial protocol being sent over a 30V / 45mA current loop and translate the signal to send / receive from an Arduino's serial port.
My thoughts for reading the data into the Arduino are to use a TLP759 optocoupler and adapt the common MIDI IN circuit (see image below) since MIDI is also a current loop protocol. Obviously the values for the resistors would need to be different? I'm not certain the TLP759 is the right fit - I'm just going on the fact that it seems 30V / 45mA tolerant?
Haven't thought ahead to sending back from the Arduino - but perhaps a MIDI OUT circuit could be adapted as well? But the 30V / 5V conflict might cause problems??