Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum TLP759 Optocoupler - 30V / 45mA current loop?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 304 subscribers
  • Views 956 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

TLP759 Optocoupler - 30V / 45mA current loop?

uxe
uxe over 10 years ago

I am hoping to be able to take a serial protocol being sent over a 30V / 45mA current loop and translate the signal to send / receive from an Arduino's serial port.

 

My thoughts for reading the data into the Arduino are to use a TLP759 optocoupler and adapt the common MIDI IN circuit (see image below) since MIDI is also a current loop protocol. Obviously the values for the resistors would need to be different? I'm not certain the TLP759 is the right fit - I'm just going on the fact that it seems 30V / 45mA tolerant?

 

Haven't thought ahead to sending back from the Arduino - but perhaps a MIDI OUT circuit could be adapted as well? But the 30V / 5V conflict might cause problems??

 

Would be eternally grateful for any assistance!!image

  • Sign in to reply
  • Cancel
  • uxe
    0 uxe over 10 years ago

    So, have had some progress on this, using an incredibly simple circuit consisting of just one 110 Ohm resistor to translate the ~2mA to 45mA current loop signal into a 0-5V voltage that can be directly read by an Arduino serial port! Like this:

     

    image

     

    The problem I have now is being able to transmit a signal back on the same loop... I have thought about triggering a digital potentiometer's resistance up and down to emulate the ~2mA to 45mA protocol, or using a transistor like this - but the problem is that by grounding the loop as shown in the above circuit I don't have a current anymore on the return loop to work with!

     

    Am hoping for an equally simple / elegant solution for being able to talk back down the loop instead of just listening in?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • uxe
    0 uxe over 10 years ago in reply to clem57

    Clem, the image I included is the standard MIDI to Arduino circuit using a 6N138 optocoupler - this is a circuit I am already familiar with and have used before.

     

    I am hoping to be able to use it as a starting point to adapt for use with TLP759 optocoupler and a 30V / 45mA current loop - but I need some help figuring out the resistor values, or even deciding if using a MIDI circuit as a starting point is the right direction?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    In the datasheet the R1 value is 1.9K ohms where you have just 270 ohms. Did you do that for any reason? I assume you are doing a modified timing test circuit.

     

    Clem