Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum control multiple TLC5940?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 303 subscribers
  • Views 884 views
  • Users 0 members are here
  • tlc5940
  • arduino
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

control multiple TLC5940?

magnus2112
magnus2112 over 10 years ago

So, my question is how do i control multiple TLC5940? I know i can connect them together, http://tlc5940arduino.googlecode.com/svn/wiki/images/breadboard-arduino-tlc5940.png, but i dont know how to "activate" the pins on the second TLC

In the code i have added by GreatScott!, tries Scott to make a matrix display. In his code it is following:

 

#include "Tlc5940.h"  //don't forget to download the Tlc5940 lib from arduino playground ( http://tlc5940arduino.googlecode.com/files/Tlc5940_r014_2.zip)

 

#define RowOne 8      //Gate of 1.MOSFET which connects to Row "a" (anodes of all LEDs in Row "a")

#define RowTwo 7      //Gate of 2.MOSFET which connects to Row "b" (anodes of all LEDS in Row "b")

#define RowThree 6    //Gate of 3.MOSFET which connects to Row "c" (anodes of all LEDs in Row "c")

#define RowFour 5    //Gate of 4.MOSFET which connects to Row "d" (anodes of all LEDs in Row "d")

#define RowFive 4    //Gate of 5.MOSFET which connects to Row "e" (anodes of all LEDs in Row "e")

 

my question is: How can i define a pin to be on the second TLC?, and not on the first.

  • Sign in to reply
  • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    these are a device you can simply daisy chain, data in on the first, the out of the first goes to the in of the next, etc.

     

    in the library you should be able to set the number of output that make up the chain (In units of 16 of course)

     

    it should be as simple as that

     

    oh and you need to output the complete chain in sequence on each itteration / refresh

     

    hope this helps, if not let me know and ill dig up some old code i should have somewhgere to show this

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • magnus2112
    0 magnus2112 over 10 years ago in reply to Robert Peter Oakes

    Thanks for your hjelp image

    After searching online for a while on how to "dasy chain" the TLC5940, i found a tutorial!

    http://tronixstuff.com/2013/10/21/tutorial-arduino-tlc5940-led-driver-ic/

     

    You can daisy-chain quite a few TLC5940s together to control more LEDs. First – wire up the next TLC5940 to the Arduino as shown in the demonstration circuit – except connect the SOUT pin (17) of the first TLC5940 to the SIN pin (26) of the second TLC5940 – as the data travels from the Arduino, through the first TLC5940 to the second and so on. Then repeat the process if you have a third, etc. Don’t forget the resisotr that sets the current!

    Next, open the file tlc_config.h located in the TLC5940 library folder. Change the value of NUM_TLCS to the number of TLC5940s you have connected together, then save the file and also delete the file Tlc5940.o also located in the same folder. Finally restart the IDE. You can then refer to the channels of the second and further TLC5940 sequentially from the first. That is, the first is 0~15, the second is 16~29, and so on