Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum My project Development case Idea
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 22 replies
  • Subscribers 305 subscribers
  • Views 2379 views
  • Users 0 members are here
  • ask_an_expert
  • rasberry
  • arduino
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

My project Development case Idea

chrisdracko
chrisdracko over 10 years ago

My project Development case idea


Due to limited space this case would be quick to set up as a multi functional development flight case


The case lid will be holding a 7“ vga lcd display this display works on 12v  the case lid will also have access to the raspberry pi gpio pins and the arduino gpio pins  and have the ability to connect the leds under then with jumper cables there will also be two  20mm speakers available that is connected to the raspberry pi via a small amplifier running about 5v i'm guessing


image


The bottom of the flight case will have to levels the bottom level will hold the raspberry pi and the arduino as well as a usb hub.

the top level would be interchangeable to allow for expansion  like holding a breadboard or led matrix. or relays   image


Can you help


I want to power the main components with one power supply this will need at least one 12v line as well as three  5v lines able to supply the opriate amps


lcd  Supply Voltage: DC 9-35V

Arduino 5v

Raspberry Pi 5v

usb hub 5v


  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago +2
    Ebay has plenty of pre assembled switching voltage regulators. Since you just need common voltage rails, these would be much easier than making your own.
  • chrisdracko
    chrisdracko over 10 years ago +1
Parents
  • clem57
    0 clem57 over 10 years ago

    Is this what you had in mind? http://www.alibaba.com/showroom/multi-functional-travel-storage-case.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisdracko
    0 chrisdracko over 10 years ago in reply to clem57

    I already have a small case I want to fit it in but not shore how to sort the power requirements outimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to chrisdracko

    Good looking case. Are you going to use a battery?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisdracko
    0 chrisdracko over 10 years ago in reply to clem57

    would love to but thats where im stuck at providing enough power for the lcd screen raspberry pi and ardrino although might be a good idea to also be able to switch the ardrino and pi on and off when needed so if one isnt being used at the time being able to deactivate it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisdracko
    0 chrisdracko over 10 years ago in reply to chrisdracko

    case is from a old toolset i had its nice and small and compact

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to chrisdracko

    Why both Pi and Arduino? Maybe there are other things to do what you want without too much hardware...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisdracko
    0 chrisdracko over 10 years ago in reply to clem57

    my thinking is that this would allow the pi to program the arduino on the go as well as show output and information back from the arduino to the pi then to the screen. then when finished fold the case up and put it away. If i wished to move the project ones development and testing is complete i could just take the boards out or export the work to a perminat location main problem i can see is how to power it a atx power supply would be able to but then the size would be a issue

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to chrisdracko

    Pcduino V3 Nano is:

    • Small and can run on a battery easily. You will need more power for motors etc.
    • Can program itself. It is a small Linux computer just  better than the Pi.
    • Arduino compatible. The shields will fit like the Uno. You use the same IDE.
    • Oh some pluses, it has a mSata interface for a solid state drive. It also has eMMC for flash to store the Linux system.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to chrisdracko

    Pcduino V3 Nano is:

    • Small and can run on a battery easily. You will need more power for motors etc.
    • Can program itself. It is a small Linux computer just  better than the Pi.
    • Arduino compatible. The shields will fit like the Uno. You use the same IDE.
    • Oh some pluses, it has a mSata interface for a solid state drive. It also has eMMC for flash to store the Linux system.

    Clem