My project Development case idea
Due to limited space this case would be quick to set up as a multi functional development flight case
The case lid will be holding a 7“ vga lcd display this display works on 12v the case lid will also have access to the raspberry pi gpio pins and the arduino gpio pins and have the ability to connect the leds under then with jumper cables there will also be two 20mm speakers available that is connected to the raspberry pi via a small amplifier running about 5v i'm guessing
The bottom of the flight case will have to levels the bottom level will hold the raspberry pi and the arduino as well as a usb hub.
the top level would be interchangeable to allow for expansion like holding a breadboard or led matrix. or relays
Can you help
I want to power the main components with one power supply this will need at least one 12v line as well as three 5v lines able to supply the opriate amps
lcd Supply Voltage: DC 9-35V
Arduino 5v
Raspberry Pi 5v
usb hub 5v