Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Un-grounded protection design
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 341 subscribers
  • Views 1199 views
  • Users 0 members are here
  • surge_protection
  • israel
  • newbie
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Un-grounded protection design

btfarmer94
btfarmer94 over 11 years ago

Hello,

I am currently working on a project where I need to design a simple and effective protection circuit to prevent from voltage spikes and current surges into our product, as well as brown-outs. This particular product will be used overseas where the power plugs are not grounded. My first question is: will a varistor work without a ground if I connect it between line and neutral on 230v @ 50Hz power? My next question is, can anyone provide me with some resources or advice on this type of circuit design? I am studying engineering at school, but have little electrical experience so far and am just starting my career. Thank you all for your assistance!

  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 11 years ago in reply to btfarmer94 +1
    Perhaps a transformer and relay could act as a brown out shut off. Once the voltage drops below a certain level then the relay would drop out. You'd need to match your transformer and relay well (or perhaps…
  • gdstew
    gdstew over 11 years ago in reply to Workshopshed +1
    Another solution is what is called a line stabilizer. Basically it is a 1 to 1 isolation transformer that also senses when the line voltage drops below certain thresholds and uses a relays to kick windings…
Parents
  • Workshopshed
    0 Workshopshed over 11 years ago

    Hi Brandon, sounds like there's several different challenges to overcome there.

     

    A varister for surge suppression does not require a ground so yes you can connect it between live and neutral as described, I've not used one for a while but that's how I think it's normally wired. That should protect from spikes.

    I'm wondering if the best approach for handling brownouts / variable supply voltages is to use a switch mode power supply rather than a linear regulator. If you are not confident in designing your own then you could use an example circuit from one of the chip providers or even buy in a module to attach to your design.

    If your supply is unreliable the other thing you might need to concider is if frequency variations will affect your design.

     

    You should be able to find a lot of useful inform by looking UPS designs

     

    Here's a few links to get you started:

    Protecting the Protector: Adding Circuit Protection to UPSs | Passive Components content from Power Electronics

    An Overview of Power Protection

    Brownout Protector

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • btfarmer94
    0 btfarmer94 over 11 years ago in reply to Workshopshed

    Thanks for the information Andy! And as far as the brownouts go, we would like for our machine to shut off during periods of insufficient power to prevent damage to the machine. In our testing, we found that not enough power would cause damage, and the region in which our product is shipped is notorious for these conditions at sporadic times and of various length. We would like to prevent our customers the hassle of frequent returns and repairs.

     

    Our current board design features minimal components, all passive, to control the device. There is no DC involved. Everything is wall power. Would a "brown out detector" need to use active components? I am not as familiar with these in AC electronics as I am in DC electronics, but I am certain there is a way to achieve this.   

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • btfarmer94
    0 btfarmer94 over 11 years ago in reply to Workshopshed

    Thanks for the information Andy! And as far as the brownouts go, we would like for our machine to shut off during periods of insufficient power to prevent damage to the machine. In our testing, we found that not enough power would cause damage, and the region in which our product is shipped is notorious for these conditions at sporadic times and of various length. We would like to prevent our customers the hassle of frequent returns and repairs.

     

    Our current board design features minimal components, all passive, to control the device. There is no DC involved. Everything is wall power. Would a "brown out detector" need to use active components? I am not as familiar with these in AC electronics as I am in DC electronics, but I am certain there is a way to achieve this.   

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Workshopshed
    0 Workshopshed over 11 years ago in reply to btfarmer94

    Perhaps a transformer and relay could act as a brown out shut off. Once the voltage drops below a certain level then the relay would drop out. You'd need to match your transformer and relay well (or perhaps add a few other components)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to Workshopshed

    Great answers Workshopshed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to Workshopshed

    Another solution is what is called a line stabilizer. Basically it is a 1 to 1 isolation transformer that also senses when the line voltage drops below  certain thresholds

    and uses a relays to kick windings in (or out ?) to change the primary to secondary winding ratio and bring the voltage on the secondary back up. Normally it takes

    takes less than 1/2 cycle (8.33 mS @ 60 Hz) for this to occur so the power supply it is attached to needs to be able to maintain its output for at least this long with

    no AC input voltage.

     

    This is also used in Uninterruptable Power Supplies and is usually called Automatic Voltage Regulation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 11 years ago in reply to gdstew

    Cheers Gary, I saw a reference to line conditioners but did not know how they work