Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need suggestions for a good soldering iron
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 320 subscribers
  • Views 5523 views
  • Users 0 members are here
  • pcb soldering
  • soldering tips
  • soldering
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need suggestions for a good soldering iron

rsjawale24
rsjawale24 over 4 years ago

I'm looking to buy a good soldering iron preferably with a fine needle tip that can last long. Power - 25W-35 W

 

I checked online and there are two types of irons available - Ceramic heater and coil heater type.

 

I use this one from Soldron (A popular brand in India) but the tips don't last longer esp. if you keep the iron on for longer times. The entire soldering bit starts to give off flakes (some kind of coating comes off).

The only plus point is that the tips are easy to replace and not very expensive.

imageimage

I found another one from Stanley the tip is tightened using a screw on the side. Probably uses a different heating element too as compared to the above one.

image

Please suggest good soldering irons to buy (brand, models, etc) which can last longer with power rating of 25W to 35 W. Also, which heating element is better? Coil type or ceramic type?

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 4 years ago +6
    I am not an expert in soldering irons but what I have noticed over the years is that the tips are very damaged if you do not have temperature regulation and some function for the soldering iron to detect…
  • shabaz
    shabaz over 4 years ago +4
    Hi Rushiraj, I think both could be ok for general through-hole work if nothing else is available, but both look pretty bad for surface-mount. This is just from general experience from similar-looking tools…
  • shabaz
    shabaz over 4 years ago in reply to rsjawale24 +3
    Hi Rushiraj, There's a Multicomp soldering station but is just slightly higher than your budget (it is ~ 100 USD). Personally with $70 budget, I think I would try to buy a used soldering station, but that…
Parents
  • shabaz
    shabaz over 4 years ago

    Hi Rushiraj,

     

    I think both could be ok for general through-hole work if nothing else is available, but both look pretty bad for surface-mount. This is just from general experience from similar-looking tools, not those particular tools.

    Are there any other potential candidates/brands that you're considering that are easily available to purchase at a reasonable price?

    As Enrique says, you'll probably want some regulation, if you're using it for electronics design/prototyping purposes, and for helping to prevent the soldering bit from getting damaged.

    With all things aligned (temperature regulation, good practices etc) soldering bits stop being consumables, and can then last 5-10 years or more, for normal prototype work. However at a lower price with no regulation, then as you mention, the bits may need replacing more often, so it's a balance.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 4 years ago

    Hi Rushiraj,

     

    I think both could be ok for general through-hole work if nothing else is available, but both look pretty bad for surface-mount. This is just from general experience from similar-looking tools, not those particular tools.

    Are there any other potential candidates/brands that you're considering that are easily available to purchase at a reasonable price?

    As Enrique says, you'll probably want some regulation, if you're using it for electronics design/prototyping purposes, and for helping to prevent the soldering bit from getting damaged.

    With all things aligned (temperature regulation, good practices etc) soldering bits stop being consumables, and can then last 5-10 years or more, for normal prototype work. However at a lower price with no regulation, then as you mention, the bits may need replacing more often, so it's a balance.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rsjawale24
    rsjawale24 over 4 years ago in reply to shabaz

    Hi Shabaz,

     

    Thanks for the reply. I'm planning to invest in a good soldering iron/station which can be used for normal as well as surface-mount work.

    Could you suggest some brands. My budget is under 70 USD.

    I looked for Weller and Hakko but both of them are expensive. Hakko FX888D which is the basic one, costs about 16k INR approx. 220 USD from E14 website.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to rsjawale24

    Hi Rushiraj,

     

    There's a Multicomp soldering station but is just slightly higher than your budget (it is ~ 100 USD).

    Personally with $70 budget, I think I would try to buy a used soldering station, but that's just luck, if something is available at the right price or not, or wait and purchase the $100 one.. it looks fairly reasonable, and ok choice of bits according to the datasheet. I don't know if it is available in India. In the UK it is out of stock.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 4 years ago in reply to shabaz

    Thanks! The Multicomp one looks good. It's out of stock in India as well.