Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using the experience of the E14 Community to troubleshoot a power supply
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 338 subscribers
  • Views 3519 views
  • Users 0 members are here
  • troubleshooting
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using the experience of the E14 Community to troubleshoot a power supply

colporteur
colporteur over 4 years ago

image

 

The attached schematic if for a wireless doorbell model WL-100A-A. It doesn't have any markings to indicate the manufacture.

 

It has been installed for a number of years and was supposedly working? I recently noticed people have been knocking more than ringing the door bell. I discovered pushing the remote button at the door does nothing. A quick battery change and still nothing. I removed the cover of the unit plugged directly into the wall and discovered that sweat smell of burnt Bakelite.

 

My initial question was "where is the AC step down transformer?" An internet search of transformerless power supply (PS) reveal a number of hits. One immediately caught my attention because of the warnings about mains voltage. This is my first experience with a PS that doesn't use a transformer. After doing some reading it seems to be a common design. I thought it wouldn't pass muster from a safety perspective. The warning of AC mains being potentially exposed on the lower voltage side of the circuit made me stop and take notice.

 

After some napkin drawing and initial troubleshooting I thought maybe someone in the E14 Community has experience and can offer advice.

 

There is no DC voltage. With 120VAC mains applied there is a reading through fuse F1 and nothing any point further. From observation the printed circuit board areas around A, B, C & D are darkened. A resistance measurement of R1 indicates at open. The surface of the component is scorched such that I am assuming its value is the same as R2. R3 & R4 read slightly less than their colour code, no shorts or opens. Diodes D5-D8 appear to test OK. The schematic component type is not correct. I was unable to read the markings and the diode was a fritzing listing. No shorts or opens are measured on the diodes. The same goes for the zener diodes.

 

I don't measure a short across the 12VDC rails. My first thought was to connect a supply at that point to see if the device still works. I'm not sure what took out the front end but based on what they say about currents for this type of PS design it being caused by the load. Then I recalled reading about having no load on this type of supply. Not being familiar with the design and all the warnings I figured I would post to this life line for some advice.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago +7
    I appreciate everyone's responses so I took the time to respond to Fred27 before posting this update. The door bell circuit worked after connecting an external PS. I did short intervals of power on and…
  • Gough Lui
    Gough Lui over 4 years ago +4
    That is a classic capacitive dropper power supply which is non-isolated (so be careful while probing). As long as the casing offers double-insulation and humans aren't touching anything metal, it seems…
  • dougw
    dougw over 4 years ago +4
    You should be able to inject a DC voltage through a current limiting resistor to any point in the circuit to test which components still work. 24V dc through a 10K resistor should work.
Parents
  • colporteur
    colporteur over 4 years ago

    I appreciate everyone's responses so I took the time to respond toFred27 before posting this update.

     

    The door bell circuit worked after connecting an external PS. I did short intervals of power on and off to limit the amount of smoke I generated. When I got confident it was working on left the PS on. IT didn't shutdown but the middle zener diode released a sweat puff of acid smoke at sometime.

     

    I shut the remote PS down quickly and waved away the ghosts rising from the burnt component. Looking at the schematic I got to thinking, what is limiting the current through the zener diodes. Let say my remote power supply is above 12VDC, those working zeners are going to try and clamp the voltage. I think I burnt the zener.

     

    I didn't have the components in the wattage to attempt any repair on the AC power feed circuit. I also didn't want to purchase another bell ring. This one works if it had 12V.

     

    I then rummaged through the parts bin to find a 12VDC wall wart. I removed the prongs poking through the case for the AC plug and threaded the adapter wires through the hole. An exacto knife cut the traces to isolate the zeners and all AC circuit. In the end I was left me with a working door bell that sported a wall wart.

     

    I found another location in the house with a wall plug to hold the wall wart and conveniently tucked the bell ringing housing behind the china cabinet. The door bell worked so damn good I had to put tape over the speaker hole to dampen the ring.

     

    I told my spouse I had to move the door bell. She was happy. I didn't tell her it now sported an adaptor to operate. I just said I moved it behind the china cabinet and left it at that.

     

    FM, reason for effort decided. I have a working door bell once again.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 4 years ago

    I appreciate everyone's responses so I took the time to respond toFred27 before posting this update.

     

    The door bell circuit worked after connecting an external PS. I did short intervals of power on and off to limit the amount of smoke I generated. When I got confident it was working on left the PS on. IT didn't shutdown but the middle zener diode released a sweat puff of acid smoke at sometime.

     

    I shut the remote PS down quickly and waved away the ghosts rising from the burnt component. Looking at the schematic I got to thinking, what is limiting the current through the zener diodes. Let say my remote power supply is above 12VDC, those working zeners are going to try and clamp the voltage. I think I burnt the zener.

     

    I didn't have the components in the wattage to attempt any repair on the AC power feed circuit. I also didn't want to purchase another bell ring. This one works if it had 12V.

     

    I then rummaged through the parts bin to find a 12VDC wall wart. I removed the prongs poking through the case for the AC plug and threaded the adapter wires through the hole. An exacto knife cut the traces to isolate the zeners and all AC circuit. In the end I was left me with a working door bell that sported a wall wart.

     

    I found another location in the house with a wall plug to hold the wall wart and conveniently tucked the bell ringing housing behind the china cabinet. The door bell worked so damn good I had to put tape over the speaker hole to dampen the ring.

     

    I told my spouse I had to move the door bell. She was happy. I didn't tell her it now sported an adaptor to operate. I just said I moved it behind the china cabinet and left it at that.

     

    FM, reason for effort decided. I have a working door bell once again.

    • Cancel
    • Vote Up +7 Vote Down