Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Generator bits & bobs
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 303 subscribers
  • Views 1804 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Generator bits & bobs

GeneratorBlues
GeneratorBlues over 4 years ago

Can someone advise me what specification of diode bridge rectifiers (11.) and diode (42.) I need for for the generator in my camper.  And would appreciate  if you can tell me how the three different windings in the stator can produce different voltage outputs - one  winding produces 12v and the other 230v. The centre winding with capacitor is to excite the field I presume. 

 image

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 4 years ago +1
    GeneratorBlues Bridge Rectifier: https://uk.farnell.com/multicomp/kbpc3504/diode-bridge-rect-1-ph-400v-module/dp/2675360 or similar - most likely. #42 blocking diode... depends on what it looks like…
  • kmikemoo
    0 kmikemoo over 4 years ago

    GeneratorBlues  Bridge Rectifier:  https://uk.farnell.com/multicomp/kbpc3504/diode-bridge-rect-1-ph-400v-module/dp/2675360 or similar - most likely.

    #42 blocking diode... depends on what it looks like.  Could be a simple 1N400x.  https://uk.farnell.com/vishay/gi751-e3-73/diode-standard-6a-100v/dp/9549641 is a 6A diode and it's in stock.  Axial leads.

    Disclaimer: The decision on what components to use is all yours. Neither element14 nor I accept any liability should you chose to use these or a similar item.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • GeneratorBlues
    0 GeneratorBlues over 4 years ago in reply to kmikemoo

    Thanks for the reply.   The diode that needs to be replaced had P600G stamped on it. I asked via live chat and was tod it's out of stock. Can you recommend a similar one that would be suitable.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 4 years ago in reply to GeneratorBlues

    GeneratorBlues  The GI754 looks to be the equivalent - but it is also out of stock.  With that diode being on the 12VDC control side, you could use one with a lower PIV.  400V is... quite robust.  The GI751 is actually in stock.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kkazem
    0 kkazem over 4 years ago

    I'm not sure what you mean by "tell me how the three different windings in the stator can produce different voltage outputs". I'll do my best as a power electronics engineer. The alternator has different isolated windings with differing numbers of turns. The output voltage for each winding is proportional to the number of turns. Therefore, for a 230V vs a 12V output, the turns would be 230/12 =19.166 times (approximately) more turns on the 230V winding than the 12V.  An alternator typically has a three-phase AC output which gets full-wave rectified by a 6-diode, 3-phase diode bridge. But in your case it looks different. I don't see a 3-phase winding. The non-230VAC winding appears to have a tapped output and is used for 12 VDC (after a strange rectification circuit) and for an AC hour meter for the generator. The 230VAC winding is the high-power output for your AC loads and appears to be single phase.

    For DIODE (42), I would agree that a 6A , 100V is probably OK, but I don't really have enough information on it. You might want to to go a 200V PIV diode for that. For the bridge, DIODE BRIDGE (11), I believe the 35A, 400V recommended by kmikemoo is fine (probably overkill, but better safe than sorry).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer