Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Trying to understand serial to parallel circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 32 replies
  • Subscribers 337 subscribers
  • Views 10765 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Trying to understand serial to parallel circuit

opalko
opalko over 4 years ago

Hi again folks (after some time away!),
When I was a teen, I had an Atari 800 computer/ The Atari did not have a parallel port interface.  All they had were the joystick ports, which were serial.  A clever company came up with a serial->parallel port interface.  Me, not knowing much about electronics, could not figure out how they did this.  (PS -I still don't know much about electronics!!!).

Flash forward 40 years and this past week I decided to take apart the serial->parallel interface and reverse engineer this thing! I took apart and there are 2 chips - a 74LS14, and a 74LS164, a resistor and a capacitor. Next step was to draw the schematic, which I did with pencil and paper. This became messy, so I resorted to learning to use KiCad, and came up with the attached drawing. (see attachments)

I get what makes this work is the 74LS164 8 bit parallel-out serial shift register. I still don't really understand how it works though.  As I understand it, the data on this register may be read out in parallel (from all flip-flops) at once.
So some questions!

0) Can someone explain how this whole interface works!?

1) How is the data being read on the printer side?  Is the printer polling every data pin on the parallel port at once regardless of how many are actually being used?

2) Since there are really only 2 address data pins (3 & 5) being used here, it doesn't seem a vast improvement over serial?  But I guess because the Atari only has pins 1-4 for I/O and 1 of those sends the data to the 74LS164?

Thanks for any help understanding this.
Robert Opalko

PS There doesn't seem to be nearly as many members on this forum as there was in the past... Where did everyone go?

image
image
  • Sign in to reply
  • Cancel

Top Replies

  • phoenixcomm
    phoenixcomm over 4 years ago in reply to opalko +4
    try this link: computer.howstuffworks.com/parallel-port1.htm this says that IBM did it but in fact, It was Wang labs. and en.wikipedia.org/.../Centronics
  • phoenixcomm
    phoenixcomm over 4 years ago +4
  • dougw
    dougw over 4 years ago +3
    I don't get it either. A Centronics printer needs 8 data bits and some handshaking to work - this doesn't even have enough pins connected. On a Centronics connector all pins from 19-30 and 33 are ground…
Parents
  • beacon_dave
    0 beacon_dave over 4 years ago
    opalko said:
    0) Can someone explain how this whole interface works!?

    Clocked serial data comes in via the 9-pin Atari interface into the shift register. After input 8 clocks the shift register holds 1 byte of data and the printer is strobed to tell it to look at the 8-bit data in parallel. There are some additional control lines for the computer to reset the printer and for the printer to tell the computer that it is selected and that it is ready to receive more data or not. The cycle repeats, 8bits clocked in, 1 byte clocked out. Some signals are active high and some active low, so logic inverters are used to flip the signal as required.

    The 'magic' pretty much happens in the shift register, so take a look at Karen's video on shift registers (serial in parallel out mode). 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 4 years ago
    opalko said:
    0) Can someone explain how this whole interface works!?

    Clocked serial data comes in via the 9-pin Atari interface into the shift register. After input 8 clocks the shift register holds 1 byte of data and the printer is strobed to tell it to look at the 8-bit data in parallel. There are some additional control lines for the computer to reset the printer and for the printer to tell the computer that it is selected and that it is ready to receive more data or not. The cycle repeats, 8bits clocked in, 1 byte clocked out. Some signals are active high and some active low, so logic inverters are used to flip the signal as required.

    The 'magic' pretty much happens in the shift register, so take a look at Karen's video on shift registers (serial in parallel out mode). 

    • Cancel
    • Vote Up +3 Vote Down