Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help with fuse resistors please to fix a tape deck
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 338 subscribers
  • Views 7875 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help with fuse resistors please to fix a tape deck

raymate
raymate over 4 years ago

Im new to electronics and I have an old cassette tape deck that I was getting going but managed to short something and burnt out a fuse resistor.

Now we are dealing with a tape deck thats 30 years old so no one will fix it in my area so im learning to try and fix it myself.

So I checked continuity and found the resistor that has blown I also saw smoke come from it when I killed it so im pretty sure I just need to replace it.

The service manual says its a " fusible resistor 1.5 5% (1/2W) F " located at R736 but when I look at the resistor on the board it seems to be 2.2 not a 1.5  .....  if I'm reading the resistor right?

This is the help I need, is this dead one on the board 2.2 or 1.5  ,  could it be possible they used 2.2 not a 1.5 as I think its just acting as a fuse. Should I put back what the service manual says or the same as what already in place.

Attached the picture of the resistor thats dead on the board and has no continuity, i ordered online what the service manual says and what I think is the direct replacement for whats still on the board.

So I purchased three resistors types 1.5 and 2.2 (and another 2.2 from a different vendor) also the new ones are so much smaller I guess thats OK things have moved on in 30 years.

So I would like to know have I purchased the right thing. Im just confused as the new ones seems to have arrived with 5 bars.

One I purchased said its a " res 2.2 OHM 5% 1/2W AXIAL " (this is the smaller one in the picture) the other larger ones are generic from ebay.

Thanks for your help, I know this is basic stuff.

imageimage

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 4 years ago +2
    It's possible someone has bodged a 2.2Ohm resistor in there in the past - have you had the cassette deck from new? A fusible resistor should have a white band around it (maybe, see below), like your smaller…
  • raymate
    raymate over 4 years ago in reply to Jan Cumps +2
    One of the motors in the deck is not spinning so I was probing the motor terminals and it did show me 11.5v going to the motor which is correct but for some reason I was checking it again to make sure…
  • Jan Cumps
    Jan Cumps over 4 years ago +1
    Can you post the info from the service manual, and the schematic that shows this component? Did it work before you caused the smoke? What did you do that generated the smoke? What components do you think…
Parents
  • Andrew J
    Andrew J over 4 years ago

    It's possible someone has bodged a 2.2Ohm resistor in there in the past - have you had the cassette deck from new?  A fusible resistor should have a white band around it (maybe, see below), like your smaller middle 4 resistors - the one that's in the board doesn't but maybe there is writing on it that isn't visible?

    Anyway, it's not that basic a question really.  Doing some research, I've come across:

    • A fifth white band is fusible resistor
    • A fifth black band is a fusible resistor
    • A fifth black band could be temp coefficient
    • A fifth white band means wire-wound.
    • And others...

    If the service manual says 1.5 1/2W 5% then if it was mine, that's what I'd be replacing it with (or <5% or >1/2W, view those parameters as maximum and minimum respectively.)  You could try the 2.2 Ohm as I guess it will still work and you have them on hand, but as its job is protection it may be worth shelling out for the correct one.  In either case, I would replace with a known manufacturer with datasheet specifically indicating fusible, not something off eBay (unless that of course.)  You want to minimise any issues relating to dodgy components!

    Let us know how you get on - perhaps create a blog of your testing/diagnosis/progress as it always generates interest and help.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • raymate
    raymate over 4 years ago in reply to Andrew J

    Thank you, leant something new, the fifth band can mean type,, nice. the small one was from digi-key so I assume a OK quality one, the larger ones are ebay specials, so I may get the correct value from digi-key

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • raymate
    raymate over 4 years ago in reply to Andrew J

    Thank you, leant something new, the fifth band can mean type,, nice. the small one was from digi-key so I assume a OK quality one, the larger ones are ebay specials, so I may get the correct value from digi-key