Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Power Mosfets
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 323 subscribers
  • Views 1359 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Power Mosfets

Tonyf
Tonyf over 4 years ago

Hi, I’m new to the forum I’m an electronics engineer and I hope I can contribute to the forum in the future.

at the moment I have a question about mosfets which I know little about.


I have an inverter using 104R5NT Mosfets.

The inverter uses 16 of these Mosfets and 4 of these have exploded. The Inverter still works.

im struggling to find replacements for these Mosfets.

Im wondering whether I could replace the broken ones with a similar, but not the same Mosfet or indeed whether I should replace all of the Mosfets.

Has anyone had a similar problem or better knowledge of mosfets?

Tony

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 4 years ago +1
    Hi Tony, It's hard to be sure without knowing how the circuit used them, but I can't imagine they are matched parts, they seem like low-cost MOSFETs. It could be good to just replace what is blown, and…
  • shabaz
    shabaz over 4 years ago

    Hi Tony,

    It's hard to be sure without knowing how the circuit used them, but I can't imagine they are matched parts, they seem like low-cost MOSFETs. It could be good to just replace what is blown, and see if that works.

    However, it would also be good to (mentally) explore why they got damaged if you have not already done so, e.g. is the load wrong for the use-case that the device is designed for, or is an unusual load being attached while the inverter is running (worth checking the user manual if that is inadvisable or not), or is it running in temperature extremes, and so on. It might not be possible to be sure of the cause of course.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 4 years ago

    I've had problems with large MOSFETs not being able to handle large inrush current, which is typical of inverters. My solution at the time was to use FETs with much higher current ratings. I'm not sure if lower on-resistance is better, since the on-resistance can help limit in-rush current. But with higher resistance, they will get hotter. You might want to measure the FET temperature to see if the heatsinks are adequate.

    • Cancel
    • Vote Up 0 Vote Down