Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Instrumentation Amplifier or Current Sense Amplifier ?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 338 subscribers
  • Views 1510 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Instrumentation Amplifier or Current Sense Amplifier ?

A3JBNE
A3JBNE over 4 years ago

Hello friends, this is my first experience with the design of a precision ammeter for reading. I will use a shunt resistor (60mV/1500A)

I am confused as to the choice, to use an instrumentation amplifier or a current sense amplifier?


I think using the INA190A3 (CSA) has x100 gain, will this be the correct one? I just want to read the amperage very accurately similar to a professional ammeter.


I read that an instrumentation amplifier can do the same task as a current detection amplifier and better, that's why I'm a bit confused about the choice or it doesn't matter?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago +1
    Current sense amplifiers are typically intended to work well in systems where the bulk of the ciruitry is referenced to 0V and the current snese reistor at some positive voltage with respect to it. It…
  • dougw
    0 dougw over 4 years ago

    It probably boils down to cost. You can get an instrumentation amp with zero-drift circuitry for even better performance. You need to look closely at how the instrumentation amp performs when its inputs are at the rails - not all of them will perform well. I would use a CSA unless it couldn't meet accuracy requirements, because I find them simpler and cheaper.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 4 years ago

    Current sense amplifiers are typically intended to work well in systems where the bulk of the ciruitry is referenced to 0V and the current snese reistor at some positive voltage with respect to it. It will often only be able to cope with quite small sense voltages.

    There are many different kinds of device marketed as a current sense amplifier.

    An instrumentation amplifier is more general purpose type of differential amplifier. Some have very large common mode voltage ranges (much greater than supplies) and some have convenient reference ports.

    The INA190 is a nice zero drift current sense amplifier which can cope with the positive common mode voltage of 40V whille running on a 5V supply at a reasonable price. It also semes to be available.

    Without knowing a lot more about your application it's not possible to say if it is a good choice.

    MK