Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Pool boiling experiment
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 317 subscribers
  • Views 4787 views
  • Users 0 members are here
  • resistance
  • pool boiling experiment
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Pool boiling experiment

brunopserrao
brunopserrao over 3 years ago

Dear community,

My research group is developing a pool boiling experiment. It consists basically by a heater (a Stainless Steel wire in our case) placed in a working fluid and a power supply connected to it. In a pool boiling experiment, different bubble regimes are observed depending on the temperature difference between the heater and the working fluid. Our goal is to measure the voltage across the heater in order to calculate the heater resistance and use the temperature x resistance relation to get its temperature.

Our experimental setup consists of a 5000 Watts DC power supply (0-20V and 0-250A) connected to copper wires and then connected to a 316L Stainless Steel wire (this one stays in a water tank).

We have already run this experiment a few times, but we never got a reliable voltage measurement. Our calculated resistance for the heater in general decreases with increasing the power in the power supply, what is not true for two reasons: (1) we can observe the different regimes using a high speed-camera, and (2) increasing power means increasing the heater temperature that means increasing resistance according to the temperature x resistance relation.

In addition, our power supply display is not reliable, so we measure our system current using a clamp digital ammeter. Our voltage across the heater is measured by a 6 1/2 DMM. Can someone help me to understand what we are doing wrong?

Regards,

Bruno

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +1
    The voltage over the heater is the voltage of your power supply - the voltage drop in your copper wires. The more current you send, the more voltage is dropped in the copper leads, and the less voltage…
  • shabaz
    shabaz over 3 years ago +1
    Also, the current measurement may become inaccurate over time* (this is a guess). It might be better to find an alternate way to measure current, e.g. measuring the voltage across the wires, and the voltage…
  • brunopserrao
    brunopserrao over 3 years ago in reply to Jan Cumps +1
    Jan, Thanks for your help. I will be in the lab tomorrow and I can take some pictures of our setup. Basically we have two 8 AWG stranded copper wires connected to the positive and negative sides of the…
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    The voltage over the heater is the voltage of your power supply - the voltage drop in your copper wires. The more current you send, the more voltage is dropped in the copper leads, and the less voltage will be available at your steel wire ends.

    Can you show an example of what you are measuring? A graph maybe of one of the experiments?

    A photo of the measuring points / connections

    The diameter and length of the copper wires

    And if available, how stable the supply voltage is between 0 and 250 A?

    Also put a voltmeter over each of the copper wires. See how much voltage you are losing there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • brunopserrao
    brunopserrao over 3 years ago in reply to Jan Cumps

    Jan,

    Thanks for your help. I will be in the lab tomorrow and I can take some pictures of our setup. Basically we have two 8 AWG stranded copper wires connected to the positive and negative sides of the power supply. I welded two copper clamps (designed for 100A) on the other extremities to make the connection with our heater easier and more reliable).

    We also developed a structure to make our heating element more stable. It consists of a stainless steel squared base connected to two stainless steel squared pillars. On each pillar, a teflon squared bar is attached and then a copper bar is attached on the teflon. Teflon was implemented for insulation purposes between the copper squared bar and the stainless steel structure. The heating element is placed between the copper bar and the teflon bar connecting the two sides of the structure. I'm gonna send you a picture of this structure tomorrow as well.

    Let's call the above described structure as test section. So, we attached a small length of the 8 AWG stranded copper wires to the test section to make it easier to connect with the clamps (those connected to the power supply as described in the first paragraph).

    That was actually our initial approach which included so many connections in our system. Like I said, we did not get good measurements.

    In a second approach, we tried to make a straight connection between the test section and the power supply. However, our measurements were still not good.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • brunopserrao
    brunopserrao over 3 years ago in reply to Jan Cumps

    Jan,

    Thanks for your help. I will be in the lab tomorrow and I can take some pictures of our setup. Basically we have two 8 AWG stranded copper wires connected to the positive and negative sides of the power supply. I welded two copper clamps (designed for 100A) on the other extremities to make the connection with our heater easier and more reliable).

    We also developed a structure to make our heating element more stable. It consists of a stainless steel squared base connected to two stainless steel squared pillars. On each pillar, a teflon squared bar is attached and then a copper bar is attached on the teflon. Teflon was implemented for insulation purposes between the copper squared bar and the stainless steel structure. The heating element is placed between the copper bar and the teflon bar connecting the two sides of the structure. I'm gonna send you a picture of this structure tomorrow as well.

    Let's call the above described structure as test section. So, we attached a small length of the 8 AWG stranded copper wires to the test section to make it easier to connect with the clamps (those connected to the power supply as described in the first paragraph).

    That was actually our initial approach which included so many connections in our system. Like I said, we did not get good measurements.

    In a second approach, we tried to make a straight connection between the test section and the power supply. However, our measurements were still not good.