Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum RFID race timing solutions
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 333 subscribers
  • Views 5232 views
  • Users 0 members are here
  • help
  • rfid
  • timing
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

RFID race timing solutions

daveob1
daveob1 over 4 years ago

I was just reading an older thread about making a RFID timer for a running race. It sounds like the technology hasn't changed that much in 7 years, but has anyone else done something similar?

My main issue (I think) is the start/finish set up. We are going to do small MTB races in the bush with the start/finish spaced about 3kms apart. Mobile reception is poor. So is there a workaround to get their staggered start time for a rider then get their finish time. We could do a workaround of set start times, but it would be easier with the tags.

It maybe as simple as loading both sets of data into a laptop program, but I haven't look at that side yet.

There are commercial solutions available but for our club its a cost issue.

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 4 years ago in reply to shabaz +2
    The dog racing application is an interesting example. I was wondered if BLE tags or beacons could be used, by checking ble signal strength (rssi) with possibly direction analytics (if using BLE 5.2 tags…
  • shabaz
    shabaz over 4 years ago in reply to BigG +2
    BLE would be a neat way to augment photocell. I guess antenna tech is still a way behind to provide accuracy on it's own. I've not seen the BLE location solution in action yet, but from other AoA based…
  • shabaz
    shabaz over 4 years ago +1
    Hi, I'm not sure it would be easier with tags. While there are tags that can be read from a distance, they don't provide accurate positioning, so some sort of break-beam type of barrier might also then…
Parents
  • shabaz
    0 shabaz over 4 years ago

    Hi,

    I'm not sure it would be easier with tags. While there are tags that can be read from a distance, they don't provide accurate positioning, so some sort of break-beam type of barrier might also then be needed (I don't know if that's needed for a 3 km race or not).  Failure to read a tag might be quite likely, especially if the runner is going fast - the long-range tags are designed to be on products, not humans.

    Personally I think the easiest solution would be video based, perhaps an app on the mobile phones of race assistants. As a person starts or stops the race, they could be identified on the video at the start or stop time, and then the times could be collected up, since the phone will be aware of the time that the video was captured. The race assistant would merely need to go to the position in the video capture where a contestant has started or finished, and tap to select the contestant name, and let the app handle the rest. It sounds like a nice opportunity for someone to write an app for a mobile phone basically, and perhaps a cloud app for uploading the data once there is mobile coverage. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 4 years ago in reply to shabaz

    I seem to recall start / finish line mat antennas being used for this sort of thing. Something like this perhaps:

    https://www.youtube.com/watch?v=MnkCDdUjP5w

    Looks like these folks have a how to guide on DIY race timing systems which may be of interest:

    https://www.atlasrfidstore.com/rfid-insider/build-your-own-rfid-race-timing-system

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to beacon_dave

    Hi Dave, good videos. They're definitely the right sort of tags, I've worked with a solution with them on products, for reading at a distance (can even be read from 10 feet away or more, depending on the antenna, and on the tag shape/size), but the system would take several seconds to read them - although that could partially have been be the back-end doing the processing, rather than the RFID reading portion.  

    Interesting how they suggest wearing two tags, just in case one fails to be read. I'm still not sure how accurate it is; perhaps for long distance races it is sufficient for determining the approximate time, and then the precision comes from video footage maybe.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 4 years ago in reply to beacon_dave

    Hi Dave, good videos. They're definitely the right sort of tags, I've worked with a solution with them on products, for reading at a distance (can even be read from 10 feet away or more, depending on the antenna, and on the tag shape/size), but the system would take several seconds to read them - although that could partially have been be the back-end doing the processing, rather than the RFID reading portion.  

    Interesting how they suggest wearing two tags, just in case one fails to be read. I'm still not sure how accurate it is; perhaps for long distance races it is sufficient for determining the approximate time, and then the precision comes from video footage maybe.