Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum MOSFETs in linear operation
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 33 replies
  • Answers 1 answer
  • Subscribers 338 subscribers
  • Views 10991 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

MOSFETs in linear operation

ben0127
ben0127 over 3 years ago

Hi,

Im new here, first post, and am a fairly junior engineer so could do with some help regarding a charging circuit. I am designing a mosfet based current control circuit with a P-channel (needs to be high-side) and am having problems with the mosfet destroying itself. I have done some research into the use of mosfets in the linear region so I believe I am biasing it correctly and not putting much strain on it, keeping Vds low etc,  but when trying the circuit out it works for about 10 seconds before a wisp of smoke and charming aroma fills the lab. I have tried several different mosfets now and had the same problem with each of them, all setup to work comfortably within specs. 

After some more research I came across "Power Mosfets" which sounded like the answer to my problems, several articles I read talked about how standard mosfets cannot dissipate the heat being generated but power mosfets can. I started looking at the datasheets of some of these to select some samples but each one I looked at had the same issue which, with the knowledge I have so far, has ruled them out. The ZTC point on the transfer characteristics graph was very high.

My understanding of the operation of mosfets is that they need to be biased on (Vgs) above the ZTC point so that they are thermally stable. This is one of the key properties I have looked for in datasheets, along with the SOA, but what Im seeing with power mosfets is, for example, a ZTC point at 20A with a realistically useful maximum current of around 20A. This is of no use to me as there is no range. The standard mosfets have a much lower ZTC point so can be used to regulate current over a significant range which is what Im looking for. 

Im starting to doubt some of the things Ive learned about these devices and so definitely need some help with some questions:

Ive got used to thinking that I can only use mosfets above the ZTC point but these power mosfets look like using them below it would be necessary. Im wondering if it is safe to do so, as long as you have a feedback system to back off the current as it warms up?? If this is the case, is it safe to use at Vgs extending all the way down to the Vgs threshold? 

During research another confusing piece of info I came across, which completely contradicts what I had come to understand about power mosfets, was that they can fail in operation above the ZTC point even when within the SOA. I thought the whole point of a "power mosfet" was that it could handle operating in linear mode? Isnt this what differentiates it from a standard mosfet?

Im starting to wonder what it is Im missing with this as it seemed relatively simple to begin with so any help or advise on any of these points would be greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago in reply to michaelkellett +5
    I had to look up ZTC as well. Michael is making some useful points here: before blowing any more MOSFETs or spending money on buying more to blow in a similar manner, you should do a bit of research on…
  • dougw
    dougw over 3 years ago +3
    Have you calculated the maximum power that needs to be dissipated in your transistor? Are you familiar with how to calculate the amount of heat sinking you need based on the power levels? If you have amps…
  • michaelkellett
    michaelkellett over 3 years ago +3
    To make helpful comments we need more information. A schematic (with component types and values) and some pictures would be a good start. A specification always helps. Mostly power MOSFETs are not…
  • ben0127
    0 ben0127 over 3 years ago in reply to Andrew J

    Thanks thats really helpful. Absolutely, I wont be blowing any more components up unless I make some other mistake. I will do the calculations needed to make this work. The price isnt really prohibitive at the moment so not concerned about that.

    As you say, getting the approach right and then scaling up is what I had in mind. I want to know that fundamentally it works, then I will see how far I can take it. If in the end I can only manage 10A max, thats ok, at this point anyway. 

    As several very helpful folks here have asked for some details on circuitry (understandably!) I will put something up but Im afraid I wont be able to do that until monday now so please bare with me. In all honesty I have been rather shy, I dont do social media so posting anything let alone ideas or designs is quite daunting. The circuit I have is very simple but its purely my own design/idea and I half expected to be pelted with rotten tomatoes by any experienced engineers looking at it. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • javagoza
    0 javagoza over 3 years ago in reply to ben0127

    You're welcome. I have learned a lot with your question, the element14 community is great, always willing to help those of us who are just starting out.

    From the element14 Participation Guidelines and Code of Conduct

    "The element14 Community is intended to be a safe and inclusive space, free from violence, harassment, hate speech or exclusionary behaviour."

    "

    • Don’t judge – instead share your knowledge! Knowledge is not a competition – instead of judging people for what they don’t know (or seemingly haven't google searched for), help them. Elitism is not welcome, even unintended. Remember that different people have different approaches and may have valid reasons for why they're asking.
      • Similarly 'back handed' assistance which criticizes the person asking and then provides the answer requested is also not tolerated and can be seen as a form of emotional abuse.

    "

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 3 years ago in reply to ben0127

    What Javagoza says: you'll find that Element14 isn't like other sites and you won't get any grief at all for asking questions or posting things up.  You'll get as much help as you ask for, given politely and with encouragement.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 3 years ago in reply to ben0127

    Hopefully the comments here don't sound like flames - that is not a motive on this site. Many of us have similar stories to yours. Shy about publishing ideas and not into social media. I also burned my finger on my first linear power supply design. What we learn from these experiences is more valuable than the components we smoke.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ben0127
    0 ben0127 over 3 years ago in reply to ben0127

    Morning folks,

    This is my circuit, essentially a battery charger but the point is that the charge rate is fully controlled. The supply will be a DC-DC with some level of output control for the purpose of reducing voltage across the mosfet. There will be other circuitry in there as well for detection of faults etc but the main design is shown. The 1.3k resistor is several in series to handle the power, this is to drop most of the remaining voltage (protecting the 2N7000) as the supply is around 50V (for 48V battery). This drive circuit still needs work but the focus for now is on the main mosfet.

    Im thinking about maybe using this as a module which can be paralleled to get more current, the mosfets could be individually monitored that way rather than just assuming that each mosfet is taking the same current as the others.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ben0127
    0 ben0127 over 3 years ago in reply to jc2048

    Hi, yes it needs to be linear as opposed to PWM to protect the battery. Thanks anyway.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to ben0127

    First thought, you have a feedback loop where you are sensing the current with theresistor and  INA282, measuring the signal with the processsor ADC, working out the feedback required, driving the processor DAC and then controlling the 2N7000 via a filter with a 20ms time constant.

    I was going to say that this is a very bad way to do it, but I'll settle for observing that it is a very unusual way.

    The feedback loop will alwas be very slow because the micro's ADC and DAC conversion are inside it. This means that if you short the output the MOSFET will alwas blow !

    A much neater way to do it is use an anlogue voltage feedback loop and control the reference voltage with the processor.

    I'm suspicious of the 48V charge voltage - real '48V'  batteries charge between roughly 40 and 52V (lead acid) and maybe 35 - 54V (lithium ion). The range can be bigger than this.

    So I think your PSU will need to provide maybe 56V and deliver full charge current with the load at 40V.

    There a a million and one different ways of doing this.

    You can buy controller chips that manage a switching power supply (eg LTC 4000) but I think you might find this very hard to work with.

    It's much easier to use low side current sensing, but there is a disadvanatage that your controller 0V and the batteries load 0V are not the same.

    You don't need such a low gate source resistor on the MOSFET so you can reduce the power in the level shifter.

    This type of design work is vastly facilitated by using a ciruit simulator.

    I suggest that you donwload LTSPice from www.analog.com. It's free and very widely used.

    I've thrown together (very quickly) a simple all discrete part, linbear regulator. This is nowhere near a final circuit but it might help you get started.

    V2 and V4 between them are the control input or reference.

    Q1 and Q2 make a diff amp which compares a proportion of the output with the reference and adjustes the drive to M1 via the emitter follower Q3.

    V3 and R1  represent the battery.

    R3 senses the battery current (not used at the moment, this is waht your micr can measure and decide how to tweak the drive voltage to adjust the charge current.

    It's easy to add hardware current limit with an NPN transistor driven by the voltage drop on R3, but there are other better ways.

    If you get this design into LTSpice and spend soem time playing both with the tool and the circuit you'll get a much better idea of where you are going.

    But you really need to pin down the spec:

    range of input volts, range of output volts, max current, max voltage before battery explosion, must it stand shorts to ground as well as across the battery, operating temperature range, accuracy of current and voltage measurement and must the battery 0V be a system common rail , to name just a few things you need to know.

    image

    MK

    .

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 3 years ago in reply to ben0127

    For a one off prototype, I would just use the classic op-amp servo'd current source only in a high-side topology such as:

    image

    Source: https://www.ti.com/lit/an/slaa867/slaa867.pdf

    OP-amp A1 can be powered off 5 V (or similar).

    OP-Amp A2 would need a supply referenced to the Vin. The can be done with a simple shunt regulator, such as a zener diode or a TL431. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ben0127
    0 ben0127 over 3 years ago in reply to michaelkellett

    First of all I would like to say thankyou for putting what must have been a very significant amount of time into your reply, with constructive criticism, alternate ideas and an entire circuit design. Unfortunately, reading through the points made there seems to be quite a lot of misunderstanding of the circuit. This may well be my fault for not explaining everything but I was attempting to not draw attention to things that at the moment are not the focus.

    The thread was really about making sure I was not misusing or abusing the main mosfet with my circuitry, although I dont want to sound ungrateful for the opinions and advice on the whole circuit. 

    I would like to go through some of the points just to clear things up:

    The feedback - this was never meant to replicate a classic closed loop control system, it would be useless in that respect, it was just basic feedback to nudge the gate drive if and when it needs it. That probably sounds ridiculous but its not so much that I think its a good way of doing feedback in the conventional sense, although its perfectly adequate for this purpose, but more that I like the idea of the micro being involved, it knows how hard its driving the gate etc.  The 20ms filter you mentioned is there to remove the switching of the 2N7000 drive signal. I use PWM from the micro as I get a much better resolution than that offered by the DAC. As mentioned in the post I am still working on the drive circuitry as it has other issues. 

    If the output goes short the system will not rely on the feedback system, the battery voltage will be seen as 0V (or extremely low) and the mosfet will be switched off, assuming that the battery PCM doesnt get there first and disconnect the battery. 

    Regarding the battery voltage I mentioned (48V) I can see where this caused confusion and slightly regret mentioning it, but it wasnt meant to draw attention to itself. Just for clarity the battery is Lithium with a range of 33.6V to 50.4V. 

    Low side current sensing, indeed low side anything, causes problems which are unacceptable in this system. Ground must be ground.

    The gate-source resistor on the main mosfet is as low as it is for improved resolution. Controlling the main mosfet over a wide range of charge current and with accuracy isnt easy and as I mentioned earlier its still being improved.

    LTspice is great and Ive used it quite a bit but it doesnt tell you that your mosfets going to blow up :)

    Youve gone to a lot of trouble designing a circuit which is above and beyond, thankyou. Even if I dont change my approach it shows me more established methods which are good tools to keep in the box. My circuit was not intended to be a reinvention of the wheel, Im part of an innovation centre which is investigating new smarter charging methods.

    My initial reason for reaching out with this thread was that the mosfets kept blowing but the thermal issues causing the problem are understood now so thats sorted out.  Thanks to you and all others that have replied for your help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to ben0127

    Thanks for explaining where you are with this.

    I think you will always have trouble using power MOSFETs in linear mode without an analogue feedback loop to control them, the problem with controlling the gate precisely is that the relationship between gate source voltage and drain source current is not well defined.

    Most of the modern power MOSFET specs seem to be concerned with switching them hard on or off.

    Good luck with your project, perhaps you can post some more about it as it progresses.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>