Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum MOSFETs in linear operation
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 33 replies
  • Answers 1 answer
  • Subscribers 338 subscribers
  • Views 11014 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

MOSFETs in linear operation

ben0127
ben0127 over 3 years ago

Hi,

Im new here, first post, and am a fairly junior engineer so could do with some help regarding a charging circuit. I am designing a mosfet based current control circuit with a P-channel (needs to be high-side) and am having problems with the mosfet destroying itself. I have done some research into the use of mosfets in the linear region so I believe I am biasing it correctly and not putting much strain on it, keeping Vds low etc,  but when trying the circuit out it works for about 10 seconds before a wisp of smoke and charming aroma fills the lab. I have tried several different mosfets now and had the same problem with each of them, all setup to work comfortably within specs. 

After some more research I came across "Power Mosfets" which sounded like the answer to my problems, several articles I read talked about how standard mosfets cannot dissipate the heat being generated but power mosfets can. I started looking at the datasheets of some of these to select some samples but each one I looked at had the same issue which, with the knowledge I have so far, has ruled them out. The ZTC point on the transfer characteristics graph was very high.

My understanding of the operation of mosfets is that they need to be biased on (Vgs) above the ZTC point so that they are thermally stable. This is one of the key properties I have looked for in datasheets, along with the SOA, but what Im seeing with power mosfets is, for example, a ZTC point at 20A with a realistically useful maximum current of around 20A. This is of no use to me as there is no range. The standard mosfets have a much lower ZTC point so can be used to regulate current over a significant range which is what Im looking for. 

Im starting to doubt some of the things Ive learned about these devices and so definitely need some help with some questions:

Ive got used to thinking that I can only use mosfets above the ZTC point but these power mosfets look like using them below it would be necessary. Im wondering if it is safe to do so, as long as you have a feedback system to back off the current as it warms up?? If this is the case, is it safe to use at Vgs extending all the way down to the Vgs threshold? 

During research another confusing piece of info I came across, which completely contradicts what I had come to understand about power mosfets, was that they can fail in operation above the ZTC point even when within the SOA. I thought the whole point of a "power mosfet" was that it could handle operating in linear mode? Isnt this what differentiates it from a standard mosfet?

Im starting to wonder what it is Im missing with this as it seemed relatively simple to begin with so any help or advise on any of these points would be greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago in reply to michaelkellett +5
    I had to look up ZTC as well. Michael is making some useful points here: before blowing any more MOSFETs or spending money on buying more to blow in a similar manner, you should do a bit of research on…
  • dougw
    dougw over 3 years ago +3
    Have you calculated the maximum power that needs to be dissipated in your transistor? Are you familiar with how to calculate the amount of heat sinking you need based on the power levels? If you have amps…
  • michaelkellett
    michaelkellett over 3 years ago +3
    To make helpful comments we need more information. A schematic (with component types and values) and some pictures would be a good start. A specification always helps. Mostly power MOSFETs are not…
  • ben0127
    0 ben0127 over 3 years ago in reply to michaelkellett

    Ive been thinking about what you said regarding linear mode without analogue feedback as Ive been able to do some testing with mosfets over the last day or two. All is running smoothly now with good heatsinking so Ive been able to see my feedback solution in operation and it seems to be working very nicely but I cant help being slightly nervous, considering your comment.

    Its really crude but seemed like it might be good enough considering that the mosfet doesnt need a closed loop control system to operate (as opposed to an SMPS chip for example). Essentially the current value is read by the ADC and a simple algorithm adjusts the duty cycle to maintain the desired current. 

    It seems to work exactly as expected with a significant reduction in duty cycle initially as the mosfet warms up, then it settles and stays put. My tests include mosfet temperature so I can see the heating tracking with the algorithm adjustments, which presumably is down to the gate threshold reducing with heat as its operation is below the ZTC point. 

    Once everything settled down (within about 5 minutes) and was left for another 10 minutes or so I tested the feedback by putting my fingers over the drive mosfet (cooling it). The result was as expected, the duty cycle started increasing quickly to compensate but the current held nicely. When I let go the opposite happened and it returned. 

    Im really interested to know what you think, it seems to work great but am I fooling myself? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to ben0127

    When everything is about right I would expect it to work OK as you describe. Might be worth checking that the currrent isn't fluctuating which might be an indication of instability. If you wind up the gain enough in your control loop you will be able to make it unstable.

    My main worries would be the slow response to serious fault conditions.

    (It is possible that this doesn't matter in your application.)

    I would normally include a software bug as a fault condition to be protected against.

    Since failures in chargers for big Lion batteries have such serious consequences (don't trust the internal protection - that's just insurance) I would like to see processor independent over voltage and over current protection.

    Overcurrents will happen when some fault shorts the output to ground, on a good day this blow the MOSFET open circuit, on a bad day it will blow it short circuit and the large current into the battery may pull the supply down a bit leaving you in a very bad position.

    The other overcurrent that can happen is when the processor (during development) decides to set maximum possible current (PWM output sticks high).

    I'm a bit busy right now but I may be able to get back to this tomorrow morning. Let me know if you need some tips re. how to limit the MOSFET current.

    For thermal protection I would glue some electro-mechnical thermal switches to the battery.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ben0127
    0 ben0127 over 3 years ago in reply to michaelkellett

    Thanks for that, no rush to come back if you think of anything else, whenever you have time. 

    Fault conditions will be dealt with later on, the feedback is only to hold the current stable. Good points made though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<