Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Jetson NANO power problem!!!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 338 subscribers
  • Views 6479 views
  • Users 0 members are here
  • jetsonNANO'
  • problem
  • switch mode regulator
  • plz help
  • boost converter
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Jetson NANO power problem!!!

Chuitoto
Chuitoto over 3 years ago

Hi! we are doing a project need to power up jetson NANO with a 5V 3A capable pwoer bank. Since our Jetson NANO board needs 12V, we add a boost converter in our design.
the logic flow is like this:

PowerBank 5V  ->  5Vin boost converter 12Vout  ->  12V jetson NANO

The problem is when we run some code on Jetson NANO, it's shut down unexpectedly...

We checked the V and I in both path (both PowerBank to Boost && Boost to Jetson) and we found out that the power loss is really high, it hit 50% loss

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

here is the schematic of our boost converter, are we doing something wrong? 

any suggested solution for this ?? 

image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +2
    Hi, You may have fried it. Jetson nano uses 5V, it doesn't use 12V.
  • colporteur
    colporteur over 3 years ago in reply to shabaz +1
    If S is correct then toast you might be. Ouch! I have yet to encounter a micro USB connector using a 12VDC supply.
Parents
  • shabaz
    0 shabaz over 3 years ago

    Hi,

    You may have fried it. Jetson nano uses 5V, it doesn't use 12V. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Chuitoto
    0 Chuitoto over 3 years ago in reply to shabaz

    Hi shabaz! thnk you for your reply! However, our board is not the standard NVIDIA jetson NANO dev kit. this board is made by 3-party company. So thats why I said using 12V to power it up. 

    and the problem right now is when the currect increase, the efficiency of my boost converter decrease as shown at the video. how thats going to happended...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Chuitoto

    You could check your boost converter using a resistor or resistors in parallel, and measure the voltage, to see if the circuit can actually deliver the load or not. The video does not help, it doesn't show anything much. The IC you're using only supports up to 2A max, whereas the Jetson Nano uses more than that if there are peripherals which there may well be on the third party board. The circuit may be badly laid out or the inductor may not support the load. I have no idea because there is so little information.

    In any case, I think you need to reconsider this project, and simply power it from a 12V source (e.g. 12V battery pack) instead of trying to build a high current capable boost converter from 5V to 12V. There are even camera batteries which are 7.2V or so which would have been a better choice than a 5V source. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago in reply to Chuitoto

    You could check your boost converter using a resistor or resistors in parallel, and measure the voltage, to see if the circuit can actually deliver the load or not. The video does not help, it doesn't show anything much. The IC you're using only supports up to 2A max, whereas the Jetson Nano uses more than that if there are peripherals which there may well be on the third party board. The circuit may be badly laid out or the inductor may not support the load. I have no idea because there is so little information.

    In any case, I think you need to reconsider this project, and simply power it from a 12V source (e.g. 12V battery pack) instead of trying to build a high current capable boost converter from 5V to 12V. There are even camera batteries which are 7.2V or so which would have been a better choice than a 5V source.