Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum My Vacuum Cleaner Motor Doesn't Work. Could the Battery Management Circuit be the Cause?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 315 subscribers
  • Views 2333 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

My Vacuum Cleaner Motor Doesn't Work. Could the Battery Management Circuit be the Cause?

jsg
jsg over 3 years ago

Hello,

I am new in this forum. First of all, I would like send greetings to everybody. I am not a native English person, so I apologize if something is not right written or expressed.

Here is my question:

I have a portable vacuum cleaner that works with a batery that contains 2 cells 18650 Li-on, 2.200 mha each, 7.4V total voltage with BMS included. The device has worked well for some months, but now, when I switch on it (after checking the battery is fully charged) the motor starts turning for less than one second and stops. If I repeat the operation, the result is the same. Seems the BMS is cutting the current to the motor. I checked the connections and dissasembled the motor, cleaned it, but the result is the same. I connected the motor directly to the battery (previously dissassemble the bms) and it works perfect.

I would ask to the community if somebody has experienced this kind of problem and what could be the root cause and, if is possible, what could be the potential solution.

The device data is:

-Portable Vacuum cleaner

-Battery: 2 cells 18650 Li-on, 2.200 mha each, 7.4V serie connected with BMS 20A included

-Total power: 120W

-Power AC adapter (for charging battrty): 8.4V, 1A

 

Thank you in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago in reply to Jan Cumps +1
    OK. That shoots that first trouble shooting sequence to crap. I'll sit on the bench now.
Parents
  • colporteur
    0 colporteur over 3 years ago

    Welcome. Please, don't concern yourself with mastering English. It is native to my tongue and I am still not very good at it.

    I rolled around you information in my mind and have some questions. My assumption is BMS is AC mains? I'm thinking BMS is an acroymn for building mains supply?

    Before failure confirm the vacuum operated on battery only and AC (with battery)? Would it operate without a battery installed. This may not be something that was checked. Operate, meaning it could be used as a vacuum.

    Now the vacuum operates on battery only and fails on AC(with battery)?

    After operating the vacuum on battery only. The battery can be recharged if plugged into AC. Any attempts to operate the vacuum with AC results in failure.

    Will the vacuum operate without batteries installed? Just running on AC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to colporteur

    I think that BMS is battery management system - the circuit that protects the battery, manages right charging profile, prevents overload and overcharge, ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to Jan Cumps

    OK. That shoots that first trouble shooting sequence to crap. I'll sit on the bench now.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 3 years ago in reply to Jan Cumps

    OK. That shoots that first trouble shooting sequence to crap. I'll sit on the bench now.