Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Make: Electronics (2nd edition) experiment 9 - capacitive coupling
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 302 subscribers
  • Views 3506 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Make: Electronics (2nd edition) experiment 9 - capacitive coupling

minimaltom
minimaltom over 3 years ago

Hi, im having a small problem with the -  part of the chapter, that is experiment 9 and the 2nd edition. In figure 2-85 and 2-86 there is an LED and a 470 ohm resistor added beneath the 10k resistor. Why have the 10k resistor in this circuit at all? Won't the capacitor charge itself fine through the 470 resistor? You don't need to measure the time the capacitor charges in this experiment and if you did wouldn't the 470 resistor alter the time it took to charge?

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago +3
    [Not posting an image of the circuit because it's copyright] The answer is in the text: when the capacitor is discharged (initial state), and you press button A, current will flow through the capacitor…
  • rsjawale24
    rsjawale24 over 3 years ago in reply to minimaltom +2
    As Andrew mentioned the copyright issue, you may delete the picture or post a hand drawn image of the circuit. Also, Andrew gave a good explanation of the working of the above circuit. There are two…
  • Andrew J
    Andrew J over 3 years ago in reply to minimaltom +2
    You could test this by removing the 10k resistor and see what happens. There has to be a certain amount of voltage for a diode to conduct so if that voltage doesn’t appear on the diode, the capacitor can…
Parents
  • Andrew J
    Andrew J over 3 years ago

    [Not posting an image of the circuit because it's copyright]

    The answer is in the text:

    • when the capacitor is discharged (initial state), and you press button A, current will flow through the capacitor, charging it, and through the 10K resistor, and the LED and 470 resistor in parallel with the 10K resistor.  If the LED did not have the 470 resistor in series then the current through it may well blow it.  The 470 is really in the circuit to protect the LED and has a coincidental small role to play in charging the capacitor - but that isn't its real purpose in this experiment.
    • Once the capacitor is charged the LED will turn off because the capacitor will not pass DC current: the current's only path is via button B which is open thus nothing flows.
    • In order to see the LED flash, the speed of charging the capacitor has to be slowed down.  This is achieved with the 10K resistor in series with it.  If you tried a small value resistor here, you may well not see the LED flash at all; conversely, trying a larger resistor you may see the LED light for longer.
    • The 470 and 10K resistor are in parallel with each other so, yes it does somewhat impact the charging rate, and that rate can be calculated by determining the actual resistance (you should be able to calculate total resistance from resistors in parallel by this stage) and thus the time constant. 

    What he's teaching you here is that even with DC, a capacitor will allow some current through whilst it is charging; what he's reinforcing though is that you should always current limit your LEDs to stop blowing them.  Note that when he moves on to replace the LED with the DMM, that 470 resistor isn't needed.

    If you have plenty of LEDs to hand you could experiment to try and make it blow: remove the 470 resistor and see what happens; try substituting larger capacitors.  I expect at some time you'll see it flash and then no more.

    Don't forget to discharge that capacitor using button B before removing it from the circuit!  Especially if you try larger ones.

    Hope that helps but feel free to ask more questions.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • minimaltom
    minimaltom over 3 years ago in reply to Andrew J

    Are the bullet points yours or from the book? I can't find that written anywhere in it.

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to minimaltom

    They are mine - just trying to rephrase what is written there to explain it in a different way.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • minimaltom
    minimaltom over 3 years ago in reply to Andrew J

    thanks, that's very helpful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • minimaltom
    minimaltom over 3 years ago in reply to Andrew J

    thanks, that's very helpful