Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Remote Control of MP730027 Digital Multimeter
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 339 subscribers
  • Views 3004 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Remote Control of MP730027 Digital Multimeter

peter
peter over 3 years ago

I recently bought the Multicomp Pro MP730027 benchtop Digital Multimeter and am having difficulty controlling the instrument using the USB or LAN interface and the DMMEasyControl software which came with the instrument. After launching the app and clicking Control > Connect, the program hangs for about ten seconds and then closes. I have tried it with both USB and LAN interfaces and the same thing happens. It has never, as far as I recall, worked with the USB interface, but occasionally, in the early days with the LAN interface.
I have not (for various reasons) tried to use remote control for a month or more. Two things since then which may/may not be significant are 1. I recently upgraded to Windows 11. 2. I bought a RS Pro programmable power supply which uses a similar app (EasyPower) and both instruments are seen by Device Manager as 'USB Test and Measurement Device (IVI). I can control the RS Pro power supply via USB, but not via LAN. Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +2
    It is a problem with low cost programmable instruments that the suplliers often do not provide easily accesible and adequate information to use them. It can also be a problem with high cost instruments…
  • KennyMillar
    KennyMillar over 3 years ago +2
    Pretty certain that model is compatible with the Owon desktop multimeter, they have some software downloads at: www.owon.com.hk/.../index.asp
  • baldengineer
    baldengineer over 3 years ago +2
    I have the MP730028, which has the same backend. On mine, LAN never connects. The UI shows the cable is connected, but the lights never flash. I have tried with different cables and have verified the cables…
Parents
  • michaelkellett
    0 michaelkellett over 3 years ago

    It is a problem with low cost programmable instruments that the suplliers often do not provide easily accesible and adequate information to use them. It can also be a problem with high cost instruments but that is unusual.

    If you want to use the supplied software I'm not able to help you. If you bought the meter from Farnell Or Newark then contact customer support or the tech help who will at least be able to get you any documentation that exists. They may know if there is a WIndows 11 problem.

    If you want to programme the meter by SCPI commands over LAN you will almost certainly be able to do so but it will involve a lot of internet trawling and some hard work. The meter will probably communicate using TCP/IP and you will need its port number. With some instruments I have had to write code to probe every possible port to find which one it uses.

    If you are using this for work then I would recomend cutting your losses and getting a big name meter (possibly second hand) where all this stuff is documented and the wide user base means you can get help. I have had no problems getting HP/Agilent/Keysight, Keithley or even Rigol DMMs to talk. (I haven't tried any other makes)

    Obviously it's a bit late for this, but I would suggest that if you can't access adequate information before you buy the instrument , then its best to look elsewhere. (this doesn't apply to the software that came with it - you are reasonbly entilted to expect that to work !).

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 3 years ago

    It is a problem with low cost programmable instruments that the suplliers often do not provide easily accesible and adequate information to use them. It can also be a problem with high cost instruments but that is unusual.

    If you want to use the supplied software I'm not able to help you. If you bought the meter from Farnell Or Newark then contact customer support or the tech help who will at least be able to get you any documentation that exists. They may know if there is a WIndows 11 problem.

    If you want to programme the meter by SCPI commands over LAN you will almost certainly be able to do so but it will involve a lot of internet trawling and some hard work. The meter will probably communicate using TCP/IP and you will need its port number. With some instruments I have had to write code to probe every possible port to find which one it uses.

    If you are using this for work then I would recomend cutting your losses and getting a big name meter (possibly second hand) where all this stuff is documented and the wide user base means you can get help. I have had no problems getting HP/Agilent/Keysight, Keithley or even Rigol DMMs to talk. (I haven't tried any other makes)

    Obviously it's a bit late for this, but I would suggest that if you can't access adequate information before you buy the instrument , then its best to look elsewhere. (this doesn't apply to the software that came with it - you are reasonbly entilted to expect that to work !).

    MK