Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Reverse protection of Multicomp pro DC/DC converters MP-K78xx?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 338 subscribers
  • Views 2740 views
  • Users 0 members are here
  • DC/DC Converter
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Reverse protection of Multicomp pro DC/DC converters MP-K78xx?

DavidOB
DavidOB over 3 years ago

Hi,

I'm unable to find rating and description of MP-K78xx DC/DC converters in respect to reverse current/voltage protection. I have some questions:

1. What happens if another voltage source is connected to the output if this converter is not powered and used with typical application circuitry with input/output 10/22uF ceramics capacitors?

2. Same question as 1. but what if the converter is powered?

3. Same question as 1. but what if the converter input is shorted to ground?

3. What would happen if that another source voltage is higher than the converter nominal output? E.g. MP-K7803-500R3 is used for a battery powered device and USB + is connected to the output power rail while connected with a PC. If USB cable is connected, its 5V would then go into this 3.3V K7803 output.

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago +3
    Good questions and you're right to research them. LM78xx (and LM79xx) don't like reverse current so I always provide diode protection in case there is any over voltage/current problem downstream. I've…
  • scottiebabe
    scottiebabe over 3 years ago in reply to Andrew J +2
    I saw the cross-section of one of those last night:
  • Andrew J
    Andrew J over 3 years ago in reply to shabaz +1
    Are there USB connectors that have an Earth switch in them like DC Barrel Jacks - when a USB cable is plugged in it disconnects an Earth turning an alternate power source off?
Parents
  • shabaz
    0 shabaz over 3 years ago

    Hi,

    There is a partial answer that is relevant, in the datasheet:

    4. Converter cannot be used for hot swap and with output in parallel;

    Even with any alternative (more expensive) product that is more fully specified, it's unlikely to allow multiple sources to be connected together in this way. Usually some 'OR' circuit is needed, perhaps with diodes, or MOSFETs. In your example, perhaps the USB source could be connected to the input of the DC-DC converter instead (via a Schottky diode). It might be slightly out-of-spec since USB power isn't exactly 5.0V, and may even go out of spec with different loads too, but maybe such a cut-down method is acceptable for some applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago

    Hi,

    There is a partial answer that is relevant, in the datasheet:

    4. Converter cannot be used for hot swap and with output in parallel;

    Even with any alternative (more expensive) product that is more fully specified, it's unlikely to allow multiple sources to be connected together in this way. Usually some 'OR' circuit is needed, perhaps with diodes, or MOSFETs. In your example, perhaps the USB source could be connected to the input of the DC-DC converter instead (via a Schottky diode). It might be slightly out-of-spec since USB power isn't exactly 5.0V, and may even go out of spec with different loads too, but maybe such a cut-down method is acceptable for some applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Andrew J
    0 Andrew J over 3 years ago in reply to shabaz

    Are there USB connectors that have an Earth switch in them like DC Barrel Jacks - when a USB cable is plugged in it disconnects an Earth turning an alternate power source off?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Andrew J

    Hi Andrew,

    Neat idea! I've not seen one, but if it exists, it would be a useful part. I once used a normal switch (microswitch) positioned such that the user couldn't physically insert the USB connector, without pushing the microswitch lever down first. Since 3D printers are so popular, maybe a sliding door for a USB connector and switch could be designed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 3 years ago in reply to shabaz

    I suppose there are alternate physical approaches: need to make sure that the alternate power source becomes un-powered.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DavidOB
    0 DavidOB over 3 years ago in reply to Andrew J

    I doubt using such nice-but-unheard-of USB connector would be practically useful for transparent power source switching as activating that mechanical switch would not be timely and instant enough to both prevent the two sources be active at the same time and therefore collide and at the same time not to cause power drop because of time gap between one source gets disconnected to the other getting connected. Or?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 3 years ago in reply to DavidOB

    They aren't designed for instantaneous power changeover, no.  They would disconnect the Earth before connecting the power so they wouldn't both be active at the same time but there would be a time where nothing was powered.  Basically, your approach should be what Shabaz and I have mentioned - you may also need to consider common grounding as well.