Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Best way to disconnect a SOIC-8 pin?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 337 subscribers
  • Views 7855 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Best way to disconnect a SOIC-8 pin?

Andrew J
Andrew J over 3 years ago

I've accidentally connected a pin to GND and it should have been left unconnected.  It's pin 5 of an 8-pin SOIC so reasonably accessible but what would be the best way to actually disconnect it without stressing other pins?  Note that the track that connects it to GND is very short and actually under the IC so isn't accessible.  I don't really want to de-solder the chip so all I can think of is to try and wick up the solder from that pad and then gently bend the pin up.  I've found that trying to wick it up is quite difficult because there's always some that remains under the pin.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +6
    Go big! lol
  • baldengineer
    baldengineer over 3 years ago +4 verified
    I would heat up the pin, lift it, and then wick any solder left making a connection. In fact, you may find adding some solder first helps to make lifting it easier.
  • michaelkellett
    michaelkellett over 3 years ago +3
    I would cut the pin, I do have a nice pair of rather expensive micro cutters for this purpose. Works well on SOIC, less good on 0.5mm pitch pins. You can (with care) use a scalpel with a nice new blade…
Parents
  • michaelkellett
    0 michaelkellett over 3 years ago

    I would cut the pin, I do have a nice pair of rather expensive micro cutters for this purpose. Works well on SOIC, less good on 0.5mm pitch pins.

    You can (with care) use a scalpel with a nice new blade. Then clean up with fine tip iron and flux. I've removed 144 pin TQFPs like this. It takes a while and you have to saw away patiently for a long time but I must have done a couple of dozen of them in the last few years and I haven't lost  a pad yet. Trying to save a £1000+ board helps one to keep focused.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 3 years ago

    I would cut the pin, I do have a nice pair of rather expensive micro cutters for this purpose. Works well on SOIC, less good on 0.5mm pitch pins.

    You can (with care) use a scalpel with a nice new blade. Then clean up with fine tip iron and flux. I've removed 144 pin TQFPs like this. It takes a while and you have to saw away patiently for a long time but I must have done a couple of dozen of them in the last few years and I haven't lost  a pad yet. Trying to save a £1000+ board helps one to keep focused.

    MK

    • Cancel
    • Vote Up +3 Vote Down