Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help with PL Ethernet with SFP module in UltraZed
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 327 subscribers
  • Views 219 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help with PL Ethernet with SFP module in UltraZed

daniel.santamaria
daniel.santamaria over 3 years ago

Hello,

I am trying to use the SFP+ interface of the UltraZedEV card to echo IP traffic (with PL Ethernet).

In my design with Vivado, I use the "GTH-10GBASE-R" IP core.

I have a problem with the "GT reference clock", since in the AVNET card the GTH clocks that can be used DO NOT have a frequency that is valid for the IP core "GTH-10GBASE-R", according to the "UltraScale FPGAs Transceivers Wizard (1.7)" of Vivado.

That is, the AVNET card has the following GTH clocks: 148.5MHz (GTH_REFCLK[0] for HDMI and GTH_REFCLK[5] for Aux) and 250MHz (GTH_REFCLK[2]-SDI). In addition, external clocks to the Carrier could be used, but I have no possibility of having them. These external clocks would be from the SMA interface (GTH_REFCLK[3] and GTH_REFCLK[7]) and from the FMC (GTH_REFCLK[4] and GTH_REFCLK[6]). The GTH_REFCLK[1] would remain, which is from the HDMI_RX.

Of these previous clocks, you would only be able to use the 148.5MHz and 250MHz ones, which are not valid in the core IP "GTH-10GBASE-R", according to the "UltraScale FPGAs Transceivers Wizard (1.7)" of Vivado.

I need to find a reference clock that works for the core IP "GTH-10GBASE-R"...

Somebody could help me?

Can anyone think of any other possibility to use the SFP interface on the UltraZedEV card?

Thank you for helping!