Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Motor's of the electrical kind
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 337 subscribers
  • Views 3175 views
  • Users 0 members are here
  • research
  • power supply
  • new_member_introduction
  • electronics
  • motor
  • newbie
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Motor's of the electrical kind

Tallboyshort
Tallboyshort over 3 years ago

All right everybody, my name is Eric Penny you can call me tall boy short. I like to say thank you for adding me to this community rather having me in this community.

I am looking to ask a question about electric motors today what electric motor can have full power, lose its source power, regain that source power and regain full RPM without slowing down to a stop? 

For instance like a bathroom fan you can turn on and off the switch multiple times and the motor will stay relatively at full RPM. But other motors that have capacitance starts and electrical stops do not allow for this to happen.

  • Is there something I can change in the capacitance or the electrical stops to make it like a fan blower.
  • Sign in to reply
  • Cancel

Top Replies

  • robogary
    robogary over 3 years ago +3
    Motors encompass a very large realm. I'm guessing you arent interested in dc motors, synchronous motors, 3 phase motors , etc, just ordinary 1 phase induction motors? The reason a blower keeps spinning…
  • colporteur
    colporteur over 3 years ago +2
    I will ask some questions to better understand your requirements. You are looking for information on a motor configuration that has an inconsistent input power source or you are looking to control a…
  • dougw
    dougw over 3 years ago +1
    I don't have experience with the various start systems for single phase motors, but dredging my memory I would think they all would continue running when power is re-applied (if they are still rotating…
Parents
  • colporteur
    colporteur over 3 years ago

    I will ask some questions to better understand your requirements.

    You are looking for information on a motor configuration that has an inconsistent input power source or you are looking to control a motor by modulating the input power source such as pulse width modulation (PWM)?

    Describe the motor configuration. Input parameters, load parameters and what the motor is driving?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Tallboyshort
    Tallboyshort over 3 years ago in reply to colporteur

    An inconsistent power supply let's just say the grid drops in and drops out a lot but the motor needs to stay running even if it is only dropping in and out for a few seconds. The motor that I have currently When the power is disengaged something inside the motor clicks and it uses the electricity from back EMF to slow itself down and this is what I wished to bypass safely of course.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Tallboyshort

    Motor theory is quite complex (at least, it is to me, it seemed to come easy for Tesla etc), but as far as I'm aware, it won't be back-EMF that is slowing the motor once any remaining magnetic field has collapsed after the grid has dropped out (which is a function of the windings), so I can't see what could be altered to make the motor continue to 'coast' longer than it currently is spinning for, which as you say isn't currently long enough for the switch to remain disengaged.
    However, if the motor is powerful enough, perhaps a flywheel could be added, to store energy, allowing the motor to continue spinning for longer even when the power is temporarily removed. It likely can't be retrofitted if the motor is sized for no flywheel, and it could cause other problems, could even be dangerous.

    What is the actual scenario/use-case? Perhaps there is a different solution (e.g. different motor would allow you to have a backup supply from a battery, etc).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to Tallboyshort

    The clicking noise you are likely hearing is the centrifugal switch on the cap winding dropping out.

    The desired behavior is not a function of the motor, but the motor feeder. 

    One way to do what you want is to have the shore power feed an inverter. The inverter drives the motor. The inverter would need a big capacitor or a battery bank on its dc link to provide the motor power while the ac feeder is switched. The feature is called power dip ride thru, but sounds like you want a beefier version for power loss ride thru. It's not a cheap solution, but can be done. 

    Miracles can be engineered given infinite time and money :-) 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 3 years ago in reply to Tallboyshort

    The clicking noise you are likely hearing is the centrifugal switch on the cap winding dropping out.

    The desired behavior is not a function of the motor, but the motor feeder. 

    One way to do what you want is to have the shore power feed an inverter. The inverter drives the motor. The inverter would need a big capacitor or a battery bank on its dc link to provide the motor power while the ac feeder is switched. The feature is called power dip ride thru, but sounds like you want a beefier version for power loss ride thru. It's not a cheap solution, but can be done. 

    Miracles can be engineered given infinite time and money :-)