Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Choosing an Oscilloscope or logic analyzer
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 338 subscribers
  • Views 4165 views
  • Users 0 members are here
  • help
  • experts
  • ask_an_expert
  • oscilloscope
  • electronics
  • ask_the_expert
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Choosing an Oscilloscope or logic analyzer

amrrahmy
amrrahmy over 3 years ago

Thanks in advance,

I am familiar with basic multimeters or avo-meters.

I wanted to know what kind of features and speeds, digital or digital and analogue, or which Oscilloscope to get for,

- reading slow-ish serial communication, UART, I2C, SPI, weigand output, at normal micro controller speeds (9600, 19200, 115200), and 3.3v, 5v, and 12v mostly

- no analogue voltage or ADC or sound, but mainly digital communication

I would like to "capture" or set "triggers" for messages coming from a device, maybe transfer it to usb drive or pc, optionally, view it as hex or ascii in Oscilloscope.

Optionally,

- reading output from HDMI 2.1 (48Gbps in bandwidth) or latest display port

- reading output from USBC with alt display port, like between PS5 and PSVR2

From what i have seen advertised, 1-2 channel, 100-200mhz,

  • Real-time sampling rate up to 1 gsa/use
  • IRecord length up to 14 Mpts

How does that equate to bitrate? can something with these specs capture hdmi signal at 48Gbps? would i need more channels for HDMI and USB C with display port?

do i need an adapter to clip onto tiny connectors like usb c and hdmi? a breakout accessory of sorts?

Update:

I was looking to get information about "regular" oscilloscopes in the range of $500-2K.

I see that logic analyzers(for slower speeds) in combination of something like wireshark for usb related packet capturing/monitoring might work better, as an affordable oscilloscope would only work for up to 100Mbps or 200Mbps.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +4 verified
    You don't mention your budget but you won't get a scope capable of direct connection to HDMI (the 4.9Gbit part) under $50k. You'll need 16GHz scope bandwidth and matching differential probes. Unlesss…
  • Gough Lui
    Gough Lui over 3 years ago +1 verified
    Scopes capable of HDMI 2.1 or even USB 3.0+ are extremely expensive. You'll be looking well above $50k. Even then, for what you want to do, you probably can't afford the precision cables and test fixtures…
  • Gough Lui
    Gough Lui over 3 years ago in reply to Gough Lui +1 verified
    If you're still interested, there are not many USB 3.2-capable oscilloscopes - these would be something like: Keysight Infiniium UXR0164A R&S RTP164B Tektronix MSO / DPO70000 Plus whatever…
Parents
  • michaelkellett
    +1 michaelkellett over 3 years ago

    You don't mention your budget but you won't get a scope capable of direct connection to HDMI (the 4.9Gbit part) under $50k. You'll need 16GHz scope bandwidth and matching differential probes.

    Unlesss you are doing something very odd you would be better off with an HDMI analyser but it won't be cheap.

    USBC at ultra speed  - same applies.

    For the low speed stuff I'd suggest a Picoscope - you get lots of decoders in the basic price and the scope parts work well. You'll need 4 channels and/or one with a logic analyser.

    You might get away with a logic analyser  - I can recomend the ones from ZeroPlus which I own and use. There are others. It can be very difficult to debug serial prootocols without a real scope - signal integrity problems are common and the best an analyser can do is tell you that there is a problem - it won't help you work out what it is.

    All the major scope manufacturers offer mixed signal scopes with protocol decoders at various prices.

    If you budget is very tight then go for a logic analyser using open source software (Sigrok) and a cheap scope if you end up needing it.

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    +1 michaelkellett over 3 years ago

    You don't mention your budget but you won't get a scope capable of direct connection to HDMI (the 4.9Gbit part) under $50k. You'll need 16GHz scope bandwidth and matching differential probes.

    Unlesss you are doing something very odd you would be better off with an HDMI analyser but it won't be cheap.

    USBC at ultra speed  - same applies.

    For the low speed stuff I'd suggest a Picoscope - you get lots of decoders in the basic price and the scope parts work well. You'll need 4 channels and/or one with a logic analyser.

    You might get away with a logic analyser  - I can recomend the ones from ZeroPlus which I own and use. There are others. It can be very difficult to debug serial prootocols without a real scope - signal integrity problems are common and the best an analyser can do is tell you that there is a problem - it won't help you work out what it is.

    All the major scope manufacturers offer mixed signal scopes with protocol decoders at various prices.

    If you budget is very tight then go for a logic analyser using open source software (Sigrok) and a cheap scope if you end up needing it.

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • amrrahmy
    0 amrrahmy over 3 years ago in reply to michaelkellett

    ok, so, the oscilloscopes that costs $500-2K are for slow speed communication, something with logic analyzer will have multiple wires/channels.

    for usb I can potentially use wireshark if there are no drivers in windows or linux, and that might work for usb 3/3.2/usb with display port/usb with lightning, doesn't matter?

    I assume if i use libusb (usb protocol)  or libusbk, which i used before for usb 2.0 devices, which is old, without device drivers, I might still be able to make a program to capture data over usb 3.2 with display port or usb with lightning?