Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Unstable driving voltage for 4 haptic by DRV2605 and mux??
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 336 subscribers
  • Views 3446 views
  • Users 0 members are here
  • esp32
  • haptic
  • i2c
  • mux
  • DRV2605
  • virabtor
  • arduino
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Unstable driving voltage for 4 haptic by DRV2605 and mux??

Chuitoto
Chuitoto over 3 years ago

Hi element 14! I am designing a Device which needs four vibrator to perform some haptic patten! I use four DRV2605 to drive one vibrator, and a multiplexer to control each DRV2605 through I2C! the main MCU I am using is ESP32. 

Unfortunately, when all vribrators vribrate at the same time, one of the haptic motor vibrate solfer than other three. and I dont know why...

I tested the voltage of that weak one, it cant rich 0.8V, which other virator can achieve.

Those are powered by RT9013 has max. 500mA should be enough.

here is the schematic and PCB design, which i think have no problem....

 imageimage

what is the reason behind this ???

Did anyone have the same expriance of this scenario? Welcome to comment if you are facing mux current/voltage problem. I wanna learn more as well! 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +3
    Not sure a maximum of 500mA in is enough - current loads for motors and drivers can be peaky and so it's the peak current you need to worry about, rather than the average. Use a scope or DMM to measure…
  • BigG
    BigG over 3 years ago +2
    I recall looking at Seeed Studio's use of DRV2605 and they used an inductor to handle inrush current etc. I tried something similar with this hack for a single vibrating motor attached to a BBC::microbit…
  • dougw
    dougw over 3 years ago in reply to Chuitoto +1
    Check the trace widths on power and ground to each driver - maybe the traces are too thin to supply enough current without a voltage drop. This could starve one of the drivers. Does the voltage at the…
  • Chuitoto
    Chuitoto over 3 years ago

    I mean four DRV2605 to drive four vibrators separately! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • charlieo21
    charlieo21 over 3 years ago

    My first thought is that the vibrator that can't achieve 0.8V has a higher resistance than the other ones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 3 years ago

    I recall looking at Seeed Studio's use of DRV2605 and they used an inductor to handle inrush current etc.

    I tried something similar with this hack for a single vibrating motor attached to a BBC::microbit (you probably don't need to use all the caps shown):

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to Chuitoto

    Check the trace widths on power and ground to each driver - maybe the traces are too thin to supply enough current without a voltage drop. This could starve one of the drivers. Does the voltage at the driver in question decrease when other drivers are active?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago

    Not sure a maximum of 500mA in is enough - current loads for motors and drivers can be peaky and so it's the peak current you need to worry about, rather than the average.

    Use a scope or DMM to measure the input voltage at each chip and the output waveform. If the waveform is unstable, a DMM may not give you an accurate result!

    - Gough

    • Cancel
    • Vote Up +3 Vote Down