Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How do I repair our Polder thermometer display?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 337 subscribers
  • Views 6145 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How do I repair our Polder thermometer display?

hafcanadian
hafcanadian over 3 years ago

The display on our Polder thermometer loses most of its crystals.  I thought I could open it up and just wipe its “zebra” contacts, but they seem to be taped over and not subject to contamination.  Plus, the crystals respond if I press on the sandwiched glass sheets.  Do I try separating the sheets to inspect contact points, or is this repair not worth attempting?

imageimage

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +3
    It's unlikely to be a problem with the LCD glass sandwich and it's more likely a failure of the LCD self-adhesive ribbon which is stuck down with adhesive in this type of assembly. The only way you can…
  • dougw
    dougw over 3 years ago +2
    Have you tried pressing right on the zebra connector area? Your first instinct was likely correct - poor contact on some of the zebra contacts. It is tough to keep uniform pressure all the way along a…
  • beacon_dave
    beacon_dave over 3 years ago +2
    I recall something similar cropping up on the community forum a while back. You can get anisotropic conductive film tape: https://www.3m.co.uk/3M/en_GB/p/d/v000073742/ if you can manage to separate…
  • dougw
    dougw over 3 years ago

    Have you tried pressing right on the zebra connector area? Your first instinct was likely correct - poor contact on some of the zebra contacts. It is tough to keep uniform pressure all the way along a long zerba connector. In some plastic cases you can put a shim to keep more pressure on some area that is not making good contact.

    I don't think it is possible to successfully re-assemble the liquid crystal sandwich if you take it apart. I would try contact cleaner on the connections or some way of applying pressure.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago

    It's unlikely to be a problem with the LCD glass sandwich and it's more likely a failure of the LCD self-adhesive ribbon which is stuck down with adhesive in this type of assembly.

    The only way you can remedy this is to use a brand-new self-adhesive ribbon film and get a perfect alignment, squeegeeing the film down as you go. They're fiddly in my experience with constructing this kit which uses a similar type of connection: https://goughlui.com/2016/10/15/project-cd2003gpsc3610d-fm-receiver-wlcd-alarm-clock-74-108mhz/

    Not sure where one can purchase such film though .. so if carefully pressing down on the joint doesn't restore the display for long, then there's not much one can really do. In a pinch, you could try doing something mildly mechanical (e.g. use a bulldog clip and some paper to distribute a clamping force across the contact area) as a kludge.

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago

    I recall something similar cropping up on the community forum a while back.

    You can get anisotropic conductive film tape: 

    https://www.3m.co.uk/3M/en_GB/p/d/v000073742/

    if you can manage to separate and clean up the existing connection which usually requires a bit of heat eg:

    "Bonds made with 3MTm Anisotropic Condustive Film Adhesive 7303 are repairable
    by heating the bond-line to above 100°C (e.g. with a hot plate or rework tool) and
    peeling the circuits apart. The bond site then requires cleaning with a solvent, after
    which the circuit can be re-bonded using a fresh piece of ACF 7303. Solvents such
    as 3MTm NovecTm Engineered Fluid HFE-72DA or Acetone may be used."

    There was a tutorial showing someone doing this type of repair, which might be worth a search for. 

    You probably want to practise a few times on another disposable device first though as it looks a bit tricky.

    Adafruit do 'Z axis' anisotropic tape in smaller quantities:

    https://www.adafruit.com/product/1656

    I also recall there being flexible splices available with the anisotropic tape pre-attached either end, which allow you to re-terminate the ribbon if the end is damaged.    

    You can also get T-bar tips for soldering irons that help with such repairs:

    https://www.amazon.co.uk/CITALL-Soldering-T-iron-Ribbon-Repair/dp/B07BBMD8DW

    in which case a quick reheat followed by some pressure might do the trick, or alternatively help with removal without damage ready for clean-up and new tape.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 3 years ago

    This is a common problem with these displays.

    They almost always degrade with time.

    The connections corrode and contact is lost, either in the connector or the device itself.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to beacon_dave

    BD I had to go get the dictionary "anisotropic conductive film tape" where do you get this stuff. Awesome!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to colporteur

    I keep it filed next to the elastomeric connectors, which are then collectively filed under 'weird stuff'...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • hafcanadian
    hafcanadian over 3 years ago in reply to beacon_dave

    As you noted, there are videos.  Not all are particularly useful or well-made.  But this one I am going to try as it seems, as its poster alludes at its end, it is worth a try... in my case, yup.  He demos regular "zebra strip" repair at first, then at about the 7 minute mark talks about just what I need to try:

    https://www.youtube.com/watch?v=-QZk9WCz-D8&t=3s

    Just out of learning experience benefit, if that relatively simple attempt doesn't work, I might get some of your referenced tape and try replacing the old stuff, but the videos about that I've seen look very time-consuming and require delicacy my essential tremor may not facilitate.  Heck, just holding the soldering iron in place for trying the above linked method may be tricky enough for me.

    Thanks to all for your valuable input.  That thermometer isn't the only display issue clogging my workbench.  My 2 year-old Ninja coffeemaker has a crystal problem and was a *** to remove from the machine.  I suspect its problem is related to so-called "Zener" diodes on one of its two boards, but the display works on a different principal than zebra or tape;  its integral and pins to solder points directly on the board, eliminating finicky strip or tape connections. Sounds great, except it failed anyway, thus the suspicion is thrown on board components.

    But that's another story, one I think I told here last year.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to hafcanadian
    hafcanadian said:
    Heck, just holding the soldering iron in place for trying the above linked method may be tricky enough for me.

    The T-bar tip mentioned previously might help you out there if you can clamp things into place. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago

    I have had problems of this sort before. solution. Toss It into the bin.  It is a major pain, in the tush, to remove cleanly and then reapply it. In the factory, this is done with a jig, which you don't have. I hate to be the naysayer but toss it in the bin. Instead, build a new one, that is Arduino powered.

    Good Luck.