Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Flow sensor integration with the Car electronics system
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 326 subscribers
  • Views 2476 views
  • Users 0 members are here
  • flow sensor
  • car
  • car dashboard
  • electronics
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Flow sensor integration with the Car electronics system

boodle
boodle over 3 years ago

I need to integrate a Fuel flow sensor mentioned here to the car dashboard system, so as to display the flow readings on the dashboard screen and/or to a seperate display screen when fuel passes through the sensor .
I'm specifically using this device which has a Working Voltage: DC 5V~18V. 
 
Please suggest to explain what options are available & how this can be done electronically with the different car systems models?
  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago in reply to boodle +2
    I suggest you do some research, especially if you think Arduinos and DIY is expensive. How cheap do you think you'll be able to find an off-the-shelf product that meets all your needs? I work with these…
  • dougw
    dougw over 3 years ago +1
    You can obtain a simple Hall effect sensor tachometer display anywhere. If you need the display to read out in liters per minute instead of pulses per minute, you will need a smarter display.
  • beacon_dave
    beacon_dave over 3 years ago in reply to boodle +1
    Given that car dashboards can vary quite a bit, then you may find it easier to start off with a separate display. There was an example of using a similar water flow sensor with an Arduino here: https…
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    On some 'return flow' injection systems, you may need a second sensor so as you can subtract the return flow in order to get the actual fuel being used by the engine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • boodle
    boodle over 3 years ago in reply to beacon_dave

    This device is to address short-fueling.(Yes, short-fuelling is a problem in many countries).
    Not connecting with fuel pipe but fit around the tank's fuel cap so that when the vehicle is refueled, it notifies the actual volume filled in the vehicle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to boodle

    Well, that's probably not an ideal sensor for this application. They're often no more accurate than +/- 10% depending on the flow rate.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to boodle

    Well, that's probably not an ideal sensor for this application. They're often no more accurate than +/- 10% depending on the flow rate.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data