Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Best sensors for measuring fuel flow rate in vehicles
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 337 subscribers
  • Views 11422 views
  • Users 0 members are here
  • flow sensor
  • sensors
  • turbineflow
  • learning center
  • electronics
  • Hallaffect
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Best sensors for measuring fuel flow rate in vehicles

boodle
boodle over 3 years ago

We are looking for a sensor that can be fitted on the Cars fueltanks & help in determining the fuel pumped into the vehicle. A display or meter reader along with the sensor isn't the need. Just a sensor would work.  So, a simple low-priced device with good accuracy is the need. Are turbine flow (Hall affect) the only sensors that will fit this need or other sensors available to measure it?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago in reply to boodle +3
    I answered you a while ago in your other thread (it's a bit confusing when you have two on the same topic.) You probably won't like my answer any better: A flow sensor capable of giving accurate measurements…
  • phoenixcomm
    phoenixcomm over 3 years ago +2
    The best method for measuring fuel is a capacitive system. This is the same system that is used on aircraft. You need a minimum of two cap sensors, one is in the bottom of the tank and is used for calibration…
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to phoenixcomm +2
    BTW with the above solution you know the volume of your tank at a standard temperature. So the math is not that big of a deal. also, this will give you a fuel rate over time. and in airplanes, you have…
Parents
  • dougw
    dougw over 3 years ago

    There are many ways to measure flow rate. Accurate flow rate measurement may require a positive displacement flow sensor, but they aren't usually cheap. Flow can be measured at the fuel injectors as well. Usually you can just tap into the OBD2 system to extract fuel data, because every car these days has fuel measurement already implemented. It is unlikely that a low-cost external measurement system will perform better. There also questions about safety that affect the answer. More information about your application is needed to give a better answer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • boodle
    boodle over 3 years ago in reply to dougw


    1) This device is to address short-fueling.(Yes, short-fuelling is a problem in many countries).
    Not connecting with fuel pipe but fit around the tank's fuel cap so that when the vehicle is refueled, it notifies the actual volume amount going in the vehicle.

    2) This is not the best sensor but to start with but can be used with fuels. e.g. similar plastic sensors for diesel. www.amazon.in/.../B093ZNNY84 . Planning to move to other sensors as we progress. If you know any better compact, cost efective,accurate sensors that can do the job, please do share.

    3) Which is the simple, compact, cost effecient way to get refueling volume displayed to the users? On a seperate device or on a app or send a notification on SMS/Whatsapp? Please help share more in detail on devices available for each option & how it can be achieved?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to boodle
    boodle said:
    Can using it with Temperature/density sensors help giving more accurate levels?

    Likely not ... the reason purely boils down to the design of the sensor which is a windmill vane sitting in the flow. At certain rates, flow will just flow past the mill because the casing cannot be made to match very closely otherwise it could get stuck or wear out. This is the price of cheap sensors and why such sensors aren't used in actual practice where you want an accurate value of total amount as that is the time-integral of flow.

    There are calorimetric flow sensors but they're not all that much more accurate either and need to be calibrated to the heat-flow properties of the fluid. Those often run $200+ for the sensor, but it has no moving parts, so the accuracy shouldn't drift over time as much as these mechanical sensors.

    Calibration of fuel pumps as required by government where I am require the use of a "reference standard measure" - i.e. a cylinder of known calibrated volume. Notice they don't measure using a "flow sensor" because what you really care about is volume, not flow rate.

    boodle said:
    No one really wants to put the efforts to weigh the can each time refuelling :) 

    Then just buy cans of a fixed size, fill them from empty to full. I mean, these are cheap and safe options which require no major work ... nor electricity, nor complex moving parts.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • boodle
    boodle over 3 years ago in reply to shabaz

    I like your negativity & not thinking from the resolution perspective. Some time it bois down to personality!

    • Cancel
    • Vote Up -1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to boodle

    I answered you a while ago in your other thread (it's a bit confusing when you have two on the same topic.)

    You probably won't like my answer any better:

    A flow sensor capable of giving accurate measurements of the amounf of fuel pumped into a motor vehicle during re-fueling would have to be the same bore as the existing fuel filler and be installed properly in line with it. This would have to meet stringent regulatory requirements for safetey (especially in petrol powered vehicles). seperate approval would be needed for every vehicle type.

    I don't know of an off the shelf flow sensor that would work as the core of the design.

    I can't see the cost being less than a few hundred pounds/dollars per vehicle even if the product were made in reasonable numbers.

    What it boils down to is that your problem (checking amount of fuel delivered into a vehicle) can't reasonably be addressed with a flow sensor of any known type.

    This means that you will need to step back and look at other solutions to the problem, or invent a completely new kind of flow sensor.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • boodle
    boodle over 3 years ago in reply to michaelkellett

    michaelkellett  Thanks, your inputs are valuable. Agree & we are trying to figure out the complexity & cost-efficiency towards the resolution which is why reached out to this learned community for the inputs   

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to shabaz

    I'm guessing that the idea is that you would take something like this:

    https://www.amazon.in/MagiDeal-Gasoline-Delivery-Dispenser-Electronic/dp/B07JRFSPVD/ref=sr_1_10

    which already has that flow meter built into a trigger nozzle, then somehow stick the pump delivery nozzle snuggly into the back of that in such a way it forms a perfect seal and pumps the fuel at a steady rate through the meter and then into a normal petrol tank receptacle.

    However, there normally is a venturi tube in the pump delivery nozzle, which would have to be routed separately to the end of the nozzle with the flow meter in order for the delivery nozzle to open its dispensing valve. The position and size of this venturi tube probably varies widely from nozzle to nozzle.

    You then have to scale that down in such a way that the scammer doesn't notice it attached to the car and request that you remove it before they will deliver fuel and scam you.

    In theory you could insert the flow meter into the filler pipe out of view with a remote display but that would then require modifying a wide range of vehicle types and probably void any warranty / insurance in the process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • boodle
    boodle over 3 years ago in reply to beacon_dave

    @beacon_dave 

    Thanks, your inputs are valuable. Accuracy +-1% is what I'm aiming.  To start with, I agree, I'm using low cost flow rate sensor but how true it is that the overall Turbine flow rate sensors have accuracy of more than +-5% as claimed by many above. If so, how come devices like this or this are commercially viable? All i'm trying to do is make the product cheaper & for end users which makes it a buyable product rather than fitting it in the trigger nozzle. 

    What is the purpose of venturi tube. Is it to measure flow or just to maintain a steady rate?If it is just to maintain the steady rate, then e.g. 'A device like a fuel tank cap which measures and displys the readings of fuel volume pumped'. The fuel getting flown from the nozzle with the venturi tube to this device is already flowing at a steady rate, so why we would need it?  

    I didn't understand the point why it needs to be hidden from the scammer? The fuel pumps have the liability to give what is paid & all this device is going to do is to give an assurance that there is no short-changed. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • boodle
    boodle over 3 years ago in reply to Gough Lui

    @Gough, Accuracy +-1% is what I'm aiming.  To start with, I agree, I'm using low cost flow rate sensor but how true it is that the overall Turbine flow rate sensors have accuracy of more than +-10% as claimed by many above. If so, how come devices like this or this are commercially viable? All i'm trying to do is make the product cheaper & for end users which makes it a buyable product rather than fitting it in the trigger nozzle. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to boodle

    The original water flow meter you linked to appeared to have an accuracy of +/-3% and as previously suggested that will likely be under ideal conditions e.g. at a certain installed angle and at a certain flow rate. That will be still be viable for many applications.

    I think that petrol pumps tend to use a piston type flow meter rather than a turbine arrangement and they will also likely be well matched to the flow rate of the pump passing the liquid through them. They are likely to be serviced and calibrated at regular intervals as well.

    Hence why I was wondering about the accuracy necessary to make it viable over say the existing fuel gauge. At what point do you challenge the reading on the pump.

    If you doubt the advice given about accuracy, then perhaps do some experiments with some of the cheaper flow meters and see what accuracy you can achieve under different conditions. Perhaps also get a piston flow meter from an old decommissioned petrol pump and try that for comparison.

    The venturi tube controls the trigger mechanism in the petrol pump nozzle. It shuts off the pump when the tank is full or if you get blow-back.or if the tank's venting is faulty. It's a simple principle but the design is quite intricate. If your design attempts to couple a petrol pump nozzle directly into the input of a flow meter, you may find it affects the functioning of the venturi tube and shuts off the pump in the process. Some tubes vent to the outside of the nozzle through a small hole, others are contained inside of the nozzle itself so any design needs to accommodate the different types. 

    A scammer wants to make money so if they see such a device fitted then they may not want to serve you and wave you on so as they can scam the next person. Others may think it simply looks like a suspicious device and refuse to serve you. Depends on the type of petrol station it is though - attendant at the pump, self-serve but pay the attendant in the exit booth, or self-serve, pay with card at the pump. If it is hidden from view, then you avoid these sorts of scenarios.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to boodle

    I've already told you. I've used these sensors in various versions - brass, plastic, clear plastic ... they're all not very accurate especially in case of varying flow rates or flow rates that include rates below the minimum that the sensor is capable of. I used them in a number of applications including dispensing water for developing countries - we couldn't get it to accurately fill a 600mL bottle even with a consistent flow rate - even if you do calibrate it once and get it right, it doesn't take too long for it to drift away from the calibrated value due to changes in temperature, or movement of the sensor, or wear, or biofilms in the water, etc. Similarly, I have wanted for better, cheaper sensors for a long time ... but to no avail.

    Devices like that aren't really viable ... I don't see any reputable company ever selling them. I don't see anyone who cares ever using them either. The fact they need to be calibrated first and only have 0.5% repeatability (i.e. discounting accuracy, the relative error is 0.5%) is pretty shocking to me.

    You need to think carefully about the basics of metrology - as a rule, you can't use a clock of the same sort to check if a clock is accurate. You need something with more accuracy - usually 10x to 100x more accuracy to verify. Otherwise, all you're doing is measuring with very little certainty as the errors can go both ways for both devices in a nearly equal manner.

    Why are you asking questions of people over and over when you could buy 20 of them and test them out yourself with your own code and a calibrated pumping system to see what the errors are like yourself? Do some of your own science - don't expect people to have all the answers you seek!

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to boodle

    But since you asked - this is probably the closest thing to what you're looking for that I can find on the open market with a remote display:

    https://www.digiten.shop/products/digiten-lcd-flow-control-meter-g1-2-fuel-oil-gasoline-diesel-milk-gear-flow-counter

    Claims a 0.5% accuracy just like your Chinese stuff because it's likely built around the same thing.

    I have some of the 2%-rated Digiten stuff that is the same as the YF-201C /YF-S201 and similar Chinese flow sensors ... I measured the accuracy in a university lab to about 10-12% under a fixed flow rate, which is why i wouldn't trust the claimed accuracy regardless. That being said, you might get lucky ...

    Otherwise, you'll just have to build your own as I previously explained.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to boodle

    But since you asked - this is probably the closest thing to what you're looking for that I can find on the open market with a remote display:

    https://www.digiten.shop/products/digiten-lcd-flow-control-meter-g1-2-fuel-oil-gasoline-diesel-milk-gear-flow-counter

    Claims a 0.5% accuracy just like your Chinese stuff because it's likely built around the same thing.

    I have some of the 2%-rated Digiten stuff that is the same as the YF-201C /YF-S201 and similar Chinese flow sensors ... I measured the accuracy in a university lab to about 10-12% under a fixed flow rate, which is why i wouldn't trust the claimed accuracy regardless. That being said, you might get lucky ...

    Otherwise, you'll just have to build your own as I previously explained.

    - Gough