Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Multimeter DMM6500
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 325 subscribers
  • Views 2330 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Multimeter DMM6500

colegrand
colegrand over 3 years ago

Hello, I want to know if the multimeter DMM6500 can be controlled by a PC application. And if it can work on a LAN network. Where can I find a document with the driving needed to pilot the multimeter via a PC application ? Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +4
    I wrote a blog series on element14 about the remote options of the dmm6500: community.element14.com/.../dmm6500 possible place to start: Keithley DMM6500: Software Control Options Pt 1 - TSP Script Builder…
  • Gough Lui
    Gough Lui over 3 years ago +3
    colegrand said: DMM6500 can be controlled by a PC application Yes, Keithley DMM6500 is a SCPI-compliant DMM, thus you can control it from a PC using SCPI standard commands. Tektronix/Keithley do sell…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +1
    It is SCPI (Standard Commands for Programmable Instrumentation) compliant. This means you can use libraries like pyvisa with python to automate with it, you could probably also use anything that supported…
  • Gough Lui
    0 Gough Lui over 3 years ago
    colegrand said:
    DMM6500 can be controlled by a PC application

    Yes, Keithley DMM6500 is a SCPI-compliant DMM, thus you can control it from a PC using SCPI standard commands. Tektronix/Keithley do sell Kickstart 2 which supports the DMM6500. In addition, it also supports TSP scripting and TSP-based remote control. You can use it with NI LabVIEW too.

    colegrand said:
    work on a LAN network

    Yes, it has an Ethernet port on the back.

    colegrand said:
    document with the driving needed to pilot the multimeter via a PC application ?

    Read the full reference manual - https://www.tek.com/en/tektronix-and-keithley-digital-multimeter/dmm6500-manual/model-dmm6500-6-1-2-digit-multimeter-3

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colegrand
    0 colegrand over 3 years ago in reply to Gough Lui

    Thank you for your quick and efficient answer !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to Gough Lui

    When you say yes does that mean without barriers or can you communicate with the device only through the licenced product?

    The meter having an ethernet connector would give the assumption it can be connected to an IP network but controlling it may only be capable with the vendors software and not an open-source software solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to colporteur

    It is SCPI (Standard Commands for Programmable Instrumentation) compliant. This means you can use libraries like pyvisa with python to automate with it, you could probably also use anything that supported IVI and/or third party tools like NI LabVIEW.

    The vendor's package, KickStart 2 uses the instrument in TSP mode, which is Lua based but much more flexible. You can use their free TSB (Test Script Builder) IDE to build scripts to run on device or while connected to the host as another form of automation.

    It is connected to an IPv4 network, DHCP by default with manual configuration possible. Web interface remote control is possible. SCPI raw and TSP can operate through standard port 5025 in TCP.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago

    I wrote a blog series on element14 about the remote options of the dmm6500: community.element14.com/.../dmm6500

    possible place to start:  Keithley DMM6500: Software Control Options Pt 1 - TSP Script Builder, LabVIEW, Web Interface 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bidrohini
    0 bidrohini over 3 years ago

    This blog post may be helpful: community.element14.com/.../keithley-dmm6500-software-control-options-pt-1---tsp-script-builder-labview-web-interface

    • Cancel
    • Vote Up -2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colegrand
    0 colegrand over 3 years ago in reply to Gough Lui

    Hello

    I bought the DMM6500 and I have to run SCPI commands from a PC application. In my application, I must specify the port to write in. Where I can find the port number of the DMM6500  ?

    Thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to colegrand

    It depends on how you have connected your device to the PC and what VISA layer you have installed.

    If you're using NI-VISA, then you'll need to look at your instrument under NI MAX.

    Alternatively, if you have another VISA layer, you'll need to use whatever "Connection Manager" may come with that VISA layer. Alternatively, there may be a VISA resource string you can find on the instrument's menus, usually in the Info section somewhere, but you are best to use what the PC's VISA layer says.

    These are basic VISA questions which are covered by most automation tutorials online. I suggest you read them first before asking questions.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to Jan Cumps

    Like the post. The site is rich with content. I've made similar references when I can remember them:) 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer