Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum MPS1474 DC DC Buck regulator design
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 335 subscribers
  • Views 988 views
  • Users 0 members are here
  • buck
  • regulator
  • mps
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

MPS1474 DC DC Buck regulator design

Nilutpal66
Nilutpal66 over 3 years ago

Hi. I am designing a DC DC buck regulator using MP1474S. MP1474S | 2A, 16V, 500kHz, Synchronous, Step-Down Converter with PG | MPS (monolithicpower.com)

MPS have an online tool for designing buck regulator DC DC Designer Online - Design Tools - Design (monolithicpower.com)

These are my input specifications that I had given:

image

For which I got the following schematic circuit:

image

My query is why R4 is 0 ohm here? According to the datasheet, R4 should be nearby 16k as shown in the TYPICAL APPLICATION CIRCUIT of 5V,2A

Looking forward from hearing from you. 

Regards,

Nilotpal Baruah

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +1
    From what I can see, Vfb in the above is formed by the divider R1/R2, the R4 being zero just means no R4 is necessary. The ratio 47k / (301+47k) * Vout gives me Vfb = 0.810V which is about right - datasheet…
  • charlieo21
    charlieo21 over 3 years ago +1
    In the design validation stage is common to put a 10Ω resistor in that net for stability measurements.
  • Gough Lui
    Gough Lui over 3 years ago

    From what I can see, Vfb in the above is formed by the divider R1/R2, the R4 being zero just means no R4 is necessary. The ratio 47k / (301+47k) * Vout gives me Vfb = 0.810V which is about right - datasheet says typical Vfb is 0.807V.

    R4 itself is referred to as the T-type network and is recommended for low output voltages only - see datasheet Page 14:

    image

    As per the table, Rt is usually pretty close to R2, but the recommended resistor values are so much smaller than your R1/R2 values so maybe Rt is only significant in that case and the high resistances in your R1/R2 would mean that having an Rt (R4) may result in voltage errors due to the input impedance of the FB input. At least, that is my presumption.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • charlieo21
    charlieo21 over 3 years ago

    In the design validation stage is common to put a 10Ω resistor in that net for stability measurements.