Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need help reverse engineering a control box for an EV charger
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 337 subscribers
  • Views 4145 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need help reverse engineering a control box for an EV charger

Wolfmane
Wolfmane over 3 years ago

Hi folks,

I'm at a loss. I have a 2016 Zero SR electric motorcycle. A couple of years ago I ordered a high-powered charger kit on IndieGoGo from a company that had been around for quite a while. It was three 3.3 kW AC chargers in a custom belly pan, with all the wiring and a control box for plug-and-play installation. I was led to believe that I would be able to adjust the chargers for whatever situation I was in so that I could charge with anything from a regular wall socket to a 3-phase Type 2 EVSE. Past versions of these chargers could be connected via Bluetooth to a mobile phone and have the settings changed at will. However, when I received it it turned out to be hardcoded to run the chargers full blast. That means I can _only_ charge from 3-phase 10 kW+ EVSEs, which is far from ideal. There were other problems as well, including insufficient cooling that caused the chargers to overheat and throttle down to a trickle after only a few minutes, meaning I couldn't actually complete a charge session in one go. It took 3 or 4 tries with cooling pauses between in order to fully charge the battery pack. I got fed up with it and went back to totally stock.

The problem is that the company that made the kit promptly left the market and completely ceased all support. They stopped responding to any contact. That leaves me with a charge kit that cost me several thousand dollars just sitting collecting dust, and a bike that is otherwise awesome that is only good for commuting and day joyrides and can't be road-tripped as I was hoping to do when I ordered the kit. (The factory charger takes 8.5 hours to charge, vs. 45 minutes to an hour with the kit.)

I can solve the overheating by not using the belly pan that came with the kit (it was too deep anyway and caused some clearance issues with speed bumps) and mounting the chargers in another location with better airflow complete with heatsinks and fans. However, the control issue is far beyond my capability. I'm good with basic electronics and have played around with Raspberry Pis and even dabbled with ESP8266 (I have plans for a LOT more of that) but when it comes to analyzing signals and protocols and programming them I'm completely out of my depth. But I don't know where to turn for help.

What I really need is to make a new control box with a few buttons and knobs that will allow me to set the modes of the chargers quickly and easily without having to get out my phone or another device and go through the hassle of connecting and fiddling with that other device. Especially since using touch screens with motorcycle gloves is a far from optimal experience.

There are some things I know: I believe the chargers were based on, if not made by, Elcon. The control box connects to them via 4 wires. The control box doesn't care how many or which chargers are running, the control wires are simply connected in parallel to the chargers and whichever chargers are physically connected to power will run at whatever settings the control box is sending out. I believe it's a CAN Bus protocol. The communication is probably not even 2-way; the controller just sends out the settings and the chargers' internal control circuitry takes care of the rest.

Can anybody help me, or give me some idea of where I can go to get help reverse engineering the control protocol and programming an ESP8266 or similar to control the chargers? I would be happy to pay a reasonable fee for any help. I can't afford to pay a large percentage of what the kit cost, though. Any help would be immensely appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago +3
    Having been down this road myself (1985 engine control unit with zero documentation) I'd say collect what info you can and then start sniffing the control wires with a basic scope to see what is there…
  • charlieo21
    charlieo21 over 3 years ago +1
    Some pictures would help to understand with what we are dealing here.
  • charlieo21
    charlieo21 over 3 years ago in reply to Wolfmane +1
    Here is the CAN protocol for a Elcon charger, I think you can use any microcontroller with CAN bus and start playing with some messages.
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    There are people on E14 who could probably help you. Since you don't have the right gear to do the sort of testing needed you will need to get the whole caboodle to someone who does. So you need to tell us where you are located and see if anyone volunteers to give you a hand.

    If you can get to Castle Douglas in South West Scotland I'd be willing to have a go myself.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Wolfmane
    Wolfmane over 3 years ago in reply to michaelkellett

    I don't know if it would be reasonable to ship the system to someone who can make sense of it. Shipping costs are pretty steep these days, and while the control box is pretty small and light the chargers are fairly big and heavy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to Wolfmane

    They would need the bike as well !

    (I'm assuming you don't take the batteries out to charge them ?).

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 3 years ago in reply to Wolfmane

    They would need the bike as well !

    (I'm assuming you don't take the batteries out to charge them ?).

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Wolfmane
    Wolfmane over 3 years ago in reply to michaelkellett

    It's really only the control box that's needed. The first thing I need to do is identify the power wires to the control box. It should turn on and start sending control messages regardless of anything else being connected. I just need to find out if the control box runs on 110/220V, main pack voltage, 12V or something else. Then I can use an appropriate power supply to power it while doing the testing. I'll have to hook it up to at least one charger in order to figure out which are the power wires, but after that it's just the control box that I'm interested in. The chargers will probably throw up errors and not do much if not connected to the battery pack, but that doesn't matter. When I get to the stage of testing a new control box, there's an auxiliary charge port on the bike specifically for attaching external chargers, so they don't have to be installed or mounted, just connected.