Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Strobing Using RGB LEDs Instead Of Flash Tubes
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 335 subscribers
  • Views 3429 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Strobing Using RGB LEDs Instead Of Flash Tubes

publicimage
publicimage over 3 years ago

I would like to create a something like a strobe but with very bright RGB LEDs.

Can anyone suggest a product?

Can I use a MOSFET to power something like this? 

Which Arduino Would work best?

Please help!

--Vince

  • Sign in to reply
  • Cancel

Top Replies

  • robogary
    robogary over 3 years ago +1
    The Junk-Pile Strobe Tachometer.....and it really works! See the blog for some ideas. It's not so much the arduino, or the mosfet, but your LEDs are a critical component. A strobe has alot of power for…
  • robogary
    robogary over 3 years ago in reply to publicimage +1
    So more like flashing lights than a strobe...
  • ggabe
    ggabe over 3 years ago in reply to robogary +1
    Both Amazon and AliExpress has LED strobe party lights. Hard to beat Ali’s price, unless you already have the components on hand. You can always reverse engineer and replace the controller with an Arduino…
  • shabaz
    shabaz over 3 years ago in reply to publicimage

    As well as the ideas mentioned by everyone, it could also be worth experimenting with just white LEDs, since they will be simpler to drive (just a single output), easier to obtain with high output, and then for deep bright colors, look for a dichroic style filter (they are available on AliExprress too). If rotated with a servo, you'll get stunning bright colors, at your strobe speed of course, that can be altered in color as the servo changes. It might be no bad thing to implement this partially mechanically/optically, rather than RGB LEDs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ggabe
    ggabe over 3 years ago in reply to publicimage

    Reverse engineering can be done by redrawing the schematics without powering it up, so at that point  it’s safe.  Depending on your skills, it might not work again or be safe again….  

    Another way is to use the leds, the enclosure and the driver (presumably mosfet) and rebuild the rest of the controls, and using a safe external power brick. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to publicimage

    A simple 555 timer can generate a square wave signal to trigger a MOSFET or transistor easily at 60 times a second, 16 milliseconds, which is the same frequency as the AC outlet.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to ggabe

    Geez, you cant even buy the LEDs for 6 bucks, let alone thrown in an enclosure and pots with knobs.  For sure if the LEDs are change color based on loudest sound frequency and flash according to the bass beat - add a electret mike and a couple filters or equalizer IC MSGEQ7 , battery or power supply , cost adds up. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to publicimage

    How you approach it depends a lot on how much like a Xenon tube you want it to be.

    Xenon tubes produce very short very high power flashes.

    (I had a quick hunt around the internet and you would expect less than 100us pulse length. If the average power is 10W at 60 flashes per second that about 1600W during the flash.)

    If you want "freeze" human movement you may not need to go so fast  - I'm going to guesstimate that quick wavy hand or arms move at about 5m/s and to avoid blurring you want the flash to last the time the subject moves no more than 1cm - which results in a maximum flash time of 2ms and a power during the flash of about 160W.

    You can overdrive an LED so long as the average power is within spec - but the light output won't go on increasing as the current rises.

    let's look at some high power LEDs

    Here's one from Farnell:

    image

    You can put 1.3A maximum into it, and the efficiency is falling off at that level, you could push it a bit further maybe with short pulses.

    At 1.3A the forward voltage will be 4.3V so you'll be putting 5.6W in during the flash but the average power will only be 166mW with 1ms flashes.

    To get a decent level of brightness you will need 10 of each colour and a peak current of 13A per colour. The average power will only be 6.4W.

    As  shabaz suggested white LEDs will be easier and brighter (but I expect you want colour).

    This may seem a bit over the top - but you did say you wanted very bright !

    It's not that easy - or cheap -  the LEDs will cost at least £20 but I think the power drivers will cost the same again. Almost any Arduino could manage the 1ms control pulses.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to michaelkellett
    michaelkellett said:
    As  shabaz suggested white LEDs will be easier and brighter (but I expect you want colour).

    There's an English stage / art lighting specialist on EEVblog (Mike), who says that - if significant brightness is needed - he always uses white LEDs for white. Even if there is demand for colour, he will add the white ones in the mix.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago

    Trying the WLED app on an ESP wifi module is definitely a project worth considering in the future, it works great.

    image

    https://kno.wled.ge/features/effects/

    image

    Not saying its the ideal solution but worth a try...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    I visited this place with some friends ages ago:

    https://www.youtube.com/watch?v=kW4U5zdb8F0

    It's like an alternate reality where pretty much the _only_ lighting that exists throughout is strobe! I was just amazed there were no fights, considering you couldn't see anyone else for the (quite lengthy) 95% of the dark time in-between the flashes!  Bumping into others was inevitable, no way to avoid that there!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<