Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum The best transistor replacement
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 335 subscribers
  • Views 6644 views
  • Users 0 members are here
  • Replacement transistor grundig ts1000
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

The best transistor replacement

b139b
b139b over 3 years ago

Hello everyone. Hope you all are doing well Thumbsup
I need some smart input from you... I am looking for some replacement transistors for my old tape recorder. The recorder sounds like a thunderstorm, so I think one transistor is bad. Since those transistors (BC330C, BC237B, BC238B) not are available anymore, I am looking for replacements.

In this case, since the design already is given, is "typical hfe" the parameter witch is most important to match with the original transistor? - To keep the same amplification steps. 


All maximum-voltages must of course to be the same or higher to the original.

I have some BC550C with hfe=420-800. Is it correct to think that the typical hfe for the BC550C is in the middle of this values =610 ? Too much amplification in my case?
Any input is appreciated Blush
Christian

image

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +3
    b139b said: The recorder sounds like a thunderstorm, so I think one transistor is bad Have you already replaced the electrolytic capacitors? They are far more likely to have gone bad.
  • Gough Lui
    Gough Lui over 3 years ago in reply to baldengineer +3
    That and potentiometers ... *crackle crackle - Gough
  • shabaz
    shabaz over 3 years ago +2
    Hi, The BC550 is likely fine for all of these NPN transistors, since the actual transistor gain doesn't matter usually (because the circuit will control the actual gain). The BC550 is a very decent substitute…
Parents
  • shabaz
    shabaz over 3 years ago

    Hi,

    The BC550 is likely fine for all of these NPN transistors, since the actual transistor gain doesn't matter usually (because the circuit will control the actual gain). The BC550 is a very decent substitute for most TO-92 NPN transistors I expect. It's my standard go-to transistor (well, the BC549 version) for non-RF stuff.

    You could swap out one transistor at a time, replacing it back if it makes no difference. However you have voltages labelled on the schematic, so you can actually do the testing in-circuit with a multimeter.

    Are you sure it's not just a faulty switch or noisy potentiometer? Silicon transistors are very reliable. I have a ~60 year old radio receiver on my desk and it is still functioning.

    You could also use a test tool (or a crystal earpiece) to view or listen to the audio too; the crystal earpiece is non-intrusive to most of the circuit. Ideally you'd want to use an oscilloscope if you have access to it however.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    Hi,

    The BC550 is likely fine for all of these NPN transistors, since the actual transistor gain doesn't matter usually (because the circuit will control the actual gain). The BC550 is a very decent substitute for most TO-92 NPN transistors I expect. It's my standard go-to transistor (well, the BC549 version) for non-RF stuff.

    You could swap out one transistor at a time, replacing it back if it makes no difference. However you have voltages labelled on the schematic, so you can actually do the testing in-circuit with a multimeter.

    Are you sure it's not just a faulty switch or noisy potentiometer? Silicon transistors are very reliable. I have a ~60 year old radio receiver on my desk and it is still functioning.

    You could also use a test tool (or a crystal earpiece) to view or listen to the audio too; the crystal earpiece is non-intrusive to most of the circuit. Ideally you'd want to use an oscilloscope if you have access to it however.