Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How does the oscillating frequency of a charge pump make a difference?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 335 subscribers
  • Views 4388 views
  • Users 0 members are here
  • charge_pump
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How does the oscillating frequency of a charge pump make a difference?

BigG
BigG over 3 years ago

I recently purchased some Microchip TC7660S charge pumps as I plan to use them to generate a -12V DC output from a +12V DC input.

Based on the datasheet, the circuit seems simple enough.

However, I am rather puzzled by Pin 1, which the datasheet refers to as the Switching Frequency boost pin. Now, why would you need to boost the oscillating frequency - I'm guessing this is for when you want to generate a positive voltage multiplier.

Then on the bottom of page 10 (section 5.4 Changing the TC7660S Oscillator Frequency) it then talks about slowing the oscillating frequency using the following method:

For example, the addition of a 100 pF capacitor between pin 7 (OSC) and pin 8 (V +) will lower the oscillator frequency to 1 kHz from its nominal frequency of 10 kHz (a multiple of 10), and necessitate a corresponding increase in the values of C 1 and C 2 (from 10 μF to 100 μF).

So, as a learning exercise I'm also trying to fathom when does one decrease the frequency. I believe a clue is given in the datasheet, but not still not sure why one would want to, that you should only slow down the frequency for low currents. I'm given very little else.

I'm sure there's good reason for all of the above.

I look forward to receiving some insight.

Thanks.

Colin.

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 3 years ago +4
    The higher frequency will allow you use small capacitors, while low frequency will require larger capacitors, but also reduce EMI.
  • Jan Cumps
    Jan Cumps over 3 years ago +4
    BigG said: Now, why would you need to boost the oscillating frequency 5.4 Changing the TC7660S Oscillator Frequency It may be desirable in some applications (due to noise or other considerations) to…
  • shabaz
    shabaz over 3 years ago +4
    Hi Colin, It will affect the output. Surprisingly the TC7660S PDF datasheet doesn't mention the output waveform in any detail, but the TC7662B PDF datasheet does, and the same info will apply. There…
Parents
  • dougw
    0 dougw over 3 years ago

    Just speculating .... Charge pumps can transfer "fixed" charge on each cycle of the clock. At higher frequencies the amount of charge and thus average current is increased (more charge transfers per second) which allows a heavier load and lower ripple. There may be higher switching losses at higher frequencies and some components may get hotter so you would only boost the frequency when you need the extra current.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 3 years ago

    Just speculating .... Charge pumps can transfer "fixed" charge on each cycle of the clock. At higher frequencies the amount of charge and thus average current is increased (more charge transfers per second) which allows a heavier load and lower ripple. There may be higher switching losses at higher frequencies and some components may get hotter so you would only boost the frequency when you need the extra current.

    • Cancel
    • Vote Up +3 Vote Down