Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Radio Broadcasting from Online Stream
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 335 subscribers
  • Views 3243 views
  • Users 0 members are here
  • broadcast
  • radio
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Radio Broadcasting from Online Stream

Bucks141
Bucks141 over 2 years ago

How do I take an online livestream commentary, and broadcast it to radio?

Context: 

In a highly populated area, wifi bandwidth is insufficient to allow for live streaming.

How can I create a radio broadcast from one wifi connection?

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 2 years ago +6
    By your points total you are new to the community. Welcome. Can you provide (a lot) more details? You may be in violation of some laws doing an RF broadcast. That is if my assumption of Radio you mean…
  • dougw
    dougw over 2 years ago +4
    In some countries you are allowed to broadcast license-free at very low power levels in some bands. (but not in the UK) With good equipment and no noise nearby, you might get 100 feet of broadcast range…
  • shabaz
    shabaz over 2 years ago in reply to Bucks141 +3
    Hi, Unfortunately the amateur radio licenses explicitly forbid broadcasting. Any communication via amateur radio licence has to be licensed user to licensed user (apart from a request for a contact)…
Parents
  • Bucks141
    0 Bucks141 over 2 years ago

    Thank you for the warm welcome colporteur, yes I'm new to the community.

    Greatly appreciate both of your comments and apologies for the lack of clarity. That question was overly simplified and vague.

    It would certainly be amateur radio and I feared there could be some local law broadcast violations which I'd look into individually. 

    In short, we often attend live sporting events where either there are no RF commentary broadcasts, (but there is online audio commentary available via an app) or there is an RF broadcast in a local language (and the English commentary is available via an app).

    Where wifi is available at these events, the signal strength is often poor and it's heavily over subscribed. 4/5g connections are also unstable simply due to the number of mobile phones in the vicinity. Therefore the online audio commentary is inaccessible. 

    In theory, I thought "perhaps" it was possible to acquire/configure a device that could take audio from a live online audio stream, and transmit it through a RF to a small group of receivers/headsets.

    I appreciate there may be broadcast licences involved and local law also, but wanted to understand how complex this would be to setup.

    Thanks again for your comments and quick responses.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Bucks141
    0 Bucks141 over 2 years ago in reply to Bucks141

    To clarify, I'm talking about race events where attendance is between 200,000-300,000 people in attendance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 2 years ago in reply to Bucks141

    I'm thinking you are describing a problem most of us have experienced. I have problems with wifi at my local sporting event with less than 100 fans in attendance. Heck my daughter at here home has the problem on wifi and streaming. I moved her TV service from wifi to CAT5 and she has never complained since.

    The Canadian Football league has some RF broadcasts for games. I would sit with an AM transistor radio in my ear to hear commentary while watching the game. That is a commercial broadcast service.

    I might understand your problem but not sure I can provide a workable solution.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to Bucks141

    Depending on your budget and whether or not this is an outdoor event, then you could perhaps take a look at some of the satellite phone data services such as Iridium GO. Looks like they can achieve 88kbps download, which is enough for an audio commentary, especially if you transrate the audio stream first before accessing it via satellite link. Voice data can be heavily compressed and thus  reduce the data rates required over expensive comms links.

    If you are doing a group booking and can get enough space for the group at the event then there is the likes of Starlink Roam for satellite broadband. May also be an option if you have a campervan parked nearby.

    You could perhaps use a PMSE license to do short audio links between two points, especially using directional antennas with line of site. This might be tricky however as different countries use different frequency allocations and licensing.

    On-site this might be a use case for Bluetooth Auracast for public locations allowing the receiving device to broadcast to a number of local listening devices.

    Other approaches may be to try improving your WiFi/mobile set-up for better reach. Directional external antennas and/or cellular multiplexing can sometimes help you reach beyond the main crowd.

    About 10 years ago, I used to have a rig similar to this one: 
    image

    which bonded up to 6 external 3G cellular modems together using external mobile providers to be able to live stream video from sites with poor access to the Internet.

    With the right USB modems, it was possible to add external antennas to get further range as described in the higher profile setup here:  

    https://www.youtube.com/watch?v=xovEfYqNPG8&t=180s 

    I seem to recall at the time you could get more generic 'cellmux' boxes to create ad-hoc Wi-Fi hotspots for similar reasons. Might be worth a look to see what there is these days.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to Bucks141

    Depending on your budget and whether or not this is an outdoor event, then you could perhaps take a look at some of the satellite phone data services such as Iridium GO. Looks like they can achieve 88kbps download, which is enough for an audio commentary, especially if you transrate the audio stream first before accessing it via satellite link. Voice data can be heavily compressed and thus  reduce the data rates required over expensive comms links.

    If you are doing a group booking and can get enough space for the group at the event then there is the likes of Starlink Roam for satellite broadband. May also be an option if you have a campervan parked nearby.

    You could perhaps use a PMSE license to do short audio links between two points, especially using directional antennas with line of site. This might be tricky however as different countries use different frequency allocations and licensing.

    On-site this might be a use case for Bluetooth Auracast for public locations allowing the receiving device to broadcast to a number of local listening devices.

    Other approaches may be to try improving your WiFi/mobile set-up for better reach. Directional external antennas and/or cellular multiplexing can sometimes help you reach beyond the main crowd.

    About 10 years ago, I used to have a rig similar to this one: 
    image

    which bonded up to 6 external 3G cellular modems together using external mobile providers to be able to live stream video from sites with poor access to the Internet.

    With the right USB modems, it was possible to add external antennas to get further range as described in the higher profile setup here:  

    https://www.youtube.com/watch?v=xovEfYqNPG8&t=180s 

    I seem to recall at the time you could get more generic 'cellmux' boxes to create ad-hoc Wi-Fi hotspots for similar reasons. Might be worth a look to see what there is these days.