Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Trying to find a high-speed, high-power transistor to use as a switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Subscribers 334 subscribers
  • Views 6051 views
  • Users 0 members are here
  • mosfet
  • components
  • igbt
  • ask_an_expert
  • circuit
  • switch
  • power
  • power_electronics
  • question
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Trying to find a high-speed, high-power transistor to use as a switch

ZappaMap
ZappaMap over 3 years ago

I'm designing a high power H-bridge circuit, and I'm trying to find the best transistor for the design. The most important parameters are that it has
- 10MHz switching speed frequency

- Low on-state resistance

- Low off-state capacitance

From there, I would need it to handle high voltages and have a low gate charge. With that in mind, does anyone know of any parameter relationships I should be aware of or what products potentially match that description? Thank you!

EDIT:

Thank you all for your responses! To answer a couple questions I saw:

- I do not have a preference between MOSFETS and BJTs.

- For voltage and amperage, I don't have hard numbers for those. I'm still operating in the tradespace stage of the design right now, so I'm still figuring out what options I have. To give a ballpark range, a component that works with volts on the order of 10V or 100V and amps on the order of 10A wouldn't hurt. I am more concerned with the switching frequency, on-state resistance, and off-state capacitance.

I also learned a little more about switchmode amplifiers, and that is another avenue that I am now looking down (specifically class D and E).

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +5
    I think you'll need to quantify the current and voltage to get good advice. 10MHz is very fast for typical H bridge type applications. Do you have a preference between MOSFETs and BJTs ? As you probably…
  • dougw
    dougw over 3 years ago +3
    You might have a look at Gallium Nitride transistors.
  • scottiebabe
    scottiebabe over 3 years ago +3
    You may also consider pre-engineered GaN half-bridge modules or ultrasound pulse drivers.
Parents
  • shabaz
    +1 shabaz over 3 years ago

    No real information of what is a high voltage and what current needs to be supported.

    You could examine RF power transistors, discrete or otherwise. Here is an example dual transistor (i.e. half a H-bridge so two would be needed for a full H-bridge) which is pretty high-power and high-voltage, with a driver built-in. https://ww1.microchip.com/downloads/en/DeviceDoc/DRF1400_%20B.pdf 

    The price is as expected...

    Discrete transistors are going to be pricey too. They will come in funny packages, and you may need "opposite-packaged" pairs, otherwise it's a bit hard to route traces for them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    +1 shabaz over 3 years ago

    No real information of what is a high voltage and what current needs to be supported.

    You could examine RF power transistors, discrete or otherwise. Here is an example dual transistor (i.e. half a H-bridge so two would be needed for a full H-bridge) which is pretty high-power and high-voltage, with a driver built-in. https://ww1.microchip.com/downloads/en/DeviceDoc/DRF1400_%20B.pdf 

    The price is as expected...

    Discrete transistors are going to be pricey too. They will come in funny packages, and you may need "opposite-packaged" pairs, otherwise it's a bit hard to route traces for them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • ZappaMap
    0 ZappaMap over 3 years ago in reply to shabaz

    This looks great, thank you! I haven't worked with RF power transistors before. Would you recommend specific manufacturers or types? Is there anything I should keep in mind while looking into these?