Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Trying to find a high-speed, high-power transistor to use as a switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Subscribers 334 subscribers
  • Views 6056 views
  • Users 0 members are here
  • mosfet
  • components
  • igbt
  • ask_an_expert
  • circuit
  • switch
  • power
  • power_electronics
  • question
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Trying to find a high-speed, high-power transistor to use as a switch

ZappaMap
ZappaMap over 3 years ago

I'm designing a high power H-bridge circuit, and I'm trying to find the best transistor for the design. The most important parameters are that it has
- 10MHz switching speed frequency

- Low on-state resistance

- Low off-state capacitance

From there, I would need it to handle high voltages and have a low gate charge. With that in mind, does anyone know of any parameter relationships I should be aware of or what products potentially match that description? Thank you!

EDIT:

Thank you all for your responses! To answer a couple questions I saw:

- I do not have a preference between MOSFETS and BJTs.

- For voltage and amperage, I don't have hard numbers for those. I'm still operating in the tradespace stage of the design right now, so I'm still figuring out what options I have. To give a ballpark range, a component that works with volts on the order of 10V or 100V and amps on the order of 10A wouldn't hurt. I am more concerned with the switching frequency, on-state resistance, and off-state capacitance.

I also learned a little more about switchmode amplifiers, and that is another avenue that I am now looking down (specifically class D and E).

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +5
    I think you'll need to quantify the current and voltage to get good advice. 10MHz is very fast for typical H bridge type applications. Do you have a preference between MOSFETs and BJTs ? As you probably…
  • dougw
    dougw over 3 years ago +3
    You might have a look at Gallium Nitride transistors.
  • scottiebabe
    scottiebabe over 3 years ago +3
    You may also consider pre-engineered GaN half-bridge modules or ultrasound pulse drivers.
Parents
  • anniel747
    anniel747 over 3 years ago
    This reply was deleted.
    • Cancel
    • Cancel
  • rsc
    0 rsc over 3 years ago in reply to anniel747

    IGBTs are very slow.  100khz is pushing the limits.10mhz I've never heard of with an IGBT.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    anniel747 over 3 years ago in reply to rsc
    This reply was deleted.
    • Cancel
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to anniel747

    http://www2.arrl.org/files/file/QEX_Next_Issue/2014/May-Jun_2014/Horowitz.pdf

    But .... this is a quasi linear application of an IGBT.

    The rise and fall times (of the IGBT they used) add up to 37ns so they wouldn't work in a switching H bridge at anything like 20MHz - might scrape1MHz but they would get warm.

    But unless the OP comes back an explains better what they are looking for we are, to coin a phrase, "switching in the dark" (although he did say switching speed, but he might have meant switching frequency which is more commonly measured in Hz)

    Has anyone (here on E14) used IGBTs in a linear application.

    There is a nice Analogue Devices app note for an audio power amplifier design but you can't buy the P channel parts any more.

    I've used IGBTs in linear (high-ish) power regulators with reasonable success.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to michaelkellett

    I have not used them (linear or otherwise), although I'm interested. IGBTs passed me by, they were not taught when I was at uni, and I didn't come across them in any on-the-job (or otherwise) applications or training. I missed out. And now there are interesting high power and voltage semiconductors like SiC for high power or GAN for power+speed, so I'm unsure when IGBTs would be selected (presumably they are lower-cost than SiC). I've experimented a bit with SiC parts for switching, but even the experiments end up pricey.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago in reply to michaelkellett

    I have not used them (linear or otherwise), although I'm interested. IGBTs passed me by, they were not taught when I was at uni, and I didn't come across them in any on-the-job (or otherwise) applications or training. I missed out. And now there are interesting high power and voltage semiconductors like SiC for high power or GAN for power+speed, so I'm unsure when IGBTs would be selected (presumably they are lower-cost than SiC). I've experimented a bit with SiC parts for switching, but even the experiments end up pricey.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to shabaz

    You can use them like NPN power transistors (no one makes P type parts any more) . They are quite cheap and have good but not perfect SOA.

    This design was done initially to make 55V 5A power supplies for audio nonsense (replicating ancient Mullard transistor designs). Its very loosely based on the power supply design for the Quad 303 power amp.

    image

    If you want to build one I'll sort out the component values  - I must have written them down somewhere.

    I might even have a board left.

    Note the position of the N type sereis pass device in the negative rail !

    The load goes across J2 and pin 2 of J2 is typically connected to the system ground.

    The rectifier got way too hot at 5A - so a had to bodge the heatsinks.

    This pic is a dual 12V version, that's a 200VA transformer with two separate 12V secondaries.

    image

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • javagoza
    0 javagoza over 3 years ago in reply to shabaz

    I studied IGBT in the last years of university, in the late 80s and early 90s. I still have Ned Mohan's 1989 book at home: "Power Electronics: Converters, Applications and Design". In the book he classified IGBTs as switching devices with medium power capacity, 1200 V / 100 A, and medium switching speed similar to BJTs. Surely things have changed a lot since then. Then I was lucky enough to lead a project to change the UPS in the newsroom of a newspaper where I worked to UPS that used IGBTs.