Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How to download the files for ZedBoard Configuration and Booting Guide ("reference design").
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 334 subscribers
  • Views 521 views
  • Users 0 members are here
  • ZedBoard Booting Guide ("reference design").
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How to download the files for ZedBoard Configuration and Booting Guide ("reference design").

mvernengo
mvernengo over 2 years ago

Where can i find for downloading the following files mentioned as "reference design" in  the "ZedBoard Configuration and Booting Guide"?

BOOT.BIN: Boot image of First Stage Boot Loader (FSBL), PL bistream, and GPIO test application.

bootimage.bif: Boot image information text file.

cp_from_sdk.bat: Batch file to copy hardware bitstream and software executables from the SDK workspace.

gpio_test_0.elf: The golden ARM executable for the GPIO test application.

load_bits.tcl: TCL script to load the PL bitstream via XMD.

make_bootbin.bat: Batch file to run the command to create the boot image file.

ps7_init.tcl: TCL script to initialize the ARM processor.

run_gpio_test.bat: Batch file to run the commands to load the PL bitstream of the hardware design, initialize the processor, and download the GPIO test
application.

run_uboot.bat: Batch file to run the commands to initialize the processor and download the u-boot application.

system.bit: The golden FPGA bitstream of the hardware design required to run the GPIO test application.

u-boot_autoboot_disabled.elf: The golden ARM executable for the u-boot application used to program the QSPI Flash.

xmd.ini: Command file used by XMD to configure the PL with the hardware bitstream, initialize the processor, and download the software applications.

zynq_fsbl_0.elf: The golden ARM executable for the Zynq FSBL.doc: Contains documentation for this design:

pa: Contains the PlanAhead hardware project and SDK workspace files and folders.

SDK_sw: Contains the GPIO test software application source files.

boot_image_golden.zip: Contains pre-built BOOT.BIN boot image for this design.

demo_golden.zip: Contains the golden copies of the files in the demo folder.