Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Any interest in collaborating on a REBOOT for the Apple II?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 41 replies
  • Answers 1 answer
  • Subscribers 331 subscribers
  • Views 6654 views
  • Users 0 members are here
  • esp32
  • io
  • apple
  • arduino
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Any interest in collaborating on a REBOOT for the Apple II?

barryhills
barryhills over 2 years ago

I am seeking a solution for a single pushbutton reset/reboot for the Apple II. In my volunteer work with young children (8-10 yrs old) using the Apple II they frequently want or need to reset the Apple II (we use both //e and II+). There are several obsticals to doing a clean hard reset on the Apple. The primary issues are the reset vectors in dynamic ram, the nuanced multi-finger reset options, and the fragility of the Apple II switching power supply. The kids need a one button reset for the Apple without hitting the power supply with another power-on surge in the hope they left it off long enough for the dynamic ram to "clear" and without needing to learn a multi-finger keyboard sequence.

I understand this project is a little silly, but I prefer to think of it as a small interesting technical challenges for the right person.

Here are some of the rabbit holes I have wandered....

a) I want to keep the base machine clean and thus want to avoid custom ROMs.

b) It would be "nice" to use the existing reset button on the keyboard but a tethered reset button is perfectly ok and what I anticipate will be needed.

c) I've always assumed the solution must clear memory prior to doing the clean reboot.

d) Mostly, I've assumed a small (minimal) I/O card would be the best way to cause an interrupt and pass 6502 control over to an alternate code path to clear memory and reboot. A plug-in card would also provide an electrical home for a tethered reboot button.

e) Traditional I/O cards use a small PROM or EPROM which is ok; but the current trend of using a SOC would also be ok if it makes programming and/or hardware for the new REBOOT code easier.

f) As a side note, there was a card called the "Wildcard" that had a tethered button that presented a menu when pressed. One of the menu options was "clear memory and reboot". It seems to be exactly the functionality I want but don't want a menu and don't want to hunt down a Wildcard for all of the Apples we have in our little lab.

Ideally, I would find someone who thinks a small project like this could be fun. My hope is there are lots of I/O cards, past and modern that can be borrowed from to make such a project trivial for someone comfortable with Apple II hardware. Software is my primary domain and while I am generally comfortable with hardware, getting into memory bus timing phases is beyond my skills.

Anybody think this could be fun? Any other clever considerations to accomplish my objective?

TIA

Barry

UPDATE:

A long time later this project is done.  Check out the story here...... https://csguy.org/technotes/white-whale-reboot-project/

image

  • Sign in to reply
  • Cancel

Top Replies

  • barryhills
    barryhills over 2 years ago in reply to Fred27 +4
    These kids grow up thinking knowing little more than icons on a phone. You are correct that the Apple is "my" passion and I am sharing it with them. But I would also say the simple nature of the machine…
  • Andrew J
    Andrew J over 2 years ago in reply to Fred27 +4
    Then you'd be amazed Fred. The STEM work at The National Museum of Computing involves lots of old computers - a lot is done with BBC Micros for example - as well as newer types of technology, e.g. VR,…
  • barryhills
    barryhills over 2 years ago +4
    A long time later this project is done. Check out the story here...... https://csguy.org/technotes/white-whale-reboot-project/
Parents
  • phoenixcomm
    0 phoenixcomm over 2 years ago

     barryhills image Oh, well, some folks are blind, others are lazy, Google Image Search revealed this image (on the right). I would use a double-pole push-button. Now you have three connections:

    • Common is wired to the CPU's pin 40
    • ON is wired to a 10k resistor to p5v (this keeps the pin from flopping around
    • OFF is wired to ground.

    You will have to, do some investigation, and trace the wire on the PCB as there may be a pull-up on pin 40 already, If there is remove the resistor. 

    One word of warning.... NEVER SOLDER TO THE CPU!! I believe they were socketed. 

    ~~ Cris H. 

    Oh BTW I also have the Programers Reference & Application manuals

    let me know If you want copies there in pdf format I will have to hang them on my server. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • barryhills
    0 barryhills over 2 years ago in reply to phoenixcomm

    I am familiar with the 6502 pin definitions. The challenge has little to do with the 6502 and everything to do with the reset and power-up logic (in ROM) for the APPLE II.  I tried to make this clear.  This is an idea specifically for the Apple II. The 6502 reset simply transfers control to a routine in ROM where a multi step ridiculous flow of logic triggers various forms of soft reset and is reliant on the contents of vectors in RAM.  Dynamic Ram does not fade quickly like static ram which is why I imagine the solution will require a routine to clear memory or at least the reset vectors.

    As an aside, I posted on Element 14 in search of thoughtful professionals, enthusiasts, and experts.  I never expected the very first reply to my very first post to include  snarky BS.  If I wanted snarky I would have posted on Reddit, Twitter, or Facebook.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • PPE_COOP
    0 PPE_COOP over 2 years ago in reply to barryhills

    Funny you should say "As an aside, I posted on Element 14 in search of thoughtful professionals, enthusiasts, and experts.  I never expected the very first reply to my very first post to include  snarky BS.  If I wanted snarky I would have posted on Reddit, Twitter, or Facebook." I recently had a similar experience. Eventually the real community began to respond but one of the first comments was meant to intimidate and shame me for posting. Sorry I can't help with your current project. I just thought I would help drive your other point home.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to barryhills

    Cris is being humorous, you'd recognize it after seeing more messages over time (You can see that Cris also offered to provide you with reference manuals, it's actually a friendly response, i.e. It's easy to accidentally misinterpret the tone from text alone basically, is what I'm trying to say.

    PPE_COOP's situation was actually different, people had comments on technical points solely in that case, and probably saved PPE_COOP effort and cost in patenting something (which is what they originally referred to) that wouldn't have helped them.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago in reply to barryhills

    Cris is being humorous, you'd recognize it after seeing more messages over time (You can see that Cris also offered to provide you with reference manuals, it's actually a friendly response, i.e. It's easy to accidentally misinterpret the tone from text alone basically, is what I'm trying to say.

    PPE_COOP's situation was actually different, people had comments on technical points solely in that case, and probably saved PPE_COOP effort and cost in patenting something (which is what they originally referred to) that wouldn't have helped them.