Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Any interest in collaborating on a REBOOT for the Apple II?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 41 replies
  • Answers 1 answer
  • Subscribers 331 subscribers
  • Views 6695 views
  • Users 0 members are here
  • esp32
  • io
  • apple
  • arduino
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Any interest in collaborating on a REBOOT for the Apple II?

barryhills
barryhills over 2 years ago

I am seeking a solution for a single pushbutton reset/reboot for the Apple II. In my volunteer work with young children (8-10 yrs old) using the Apple II they frequently want or need to reset the Apple II (we use both //e and II+). There are several obsticals to doing a clean hard reset on the Apple. The primary issues are the reset vectors in dynamic ram, the nuanced multi-finger reset options, and the fragility of the Apple II switching power supply. The kids need a one button reset for the Apple without hitting the power supply with another power-on surge in the hope they left it off long enough for the dynamic ram to "clear" and without needing to learn a multi-finger keyboard sequence.

I understand this project is a little silly, but I prefer to think of it as a small interesting technical challenges for the right person.

Here are some of the rabbit holes I have wandered....

a) I want to keep the base machine clean and thus want to avoid custom ROMs.

b) It would be "nice" to use the existing reset button on the keyboard but a tethered reset button is perfectly ok and what I anticipate will be needed.

c) I've always assumed the solution must clear memory prior to doing the clean reboot.

d) Mostly, I've assumed a small (minimal) I/O card would be the best way to cause an interrupt and pass 6502 control over to an alternate code path to clear memory and reboot. A plug-in card would also provide an electrical home for a tethered reboot button.

e) Traditional I/O cards use a small PROM or EPROM which is ok; but the current trend of using a SOC would also be ok if it makes programming and/or hardware for the new REBOOT code easier.

f) As a side note, there was a card called the "Wildcard" that had a tethered button that presented a menu when pressed. One of the menu options was "clear memory and reboot". It seems to be exactly the functionality I want but don't want a menu and don't want to hunt down a Wildcard for all of the Apples we have in our little lab.

Ideally, I would find someone who thinks a small project like this could be fun. My hope is there are lots of I/O cards, past and modern that can be borrowed from to make such a project trivial for someone comfortable with Apple II hardware. Software is my primary domain and while I am generally comfortable with hardware, getting into memory bus timing phases is beyond my skills.

Anybody think this could be fun? Any other clever considerations to accomplish my objective?

TIA

Barry

UPDATE:

A long time later this project is done.  Check out the story here...... https://csguy.org/technotes/white-whale-reboot-project/

image

  • Sign in to reply
  • Cancel

Top Replies

  • barryhills
    barryhills over 2 years ago in reply to Fred27 +4
    These kids grow up thinking knowing little more than icons on a phone. You are correct that the Apple is "my" passion and I am sharing it with them. But I would also say the simple nature of the machine…
  • Andrew J
    Andrew J over 2 years ago in reply to Fred27 +4
    Then you'd be amazed Fred. The STEM work at The National Museum of Computing involves lots of old computers - a lot is done with BBC Micros for example - as well as newer types of technology, e.g. VR,…
  • barryhills
    barryhills over 2 years ago +4
    A long time later this project is done. Check out the story here...... https://csguy.org/technotes/white-whale-reboot-project/
Parents
  • jc2048
    0 jc2048 over 2 years ago

    Idea 1.
    Multipole relay on the output side of the PSU, maybe? Press the push button and a timer drops the supply to the processor board for 10 seconds. Would that work? Might be better and more controlled with MOSFETs though (perhaps look to the kind of parts used for power sequencing for ideas).

    Idea 2.
    It's about 40 years since I last did anything with a IIe, so I remember nothing about the IO boards. Do they control overriding the bus so that they can sit where there would otherwise be DRAM system memory? If so, you might be able to watch out for the address location of the 'magic number' and take control of the bus and return a different value in it's place. That would be a bit of programmable logic on a board, if you were comfortable with that, and a '245 to drive the data lines.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 2 years ago

    Idea 1.
    Multipole relay on the output side of the PSU, maybe? Press the push button and a timer drops the supply to the processor board for 10 seconds. Would that work? Might be better and more controlled with MOSFETs though (perhaps look to the kind of parts used for power sequencing for ideas).

    Idea 2.
    It's about 40 years since I last did anything with a IIe, so I remember nothing about the IO boards. Do they control overriding the bus so that they can sit where there would otherwise be DRAM system memory? If so, you might be able to watch out for the address location of the 'magic number' and take control of the bus and return a different value in it's place. That would be a bit of programmable logic on a board, if you were comfortable with that, and a '245 to drive the data lines.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • barryhills
    0 barryhills over 2 years ago in reply to jc2048

    Apple II memory is mapped in a manner that "allocates" each IO slot its own tiny bit of code space.  The NMI from the IO board interrupts the 6502 which passes control to the monitor ROM interrupt handler which determines which slot called and begins execution of the instructions hosted by the tiny bit of memory on the IO card.  Once an IO card has control of the IO card has access to all of physical memory.  But raw access of the address and data lines seems above my skillset unless I am making it harder than needed.  seems you need to understand and manage some tricky timing of the dram refresh etc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • barryhills
    0 barryhills over 2 years ago in reply to jc2048

    I understand the Mosfet idea.  Kudos for creativity.  If I am careful it may only be necessary to interrupt a single voltage such as 5V.  I may play with your idea.  I would probably have to interrupt the -12v since it is what powers the dram

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 2 years ago in reply to barryhills

    One caution - back then it wasn't unknown for SMPSs to need a minimum load on the main output for the other outputs to be in regulation. So if you do decide to experiment, check the voltages off-load with a meter first.

    I'd also be cautious with respect to the DRAM - I'd forgotten that it was before they came single-supply. With multiple rails, they may need to be sequenced properly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • barryhills
    0 barryhills over 2 years ago in reply to jc2048

    you are correct about the requirement for a load on that old switcher.... thanks for the reminder.  There is no logic per-se in the PSU to stage power-up although it could be in there and I just dont understand.  To the best of my knowledge the PSU simply jolts all power on at the same time.  There may be PON logic in the PROM to ensure everything is live but I don't think they were that clever back then.  thank you again for the reminder

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 2 years ago in reply to barryhills

    I think you're right about the DRAM sequencing. I don't recall doing anything special when using them. I've got an old Intel design manual here which includes a datasheet for the 2107B and it says "The only requirement for the sequence of applying voltages to the device is that Vdd, Vcc, and Vss should never be 0.3V more negative than Vbb", so, as long as the -5V rail is always negative relative to 0V and the positive ones always remain positive, you shouldn't have any problems.