Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum is there a locking device on the tiny connectors that activate my exercise bike monitor.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • +1 person also asked this people also asked this
  • Replies 2 replies
  • Subscribers 333 subscribers
  • Views 1037 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

is there a locking device on the tiny connectors that activate my exercise bike monitor.

Prb1
Prb1 over 2 years ago

is there a locking device on the tiny connectors that activate my exercise bike monitor. They won't stay connected and, once I finish the assembly, they will be inside the handlebar post, so not accessible. Should I use electrical tape? I don't know if the little plast icwings are locks and am afraid of breaking them.imageimage

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +4 verified
    Hi, The thing that will hold the connector mated, is the latch. If you press at the green arrow direction, then the latch will lift slightly (yellow arrow). That's used to unlatch. When you push the…
  • Prb1
    Prb1 over 2 years ago in reply to shabaz +1
    I figured out the latch right after I wrote this (typical!) but not the unlatch. thanks more than I can say. cheers, polly
Parents
  • shabaz
    +1 shabaz over 2 years ago

    Hi,

    The thing that will hold the connector mated, is the latch. If you press at the green arrow direction, then the latch will lift slightly (yellow arrow). That's used to unlatch. 

    When you push the connectors together, the yellow end will slightly lift and then latch on, using the springiness in the plastic lever. It should be able to easily handle the vibration from the bike, otherwise the manufacturer would use a different connector (e.g. a screwed connector). Once it is latched on, you can test by trying to lightly tug apart the two connectors, and they won't come apart, unless you press at that green arrow direction.

    If you really are concerned that it will come apart, then there's no harm using a bit of tape of course, provided the tape is not on so tight as to unlatch at that green arrow location. Personally I would not use electrical tape because it leaves a sticky mess. 

    image

    The items marked in blue are unrelated. They are used for panel mounting. Sometimes manufacturers use such connectors with no intention for them to be mounted in a panel, i.e. if the user instructions do not indicate any fitting into a panel, then you can ignore the blue items. They serve no other purpose.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Prb1
    0 Prb1 over 2 years ago in reply to shabaz

    I figured out the latch right after I wrote this (typical!) but not the unlatch.

    thanks more than I can say.

    cheers,

    polly

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Prb1
    0 Prb1 over 2 years ago in reply to shabaz

    I figured out the latch right after I wrote this (typical!) but not the unlatch.

    thanks more than I can say.

    cheers,

    polly