Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Audio Power Transistors - Buying in Bulk
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 18 replies
  • Subscribers 333 subscribers
  • Views 3158 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Audio Power Transistors - Buying in Bulk

dank123
dank123 over 2 years ago

Hi All,

Does anyone have a solid opinion on the quality of Multicomp Pro MJ15003 and MJ15004 power transistors (Newark# 76AH5818 and 76AH5819)? I want to stock up on these parts as I use them quite a bit and the Multicomp Pro ones come in at about half the cost of the other name brand devices. I use these parts for vintage audio amplifier repair and the occassional amp build from scratch. Not exactly critical applications, but I'd like to get some assurance that they are at least worth the money. Otherwise, I may as well just spend the extra and get ONSEMI. Has anyone tested this Multicomp Pro transistors to see what conditions they fail under as compared to the ONSEMI ones? 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago +4
    Looking at the data sheets for the parts I would sy that there are definite causes for concern: The features section of the Multicomp data sheet seems to be for a different part. Multicomp features…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to michaelkellett +3
    michaelkellett said: almost all your customers would rather have the Onsemi parts. "No one gets fired for buying IBM" was the IT equivalent for that.
  • shabaz
    shabaz over 2 years ago in reply to anniel747 +3
    "Why would you think it's a fake?" Because your photo was taken from a counterfeit transistor web-page that explains it in black-and-white: As you can see from the red highlighted text, the purchaser…
Parents
  • shabaz
    0 shabaz over 2 years ago

    There's less information on those devices, hence the low-cost. But the physical chip inside will still be made in the same factories that the branded parts are made in, it's not possible to manufacture semiconductors in lower-quality at a cheaper factory, it's a binary thing.

    However, I think if you ask your audio customers which part they would want inside their repair or new product, they will want the branded part every time.

    Every time I do an audio-related repair for anyone, I've stopped asking which parts to use.. I simply use branded parts, top-quality (or thereabouts!) ones, and just pass the cost on. No audio customer wants to know that they got the cheaper unbranded parts inside their product.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dank123
    0 dank123 over 2 years ago in reply to shabaz

    I agree.

    It is so I can keep a large stash on hand for my own stuff and I don't care about the name as long as they work equally well compared to the more expensive ones.

    So you're saying one factory makes all the internal chips and then separate factories make the metal casing and stamp their own brand on them, but put those same chips inside?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to dank123

    The internal die (chip) is made in the same factories, i.e. identical quality level, but you won't know which specific transistor that it electrically matches 100% (short of cutting one open, and taking a high-res photo and then comparing with others that might be similar). The wiring (bonding) and encapsulation may well be the same factory too, or may be different (no way to tell that).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago in reply to dank123

    The internal die (chip) is made in the same factories, i.e. identical quality level, but you won't know which specific transistor that it electrically matches 100% (short of cutting one open, and taking a high-res photo and then comparing with others that might be similar). The wiring (bonding) and encapsulation may well be the same factory too, or may be different (no way to tell that).