Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Audio Power Transistors - Buying in Bulk
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 18 replies
  • Subscribers 333 subscribers
  • Views 3160 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Audio Power Transistors - Buying in Bulk

dank123
dank123 over 2 years ago

Hi All,

Does anyone have a solid opinion on the quality of Multicomp Pro MJ15003 and MJ15004 power transistors (Newark# 76AH5818 and 76AH5819)? I want to stock up on these parts as I use them quite a bit and the Multicomp Pro ones come in at about half the cost of the other name brand devices. I use these parts for vintage audio amplifier repair and the occassional amp build from scratch. Not exactly critical applications, but I'd like to get some assurance that they are at least worth the money. Otherwise, I may as well just spend the extra and get ONSEMI. Has anyone tested this Multicomp Pro transistors to see what conditions they fail under as compared to the ONSEMI ones? 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago +4
    Looking at the data sheets for the parts I would sy that there are definite causes for concern: The features section of the Multicomp data sheet seems to be for a different part. Multicomp features…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to michaelkellett +3
    michaelkellett said: almost all your customers would rather have the Onsemi parts. "No one gets fired for buying IBM" was the IT equivalent for that.
  • shabaz
    shabaz over 2 years ago in reply to anniel747 +3
    "Why would you think it's a fake?" Because your photo was taken from a counterfeit transistor web-page that explains it in black-and-white: As you can see from the red highlighted text, the purchaser…
Parents
  • michaelkellett
    0 michaelkellett over 2 years ago

    Looking at the data sheets for the parts I would sy that there are definite causes for concern:

    The features section of the Multicomp data sheet seems to be for a different part.

    Multicomp features from data sheet.

    image

    The gain is wrong, the specified current range is wrong, what does "diode protection' even mean ?, there is no base emitter resistor in the Motorola/On Semi parts.

    The figure for Hfe is specified more reasonably in the data section fo the data sheet:

    image

    There is, as Shabaz has pointed out very little information in the Multicomp data sheet (most of the graphs on the Onsemi data sheet are omitted).

    So if the data sheet is both brief and self-inconsistent you have very little idea of what you are buying.

    On the way home last night I was thinking about the set up needed to test these parts for performance over a reasonable working range ( maybe not needing to go as far as the full specified rang).

    You would need a dual channel SMU or equivalent, capable of 10A (@ 2V) and 140V(@1A-pulsed), and most difficult, 5A at 50V

    Some way of measuring the thermal resistance - this is challenging - you need to put serious power into the device. keep the case temperature constant and measure the chip temperature.

    I guessed it would take a couple of weeks work to set up a rig to do this (non automated and over a limited number of set points) using a suitable lab power supply and standard electronic components with some kind of low power pulse generator and a scope. Or you could just buy the proper gear but expect no change from £50k.

    Is this a good use of time ?

    I would think that it isn't because the parts are not well enough specified to be sure that you would be getting a consistent product, regardless of the economics.

    The real thing from Mouser cost £4.53 if you buy 100, the Multicomp part is £3.26 - so you save £1.27 on each one and as Shabaz says, almost all your customers would rather have the Onsemi parts.

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dank123
    0 dank123 over 2 years ago in reply to michaelkellett

    I agree.

    The ONSemi parts are only slightly more expensive than the Multicomp on Newark when you buy 10 pieces. May as well just get ONsemi.

    One practical way to test the Multicomp devices would be to take a stereo amplifier and replace the transistors in one of the two channels, then run it for a while to see what happens. Or, run it with a dummy load connected and stress it out. 

    There is a pretty good diversity of opinions on here and I think I have all the info I need. Thanks to everyone who chimed in.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dank123
    0 dank123 over 2 years ago in reply to michaelkellett

    I agree.

    The ONSemi parts are only slightly more expensive than the Multicomp on Newark when you buy 10 pieces. May as well just get ONsemi.

    One practical way to test the Multicomp devices would be to take a stereo amplifier and replace the transistors in one of the two channels, then run it for a while to see what happens. Or, run it with a dummy load connected and stress it out. 

    There is a pretty good diversity of opinions on here and I think I have all the info I need. Thanks to everyone who chimed in.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to dank123

    The dummy load vs specs approach would be the safest one.

    But do we know if the original amplifier would actually have survived a bench test with a dummy load vs specs?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 2 years ago in reply to dank123

    Places where a device with a more restricted SOA might fail are usually not exercised with a dummy resistive load.

    But if you try more difficult loads you are into the region of Jan's conundrum where you don't know if the full spec part would have done better.

    So to be sure that the parts of equivalent robustness  you would need to test both types to failure - which might be fun but rather time consuming and expensive.

    Comparing both channels with different parts is a reasonable compromise but most audio amplifiers are not that well cooled so you may be mainly comparing the susceptibility to overheating - which in turn will be influenced by how well the parts are contacting the heatsink etc. etc.

    Please let us know how you get on - and if any parts fail in interesting ways !

    MK