Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Seeking Portable Solution for Rapidly Cooling 10 Tons of Water from 100°C to 30°C for Transport
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Subscribers 334 subscribers
  • Views 3257 views
  • Users 0 members are here
  • wastewater treatment
  • thermal
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Seeking Portable Solution for Rapidly Cooling 10 Tons of Water from 100°C to 30°C for Transport

Maral
Maral over 2 years ago

I'm working on a water treatment project where we need to transport 10 tons of water from the production site to a treatment plant. The challenge is that the water exits the production process at 100°C, and this high temperature risks damaging the pump system on our transport truck, leading to operational issues. I'm looking for a portable and efficient solution that can rapidly cool this large volume of water from 100°C down to 30°C before it enters the truck’s system. The cooling mechanism needs to be compact enough to fit within the truck's infrastructure and must be compatible with the truck and tunnel system materials to prevent rust and corrosion. Has anyone dealt with a similar challenge? What technologies, materials, or approaches would you recommend to achieve this rapid cooling? Any insights on energy requirements or practical considerations would also be greatly appreciated! Thanks in advance for your help! 

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 2 years ago +4
    Maral Portable and inexpensive... two options. #1 big radiator. Source second-hand from someone that blew up their large generator engine. Not common but not unobtainable either. Challenge is this requires…
  • michaelkellett
    michaelkellett over 2 years ago +2 verified
    3GJ = 817kWh of energy. And you plan to just waste this energy - think again ! If you want more helpful offers you need to explain a LOT more. Who are you (engineer, student, etc etc), what's the…
  • michaelkellett
    michaelkellett over 2 years ago in reply to Maral +2 verified
    Great - now you have explained the problem in detail I can see that most of the suggestions made are not much help ! What is the diameter of the tank access ? From what maximum depth must the water…
Parents
  • michaelkellett
    +1 michaelkellett over 2 years ago

    3GJ = 817kWh of energy.

    And you plan to just waste this energy - think again !

    If you want more helpful offers you need to explain a LOT more.

    Who are you (engineer, student, etc etc), what's the project,what's the environment. How often, is there a budget ?

    The classic way to dump this amount of heat energy is use a cooling tower where you let the water cascade down over bumps through air. The tower is designed so that convection will make the warmed air rise up through it so at least the air pumping energy comes out of the heat from the water. You still need a pump to get the water up to the top and all the energy in the water is wasted.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Maral
    0 Maral over 2 years ago in reply to michaelkellett

    Hi Everyone,

    I wanted to follow up and clarify the situation I previously described regarding the challenges we're facing with water management at a thermal power plant.

    The Core Problem:

    • Fractured Water Tunnels: We've identified that the water transport tunnels from the thermal power plant have fractures. This is causing hot water to leak into an underground concrete tank, which is situated above the heat line.

    • Temperature Escalation: Over time, this water, which starts at temperatures close to 100°C, cools down slightly during transfer, but it still maintains a temperature of about 80°C when it reaches the tank. The tank itself has a small hole, which prevents the water from cooling off naturally and instead allows it to retain, or even gradually increase, its temperature.

    Operational Challenge:

    • Vacuum Truck Limitations: Our current vacuum trucks aren’t equipped to handle such high temperatures. Vacuuming hot water means also vacuuming hot air, which leads to technical failures in the trucks. As a workaround, we've been adding cold water to bring down the temperature before vacuuming, but this isn’t efficient. The water left behind in the tank heats up again by the time the truck returns, leading to water waste and increased operational costs.

    Proposed Solutions:

    1. Cooling Before Vacuuming:

      • Implementing a heat transfer system or portable chillers to cool the water quickly.
      • Using collapsible tanks to store hot water temporarily, though this solution isn’t ideal in urgent situations.
      • Exploring the use of non-toxic chemical cooling agents.
    2. Vacuuming While Hot:

      • Considering a switch to vacuum trucks that can withstand temperatures above 80°C.
      • Adding insulation to the vacuum lines to manage heat transfer better.
      • Using specialized pumps for hot liquids, separate from the main vacuum system.

    Additional Insights Needed:

    I'm seeking further insights to refine these solutions or explore new ones. Specifically:

    • Temporary Cooling Methods: Any field-tested cooling methods that can be deployed quickly and effectively.
    • High-Temperature Vacuum Systems: Recommendations on vacuum systems or pumps designed for handling high-temperature liquids.
    • Emergency Solutions: Any innovative or unconventional approaches that could be effective in urgent scenarios.

    Thanks again to everyone who has already provided feedback. I hope this clarification helps, and I’m eager to hear any additional advice you might have!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    +1 michaelkellett over 2 years ago in reply to Maral

    Great - now you have explained the problem in detail I can see that most of the suggestions made are not much help !

    What is the diameter of the tank access ?

    From what maximum depth must the water be pumped .

    I'm thinking that you could lower a high temperature submersible pump into the tank and pump the water out. Possibly allowing it to flow through a fan assisted radiator for additional cooling before it gets into the truck.

    I found these on the web:

    https://flowsolutions.com/products/kbf-series/

    there are lots more people offering down hole submersible high temperature pumps.

    If the access is a very small diameter (< 40cm) there are more exotic solutions like hydraulic submersible pumps.

    But you might get away with a simple borehole electric pump:

    https://www.geoquipwatersolutions.com/high-temperature-borehole-pumps-4-and-5-inch-pumps.html

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    +1 michaelkellett over 2 years ago in reply to Maral

    Great - now you have explained the problem in detail I can see that most of the suggestions made are not much help !

    What is the diameter of the tank access ?

    From what maximum depth must the water be pumped .

    I'm thinking that you could lower a high temperature submersible pump into the tank and pump the water out. Possibly allowing it to flow through a fan assisted radiator for additional cooling before it gets into the truck.

    I found these on the web:

    https://flowsolutions.com/products/kbf-series/

    there are lots more people offering down hole submersible high temperature pumps.

    If the access is a very small diameter (< 40cm) there are more exotic solutions like hydraulic submersible pumps.

    But you might get away with a simple borehole electric pump:

    https://www.geoquipwatersolutions.com/high-temperature-borehole-pumps-4-and-5-inch-pumps.html

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer